Security settings In order to be able to access a Microsoft Windows 2003 server with a panel or PC you must disable the following security settings on the Microsoft Windows 2003 server.
Under "Start > Programs > Administrative Tools > Security Policy for Domain Controller > Security Settings > Local Policies > Security Options" you locate the security settings.
Applicability The settings described are to be made only
- If you are using a Microsoft Windows 2003 server with Active Directory.
- If the Windows CE 3.0 operating system is installed on the operator panel.
Operator panels with the Windows CE 5.0 operating system are not affected
(e.g. operator panels MP 277 / Mobile Panel 277 and higher). You can check which operating system is being used on the operator panel in the Control Panel under "System > General".
Disabling security settings:
- Microsoft network (server): Digitally sign communications (always).
- Microsoft network (server): Digitally sign communications (if client agrees).
- Network security: "LAN Manager authentication level" change to "Send LM & NTLM responses".
After you have made the settings you must reboot the computer. This makes the changes made effective.
Note: The changes made lower the security level of the network communications. Please check beforehand with your network administrator whether you are permitted to make these changes.
How to incorporate a panel in a local network is described in Entry ID: 13336639 .
Keywords:
Panel, Network, Server settings
|