show the entry list
WinCC flexible ES -- Creating HMI configurations -- Configuring alarms and messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Message indicator continues to be displayed despite counter at zero
How do you start a sound file via a script in the WinCC flexible PC Runtime?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How can you determine the bit number in WinCC for the "Trigger address", the "Acknowledgement PLC" bit and the "Acknowledgement HMI" bit for creating bit messages?
Which configuration steps have to be taken in SIMOTION SCOUT and WinCC flexible to enable Alarm_S messages and technological alarms to be displayed in WinCC flexible Runtime?
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
How do you display messages in WinCC flexible?
How can you evaluate the ACK button on a touch operator panel in WinCC flexible?
How can you have system error messages from a SIMATIC S7-300 / 400 displayed in WinCC flexible?
How do you change and display SIMATIC WinCC flexible system events during configuration?
How can you change the ProTool default alarm window setting in WinCC flexible?
How can I acknowledge alarms in WinCC flexible via the PLC?
Why aren't messages output on the event recorder?
Why isn't the "Message display" shown in the foreground, but is covered by picture objects?
Why are no messages from the S7 diagnostics buffer display in WinCC flexible?
How can you get the diagnostics buffer to be displayed in WinCC flexible?
Which settings need to be made in order to display alarm events after a specified point in time?
How can you create messages with externally preset texts as mass data and process them with Excel in WinCC flexible?
How do you display messages in WinCC flexible?
Part number:

 
Instructions:
WinCC flexible offers the following options for displaying messages on the operator panel:

  • Alarm View:
    The alarm view is configured for a specific picture. Depending on the size configured, the alarm view can display multiple messages at the same time. You can configure multiple alarm views for different alarm classes and in different pictures.
  • Alarm Line:
    The alarm line permits you to display the latest message available in Runtime (Alarm View: "Properties > Layout > Mode > Line").
  • Alarm Windows:
    The alarm window is configured in the "Template" for the pictures and is thus a component of all the pictures of a project. Depending on the size configured, it can display multiple messages at the same time. Closing and reopening of the alarm window can be event-controlled.
  • Alarm Indicator:
    The alarm indicator is a graphical icon that indicates messages that are available or are to be acknowledged, depending on the configuration. The alarm indicator can only be configured in the template.

Below are tips on creating/editing the alarm view/window. 

Shifting columns of the alarm view/window:
Right-click the alarm view/window. Click on "Edit" in the pop-menu that opens. Now you can move the individual "column heads" with the left mouse button.


Fig. 01
 

Creating your own alarm classes:
You can add more alarm classes to the existing alarm classes (Diagnosis Events, Errors, System, Warnings). It is thus possible to assign a separate "alarm class" for each subsystem. You then assign the alarm class accordingly to an alarm view/window.
Only the messages from that subsystem are then displayed.

The "alarm classes" are in the project tree structure under "Alarm Management > Settings > Alarm Classes". The following figure shows the modified "alarm classes" in the alarm view.


Fig. 02
 

Editing buttons:
Under "Properties > Settings" of the alarm view/window you can assign buttons to the display ("Infotext" button, "ACK" button, "Edit" button). You cannot change the icons of these buttons. If you wish to use your own texts/icons, you can create your own buttons to which you assign the desired texts/icons.

The functions are available under the Properties of the buttons ("Properties > Events > Press > Keyboard operation for screen objects > Alarm...").

Color configuration of the alarm classes:
In order to better differentiate between the messages statuses (Activated, Deactivated, Acknowledged) you can configure colors for the alarm classes. Please note that the message on which the current "focus" is positioned is not displayed in the color configured.

For the configured colors of the alarm classes to be displayed in Runtime you enable "Use alarm class colors" in the project window under "Alarm Management > Settings > Alarm Settings > General".

Configured tags in the display text:
If you have configured a tag in the display text in order to output the current measured value at the time of error, for example, this value is "static". This means that the value of the tag is displayed with the value that the tag had when the message was triggered. The value is not updated subsequently in the alarm view/window.

Line breaks in the bit message texts:
You cannot configure line breaks in an alarm line. Line breaks are made automatically on the operator panel during Runtime.

A "non-configure" alarm display is shown when an error occurs:
If you migrate a ProTool configuration to WinCC flexible, in the "Template Picture" you check whether an alarm display is there. Under "Properties > Layers" of the "Template Picture" you show all the layers ("Show all layers" button). This function once again displays all the objects that might have been deselected when selecting a layer.

Notes on configuring error messages and on handling alarm views/windows:
More information on the topics mentioned above is available in the Online Help of WinCC flexible and in Entry ID: 21976869 .

 Entry ID:23843774   Date:2006-08-30 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour