Description: The following requirements must be fulfilled for the "Routing" function with SIMATIC S7 modules via MPI, PROFIBUS and Industrial Ethernet connections:
Software requirements:
- MPI and PROFIBUS connections:
- At least STEP 7 V5.0+SP1, however a current version of STEP 7 is recommended.
- For the Softnet PROFIBUS cards (CP 5411 (ISA), CP 5511 (PCMCIA), CP 5611 (PCI), CP 5611 (on board)) you don't need any other drivers, because they are provided by STEP 7.
- For the Hardnet PROFIBUS cards (CP 5412(A2) (ISA), CP 5613/5614 (PCI)) you need the associated drivers from the SIMATIC NET CD.
- Industrial Ethernet connections:
- At least STEP 7 V5.0+SP1, however a current version of STEP 7 is recommended.
- With CP1612/ CP1512 ,CP1515 and commercially available network cards you need a current release of the SIMATIC NET Softnet IE PG driver (at least Softnet IE PG V3.1).
- With CP1613 and CP1413 you need the products SIMATIC NET IE PG 1613 and SIMATIC NET IE PG1413 respectively.
- For implementation of a TS Adapter:
- TeleService S7 V5.0 or higher.
Hardware requirements:
- You need routing-compatible modules. Refer to Entry ID 584459 for routing-compatible modules, or take them directly from the hardware catalog of the STEP 7 Hardware Configuration.
  Fig. 01
You still need one of the Online CPs mentioned under "Software requirements" or the TS Adapter V5.0 or a PC Adapter V5.0.
Note:
- The last module that is to be addressed via the routing function does not have to be routing-compatible.
- If you wish to route via an S7 CPU which is configured as a PROFIBUS DP slave, you have to activate the "Test, Commissioning, Routing" option in the HWCONFIG > DP interface properties > "Operating Mode" tab. You can also find this information in the STEP7 Online Help ("Operating Mode" tab).
Configuration procedure:
You must configure all the stations that lie between the Start device and the target device in one STEP 7 project.
Sample configurations:
- Routing with modem and TS Adapter
  Fig. 05
- Routing with ISDN Router:
  Fig. 06
|