show the entry list
STEP 7 -- Creating S7 programs -- Optimizing program sequences
Difference in the cycle time during DB accesses
Edge trigger flag misses out edges when using flag bit 0
Information on the topic of "Optimizing program sequences"
How can you increase the performance of HMI devices?
How can the program runtime be optimized if the main memory of the CPU is too small for the runtime-relevant STEP 7 program?"
How can I optimize PID Temperature Control using STEP 7 V5.3 SP2?
ProTool -- Configuring and programming communication -- Configuring communication to S7
Settings in "Status/Force" when using a WinAC MP
Communicating with an S7-200 PLC via PPI using a CP5611 Card with Protool/Pro version 5.10
PPI connection of ProTool/Pro and S7-200
Connecting a ProTool Runtime Panel / PC to an S7 200 via PROFIBUS DP
Connecting a panel to a S7 300/400 controller
Connection settings for a communication between ProTool/Pro and WinAC
How can you increase the performance of HMI devices?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect an operator panel (ProTool) to an H system (S7-400H)?
Connecting a ProTool/Pro Runtime (PC) via Ethernet to an S7-300 or S7-400 station from SIMATIC NET CD 07/2001
ProTool/ProRT and S7-200 with PC/PPI-Cable
Ethernet communication between a ProTool/Pro Runtime (PC) and a CP243-1 (S7-200)
Coupling between ProTool/Pro and WinAC
Coupling between Operator Panel and WinAC Basis/WinAC RTX V4.0
Connection between SIMATIC NET OPC server, ProTool/Pro RT and SIMATIC S7
Connecting an OP as DP slave - configuration of DP direct control buttons
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to S7
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to configure communication between an operator panel and an S7 station via S7 routing?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which ports are used by WinCC flexible?
How can you increase the performance of HMI devices?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
How can you increase the performance of HMI devices?
Part number:

Description
Through continual innovation the performance of controllers has increased by five to ten fold in the past three years. The cycle times of the controllers became increasingly shorter. The cycle times of the S7-300 controllers, for example, now frequently lie between 9ms and 16ms.
The time left for the CPU to communicate with the HMI devices is therefore becoming ever shorter, because only a certain percentage of the total cycle time is available for communication. The percentage of the time the CPU uses for communication is a minimum of about 3.5% of a cycle time of 15ms.

The FC630 function is for improving the performance of HMI services. An SFC is called in the FC630, which increases the time assignment for the HMI services according to the value of the parameter TSx:

  • TSx = 0: restores the initial status
  • TSx = 1: default setting
  • TSx = 8: increases the CPU cycle time by approx. 50%

The TSx value increases the CPU cycle time by 6.25% per unit.

Evaluation of RET_VAL:

  • 0000: no error, time factor is valid and accepted.
  • 800x: error, the block must be restarted.

The valid factor is effective without any further modification until the power is switched off.

The "HMI" task
The CPU program is executed in different tasks ("subprograms"). In the "HMI" task, the CPU communication with the HMI devices is controlled by the operating system (data acquisition, data processing, data transfer and data fetching). The "HMI" task has a certain portion of the cycle time allotted to it. If this time expires, the "HMI" task is interrupted and the CPU continues with its cyclic program processing. The "HMI" task can be interrupted by higher-priority tasks. Higher-priority tasks include time interrupts and delay interrupts, for example.

Note
The FC630 cannot be used in S7-400 CPUs because there is not the requisite firmware support. Furthermore, HMI response times cannot be shortened because the "HMI" task already has the second highest priority in the S7-400 CPUs.

Difference between FC630 and the setting in the CPU properties (cycle load through communication)
In the CPU properties there is also the "Cycle load through communication" parameter. This parameter only affects the CPU message traffic. The FC630 comes into effect early on at data acquisition and in processing the data, which is why the S7-300 CPU's cycle time can greatly extend itself if the FC630 is not handled properly.

Bus protocols for which you can use the FC630
You can use the FC630 for communication via

  • MPI
  • PROFIBUS
  • PROFINET

Requirements before using FC630
Since incorrect use of the FC630 can lead to malfunctions, in particular the CPU cycle time might increase enormously, you should check the following before using the FC630.

  • How high are the cycle times of your CPU? It is particularly useful to operate with cycle times of between 9ms and 16ms, because the percentage of the time used for communication is a minimum of about 3.5% of a cycle time of 15ms. The percentage of the time used for communication with a cycle time of about 32ms is again a minimum of approx. 4.8%. This is why it is useful to implement the FC630 also with cycle times of between 25ms and 32ms. It is not generally useful to implement the FC630 for cycle times greater than 50ms. However, whether or not it is useful to implement the FC630 always depends on your system (number of HMI devices, number of tags polled ...).

Note
Via STEP 7 under "PLC > Diagnostics/Setting > Module status > Cycle time" you can read out of your module the longest, shortest and current cycle time since transition from STOP to RUN.
Via the local data of the OB1 you can also read out the runtime of the previous cycle, the minimum cycle time since the last start and the maximum cycle time since the last start.

  • Are there time critical subprocesses in the system that do not permit an increase in cycle time? If this is the case, you can also check whether the time critical subprocesses could be controlled via a cyclic interrupt. You should note here that cyclic interrupts interrupt the "HMI" task when called and thus influence HMI performance.

You can implement the FC630 function with S7-300 CPUs and C7 devices. Whether the FC630 can be implemented depends on the CPU type and the firmware version. The function described is valid for the CPU-31x modules as from firmware versions V2.3.2, V2.1.6 and V2.0.10.

The FC630 can also be used for the CPU319-3 PN/DP modules as from firmware version V3.2. However, the firmware version V3.2 contains an improved HMI Turbo that only works for the acyclic HMI services.

  • This does not speed up the cyclic HMI services, so the FC630 continues to be need to improve performance.
  • The new function - "Prioritized OCM communication" - has been introduced in all devices as from firmware version V3.2, but it can only be configured in the CPU315F-2 PN/DP modules onwards.
  • The HMI Turbo is only hidden for the modules CPU312 to 315-2DP and can be configured with the new function FC2551.

More information about "Prioritized OCM communication" is available in Entry ID: 49749632.

The attached download contains an archived sample STEP 7 project with the FC630 described above. Use of the FC630 is described in detail in the document below.

Description_Performance_FC630 ( 93 KB )

Performance_FC630.zip ( 30 KB )

Keywords
WinCC, ProTool, Panel, HMI, Operate, Monitor, Performance

 

 Entry ID:23818213   Date:2011-05-16