show the entry list
WinCC flexible ES -- Creating HMI configurations -- Loading and testing configurations
How can you transfer a WinCC flexible configuration without configuration software to an operator panel (Pack&Go)?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC?
Which settings do you have to make so that a ProTool project or WinCC flexible project can be transferred via TeleService Adapter IE?
What can be the causes of the project download via TeleService not working?
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel?
How can you transfer a WinCC flexible project serially to a panel?
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
How can you simulate with WinCC flexible the function keys of the various Windows-based operator panels via the PC keyboard?
Which cable can you use for data transfer between a Micro Panel and a configuration PC?
Why can't you simulate the Runtime for an OP73/OP73micro/TP177A/ TP177micro or OP77A in WinCC flexible on a PC?
How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel?
Part number:

 
Instructions:
For transfer of a WinCC flexible configuration via MPI or PROFIBUS you must make settings on the Windows-based panel and on the configuration PC.

Note:

  • Direct transfer from the PC to the Windows-based panel via a PC adapter (RS232 -> MPI/PROFIBUS, USB -> MPI/PROFIBUS) is not supported.
  • Project transfer to a Micro Panel is not possible, because a Micro Panel doesn't have an MPI or PROFIBUS interface.
  • If you wish to integrate your configuration PC into an existing MPI/PROFIBUS network, you must transfer the bus settings of the available MPI/PROFIBUS subnet. Please note that the bus address of the PC in the MPI/PROFIBUS subnet must be unique.

Settings on the operator panel
The figures below are from the MP277. The illustrations might differ from operator panel to operator panel, because not all the functions are available for each operator panel.
 
No. Procedure
1

Settings in "Control Panel"
Open the Transfer dialog in the "Control Panel".

( 65 KB )
Fig. 01 - Control Panel (MP277)

The MPI/PROFIBUS transfer is enabled under "Channel 2". For this you set Channel 2 to "MPI/PROFIBUS". For Channel 2 you also set a check mark for "Enable Channel" and if you wish, "Remote Control".

( 4 KB )
Fig. 02 - Transfer Settings

Note:
The "Remote Control" option permits automatic termination of Runtime on the panel when transfer is triggered via the development environment of WinCC flexible. The panel then automatically switches to Transfer mode.

Note:
In the case of transfer via a TS adapter with modem you should enable "Remote Control", because otherwise the panel does not switch automatically into the Transfer mode.

2

More settings in "Transfer Settings"

  • Open the advanced settings by clicking on the "Advanced" button (Fig. 02).
  • Define whether the WinCC flexible project is to be transferred via "MPI" or "PROFIBUS".
  • Then click the "Properties" button.

( 12 KB )
Fig. 03 - S7 transfer settings

3a

Version A - MPI

MPI settings
If you wish to transfer a project via PROFIBUS - Version B, then you can skip this point and go directly to Point 3b.

The following dialog (Fig. 04) shows the current MPI bus parameters of the panel.

If the panel is the only master on the bus, then set the check mark for "Panel is the only master on the bus" and assign a unique bus address (Address) for the device.

Note:
If it is not necessarily required by the system to change the other network parameters, you should use the default network parameters given.
These network parameters must match the settings in the SIMATIC station (e.g.: CPU or CP).

( 26 KB )
Fig. 04 - MPI bus parameters

Note:
If other masters (panels) are to be connected to the bus, then disable the option "Panel is the only master on the bus".

3b

Version B - PROFIBUS

PROFIBUS settings
If you are using Version A via MPI, you can skip this point and go directly to Point 4.

The following dialog shows the current PROFIBUS parameters of the panel.

If the panel is the only master on the bus, then set the check mark for "Panel is the only master on the bus" and assign a unique bus address (Address) for the device.

Note:
If it is not necessarily required by the system to change the other network parameters, you should use the default network parameters given.
The network parameters must match the settings in the SIMATIC station (e.g.: CPU or CP).

( 30 KB )
Fig. 05 - PROFIBUS bus parameters

Note:
If other masters (panels) are to be connected to the bus, then disable the option "Panel is the only master on the bus".

4 Close the dialog window
Close all the open dialogs with "OK".
Also close the "Control Panel" and enable the Transfer mode.

Settings on the configuration PC
For communication between panel and configuration computer you must set the bus parameters as on the panel (except for the node address).
 
No. Procedure
1 Open PG/PC interface
In the Control Panel of your configuration computer you open the menu "Set PG/PC Interface".

( 46 KB )
Fig. 06 - Control Panel

Alternatively you can also open the PG/PC interface via the SIMATIC Manager.

( 18 KB )
Fig. 07 - STEP 7 Manager

2 Setting the PG/PC interface

( 22 KB )
Fig. 08 - PG/PC interface

For MPI transfer from the PC to the panel you select one of the following settings (CP = communication processor) that you use for the hardware:
 
S7ONLINE  (STEP 7)

-->

CP5512 (MPI)
CP5611 (MPI
CP5611 A2 (MPI)
CP5613 (MPI)
CP5613 A2 (MPI)
CP5613 FO (MPI)
CP5614 (MPI)
CP5614 A2 (MPI)
CP5614 FO (MPI)
CP5611 A2 (MPI)

For transfer via PROFIBUS you select one of the following interface parameterizations:
 
S7ONLINE  (STEP 7)

-->

CP5512 (PROFIBUS)
CP5611 (PROFIBUS)
CP5611 A2 (PROFIBUS)
CP5613 (PROFIBUS)
CP5613 A2 (PROFIBUS)
CP5613 FO (PROFIBUS)
CP5614 (PROFIBUS)
CP5614 A2 (PROFIBUS)
CP5614 FO (PROFIBUS)
CP5611 A2 (PROFIBUS)

Note:
If none of the interfaces listed above is shown, you can install interfaces manually by clicking on the "Select..." button in the "Interfaces" "Add/Remove" field.

3a

Version A - MPI

Set interface parameters

If you wish to transfer a project via PROFIBUS - Version B, then you can skip this point and go directly to Point 3b.

  • Click the "Properties..." button. (Fig. 08).
  • Set the check mark for "PG/PC is the only master on the bus" if no other master is connected in the subnet.
  • Change the network-related parameters - except the node address - to match the settings on the panel for MPI (Fig. 4).
  • Close the Properties dialog box with "OK".

( 8 KB )
Fig. 09 - MPI properties

Note:
The node address must be unique, i.e. it must not be used by any other nodes in the subnet. Please note that the address must not be greater than the highest permissible Highest Station Address (HSA).

3b

Version B - PROFIBUS

Interface parameters
If you are using Version A via MPI, you can skip this point and go directly to Point 4.
  • Perform the same steps as for the MPI interface parameters (Point 3a).
  • The network-related settings for the PROFIBUS communication - except the node address - must match the interface settings on the panel (Fig. 5).
  • Close the Properties dialog box with "OK".

( 12 KB )
Fig. 10 - PROFIBUS properties

Note:
The node address must be unique, i.e. it must not be used by any other nodes in the subnet. Please note that the address must not be greater than the highest permissible Highest Station Address (HSA).

4 SIMATIC NET Diagnostics
  • Open the "Diagnostics" to test the MPI/PROFIBUS connection between the PC and the panel.
  • Perform network diagnostics for the CP by clicking on the "Test" button.
( 13 KB )
Fig. 11 - SIMATIC NET Diagnostics
 

Node address

Node
10 HMI operator panel
2 SIMATIC station (e.g.: CPU)
0 PG/PC interface (e.g.: CP5512)
Table 01

Note:
If the operating mode is not "OK", check the hardware and the bus parameters (Points 3a and 3b) in the PG/PC interface. If necessary, check the CPU settings in the Hardware Configuration of the SIMATIC Manager and the settings on the panel.

Note:
More information on error messages is available via Help (see button) in the dialog window under "Error messages > Error message".
In order to determine the current bus parameters of a subnet you can also proceed as described in Point 5:

  • If the operating mode or network diagnostics is "OK", then click on the "Read" button. The table shows the bus node that can be reached (Address 10 = Panel).
  • Close the open dialogs with "OK".
5 Determine bus parameters
You can skip this point if the operating mode is "OK" in Point 4 and the bus nodes are displayed after read-out.

Set the CP adapter of the interface parameterization to "AUTO" and click the "Properties..." button.

Example:
"S7ONLINE (STEP7) -- > CP5512(AUTO)"

( 22 KB )
Fig. 12 - AUTO properties

Start the network identification by clicking on the "Start Network Detection" button.

( 9 KB )
Fig. 13 - Network identification

( 39 KB )
Fig. 14 - Analysis of the bus parameters

Note:
Via the "Bus Parameters..." button you can have all the relevant bus parameters displayed in detail.

Note:
If the bus parameters cannot be determined or a synchronization error occurs, then you should check the following points:

  • PROFIBUS or MPI cable (replace where necessary).
  • Correct setting of the terminators.
  • Bus parameters on the panel and in the PG/PC interface.
  • Physical connection between the CP and the panel.
  • Power supply of the SIMATIC stations.
  • If necessary, compile and transfer the Hardware Configuration in the SIMATIC Manager for all relevant SIMATIC stations (e.g. CPU).

More information is available in the Help of the MPI/PROFIBUS diagnostics in each case.

Settings in WinCC flexible
As an option you can also integrate the WinCC flexible project into a STEP 7 project. The two possible versions are explained in the following table.
 
No. Procedure
1 Create connection
  • In the project tree structure under "Communication" you select the "Connections" tab.
  • In WinCC flexible you insert a new connection in the menu under "Insert > New Object - Connection".
    Alternatively you can double-click an empty field in the table in the "Connections" tab and create a new connection.

( 89 KB )
Fig. 15 - Connections

2a

Version A - Non-integrated project

Define parameters
If you have created an integrated WinCC flexible project or would like to integrate it into STEP 7, you can skip this point and go directly to Point 2b.

Define the relevant parameters that you have already specified in the panel and in the PG/PC interface. The MPI or PROFIBUS protocol can be defined separately under the option Network > Profile.
For networking with MPI or PROFIBUS you need the interface IF1 B (for panels) or MPI/DP (for PC-based operator panels).

( 134 KB )
Fig. 16 - Connection parameters

Note:
If you do not implement an S7-300/400 CPU as communications partner, then change the communication driver.

The following communication drivers that support the MPI or PROFIBUS protocol are available:

  • SIMATIC S5 DP (only PROFIBUS)
  • SIMATIC S7-200
  • SIMATIC S7-300/400
  • SIMOTION
2b

Version B - Integrated project

Defining the station
You can skip this section and go directly to Point 3 if you do not want to use an integrated project.

If you have not already inserted the project in the SIMATIC Manager, you can do this via the WinCC flexible menu "Project > Integrate in STEP 7...".

  • Open NetPro in the SIMATIC Manager. Alternatively you can also open the Hardware Configuration of the HMI operator panel.

( 24 KB )
Fig. 17 - Open NetPro

  • In the NetPro dialog (Fig. 18) you double-click the HMI MPI/DP interface of the "SIMATIC HMI Station(1)".
  • Click on the "Properties..." button in the Properties dialog window of the HMI MPI/DP interface.
  • Mark the MPI(1) subnet of the HMI station then click "OK".

    Note:
    You can use the "New..." button to add more subnets. Note here that the HMI station and associated SIMATIC station must be in the same subnet or connected together via a routing-compatible station. More information on S7 Routing is available in Entry ID: 22255588.

( 72 KB )
Fig. 18 - Select station

  • Close the dialog window with "OK".
  • Save and compile your configuration via the menu "Network > Save and compile...".
  • Where applicable, transfer your changed hardware configuration to all the relevant SIMATIC stations and terminate NetPro.
  • Via the corresponding subnet you select the station with which the operator panel is to communicate.

( 132 KB )
Fig. 19 - Select station

3 Project transfer
  • Open the dialog window under "Project > Transfer > Transfer Settings...". Alternatively you can also open the transfer settings via the toolbar (1).
     
  • In the "Transfer Settings" dialog you select the relevant operator panel (2) - only necessary in the case of multiple operator panels.
     
  • Select MPI/DP (3) as the Transfer mode and enter the node address of the operator panel.
     
    Note:
    For the possible transfer options please refer to the relevant manual or Entry ID: 19109408
     
  • With the "Transfer" button (4) you can now transfer your configuration to the panel.

( 99 KB )
Fig. 20 - Project transfer

Note:
If you do not want to transfer yet, you can save the settings with "Apply".
With the first transfer of the project to an operator panel you should disable the "Delta transfer" option and enable the "Overwrite password list" option.

Note:
After transfer the panel adopts the parameters set in the "Connections" tab.

More information is available in the following entries.
 
Topic Entry
Project transfer (released cables,...) Entry ID: 19109408
Communication between SIMATIC station and panel in the following manuals:
"WinCC flexible 2005 Communication Part 1"
"WinCC flexible 2005 Communication Part 2"
Entry ID: 18797552
Entry ID: 18797249
Transfer via S7 Routing over MPI/PROFIBUS and Ethernet (as from WinCC flexible 2005) Entry ID: 32235096
OS update with MPI/PROFIBUS Entry ID: 19701610

 Entry ID:23802404   Date:2011-08-26 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour