Configuration Notes: With the extended PROFINET diagnostics it is possible to have functions like the diagnostics and parameterization of integrated Ethernet interfaces (e.g. fiber-optic diagnostics and topology configuration). The PROFINET IO-Devices that support extended PROFINET diagnostics are configured in the Hardware Configuration in STEP 7. They are available in the hardware catalog and have additional ports e.g. interface modules as subslots in Slot 0.
Example: ET200S with and without PROFINET diagnostics

Fig. 01
The following IO-Controllers support the extended PROFINET-Diagnostics:
| Module |
Firmware |
MLFB |
| PC CPs |
| CP1616 |
from V2.0 |
6GK1 161-6AA00 |
| CP1604 |
from V2.0 |
6GK1 160-4AA00 |
| SIMATIC NET PC-Software |
| SOFTNET PROFINET IO |
from V7.1
(Edition 2008) |
6GK1704-1HW71-3AA0 |
| Embedded and PC-based Automation |
| WinAC RTX 2008 |
from V4.4 |
6ES7 671-0RC06-0YA0 |
| S7-mEC, EC31-RTX |
from V4.4 |
6ES7 677-1DD00-0BB0 |
| S7-400 CPUs |
| CPU 414-3 PN/DP |
- |
6ES7 414-3EM05-0AB0 |
| CPU 416-3 PN/DP |
- |
6ES7 416-3ER05-0AB0 |
| CPU 416F-3 PN/DP |
- |
6ES7 416-3FR05-0AB0 |
| S7-300 CPUs |
| CPU 315-2 PN/DP |
from V2.5 |
- |
| CPU 315F-2PN/DP |
from V2.5 |
- |
| CPU 317-2 PN/DP |
from V2.5 |
- |
| CPU 317F-2PN/DP |
from V2.5 |
- |
| CPU 319-3 PN/DP |
from V2.5 |
6ES7318-3EL00-0AB0 |
| CPU 319F-3 PN/DP |
from V2.5 |
6ES7318-3FL00-0AB0 |
| Industrial Ethernet CPs |
| CP343-1 Standard |
from V2.0 |
6GK7343-1EX30-0XE0 |
| CP343-1 Advanced |
from V1.0 |
6GK7343-1GX30-0XE0 |
| CP443-1 Standard |
from V1.0 |
6GK7443-1EX20-0XE0 |
| CP443-1 Advanced |
from V2.0 |
6GK7443-1GX20-0XE0 |
| ET 200S |
| IM151-8 PN/DP CPU |
from V2.7 |
6ES7 151-8AB00-0AB0 |
| IM151-8F PN/DP CPU |
from V2.7 |
6ES7 151-8FB00-0AB0 |
| ET 200pro |
| IM154-8 CPU |
from V2.5 |
6ES7 154-8AB00-0AB0 |
The following IO-Devices can use the extended PROFINET-Diagnostics:
| Module |
Firmware |
MLFB |
| PC CPs |
| CP1616 |
from V2.0 |
6GK1 161-6AA00 |
| CP1604 |
from V2.0 |
6GK1 160-4AA00 |
| Industrial Ethernet CPs |
| CP343-1 Advanced |
from V1.0 |
6GK7343-1GX30-0XE0 |
| ET 200S modules |
| IM151-3PN FO |
from V4.0 |
from 6ES7 151-3BB21-0AB0 |
| IM151-3PN ST |
from V4.0 |
from 6ES7 151-3AA20-0AB0 |
| IM151-3PN HF |
from V4.0 |
from 6ES7 151-3BA20-0AB0 |
| IM151-3PN HS |
- |
from 6ES7 151-3BA50-0AB0 |
| ET 200M modules |
| IM 153-4PN |
- |
6ES7 153-4AA00-0XB0 |
| ET 200pro modules |
| IM154-4PN HF |
- |
from 6ES7 154-4AB00-0AB0 |
| ET 200eco PN |
- |
6ES7 141-6Bx00-0AB0
6ES7 142-6Bx00-0AB0
6ES7 142-6Bx50-0AB0 |
| Network components |
| PN/PN coupler |
- |
6ES7 158-3AD00-0XA0 |
| SCALANCE X20x IRT products |
from V2.1 |
- |
| SCALANCE X200 products |
from V2.1 |
-
see Entry ID: 25472849 |
| SCALANCE X300 products |
- |
- |
| SCALANCE X414-3 E |
from V2.1.1 |
-
see Entry ID: 25355654 |
| SCALANCE X408-2 |
- |
- |
| Gateways |
| IE/AS Interface Link PN/IO |
from V2.0 |
Single AS-i master:
6GK1 411-2AB10
Double AS-i master:
6GK1 411-2AB20 |
The PROFINET IO devices that support the extended PROFINET diagnostics can only be operated on PROFINET IO controllers that likewise support the extended PROFINET diagnostics.
There is a migration GSDML file for some of the PROFINET IO devices listed above for operating the PROFINET IO device on a PROFINET IO controller that does not support the extended PROFINET diagnostics.
Example: PN/PN coupler

Fig. 02
Note: The following applications provide a detailed description, including sample program, of the diagnostics options available in a PROFINET IO system.
- "Diagnostic Methods for PROFINET Network Components (PROFINET IO, SNMP, WBM)" in Entry ID: 21566216
- "PROFINET IO – Diagnostics Processing in the User Program"
in Entry ID: 24000238
|