show the entry list
S7-1200 CPU 12xx -- Product information -- System description
How many measuring points are stored during trace recordings with the S7-1200 and S7-1500?
All-round protection with Industrial Security - System Integrity
How do you change the operating mode with a S7-1200 CPU?
How to send a blank PKW request to the motor drive using the USS instructions as requested in the system manual?
Which SNMP requests can the S7-1200 receive and reply to?
What is the meaning of the terms "sinking" (German: "P-schaltend") and "sourcing" (German: "M-schaltend") in digital modules of SIMATIC?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
What is the range of functions of the S7-1200 App?
How do you perform a firmware update for the S7-1200 as from V3.0 in STEP 7 (TIA Portal) by means of the web server?
How do you change the pulse length for the pulse width modulation (PWM) in the user program of the S7-1200 CPU?
PROFINET general -- Product information -- System description
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
In the TIA Portal, how do you do a firmware update of the distributed IO?
Where can you find information about the configuration and calculation of RCoax systems?
Which settings do you make in LANTEK and LANTEK II from IDEAL Industries for measuring the end-to-end link of 2x2 PROFINET cables?
Which settings do you make in LANTEK and LANTEK II from IDEAL Industries for measuring PROFINET channel test profiles of 2x2 PROFINET cables?
How can you implement the the communication concept of PROFINET CBA with PROFINET IO?
Why is hardware support required for using clock-synchronized real-time communication (IRT) in PROFINET?
How is to possible to transmit real-time messages at the same time as TCP/IP communication in PROFINET?
How can real-time communication (RT) be used with standard Ethernet hardware?
What should you watch out for when reconfiguring in RUN (CiR) if the configuration contains CiR elements and a PROFINET IO system?
Which settings have to be made on the Fluke DTX-1800 cable analyzer for testing cables in a PROFINET network?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Switch on/off phase (central rack and distributed connection)
Comparison of the terms of PROFIBUS and PROFINET
Comparison of PROFINET and PROFIBUS
Industrial Ethernet S7-300/400 CPs -- Product information -- System description (protocols)
Which technical data applies for the SIMATIC Modbus/TCP blocks and for which CPUs and CPs is it released.
How many devices can you connect to an S7-300/S7-400 using the Modbus/TCP protocol?
When compiling a CFC chart, why is the error message "Time stamp conflict" displayed in connection with the Modbus/TCP FBs for S7-400 CPUs?
How many licenses are required for the Modbus/TCP block in the S7-300/S7-400?
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
How are the communication resources assigned in the S7-300?
How do you load the 3D, CAx and ePLAN data for the SIMATIC products?
What are the differences between OPEN MODBUS / TCP Redundant V1 and OPEN MODBUS / TCP Redundant V2?
What should you watch out for when you enable the "SNMP" function in the configuration of the security module?
Which security modules support the dynamic DNS function (DDNS)?
What should you watch out for when enabling and using the security functions of CP343-1 Advanced and CP443-1 Advanced?
What should you watch out for when upgrading from previous modules to the successor module CP443-1 or CP443-1 Advanced?
How do you verify the authenticity of the Siemens modules CP343-1 and CP443-1?
What should you watch out for when operating a port of CP343-1, 6GK7343-1CX10-0XE0 and 6GK7343-1EX30-0XE0 with firmware V2.1 or higher, with 10 Mbit/s half duplex?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
Where do you procure the firmware extension for the CP 343-1 ERPC for database connection?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which modules can you use when implementing software redundancy?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Using C-PLUG with network components and SIMATIC CPs
What properties have the communication services and protocols that can be used in the Industrial Ethernet network?
Behavior of the communication processors during data transfer via TCP connections without RFC 1006
What should you watch out for with the ICMP Redirect (Internet control message protocol) function regarding the IP address of the router used for Industrial Ethernet CPs?
What should you pay attention to with the autonegotiation function for negotiating the LAN mode in Industrial Ethernet CPs?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which modules support the S7 routing function?
In the case of open TCP/IP communication via Industrial Ethernet using T blocks with IE CPs and CPUs, why are different amounts of messages sent when the maximum length of 1452 bytes of user data is transferred?
What properties, advantages and special features does the ISO protocol offer?
What properties, advantages and special features does the UDP protocol offer?
What properties, advantages and special features does the ISO-on-TCP protocol offer?
What properties, advantages and special features does the S7 protocol offer?
What properties, advantages and special features does the TCP protocol offer?
What are the requirements for disabling the PROFINET CBA interface for CP443-1EX40?
"Time Wait" with TCP connection setup
What are the different data block lengths for the various protocols of Send/Receive communication?
What is RFC1006 and what do I need this service for?
Meaning and function of the "Keep Alive" in TCP connections
Industrial Ethernet network components (electrical/optical) -- Product information -- System description
Where is there information about Ethernet communication over 2-wire lines and which modules can be used for this?
How to upgrade GNU Bash on a RUGGEDCOM APE line module Linux® Version (Security Advisory SSA-860967)?
How do you upgrade OpenSSL on a RUGGEDCOM APE line module (Security Advisory SSA-234763)?
How do you upgrade OpenSSL on a RUGGEDCOM APE line module (Security Advisory SSA-635659)?
How do you load the 3D, CAx and ePLAN data for the SIMATIC products?
How do you set the "Port Mirroring" function in the Industrial Ethernet switch SCALANCE X in order to monitor data transfer from a SCALANCE X port?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
Where can you find information on the topic of PROFINET?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which devices support the "Power over Ethernet" (PoE) function?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
MIB (Management Information Base) for SNMP
Dependency of bus cycle times on switch times
S7-300 CPU 31x -- Product information -- Background and system information
How many devices can you connect to an S7-300/S7-400 using the Modbus/TCP protocol?
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
What is the emergency address (emergency IP) of a CPU and when is this enabled or disabled?
All-round protection with Industrial Security - System Integrity
What are the differences between OPEN MODBUS / TCP Redundant V1 and OPEN MODBUS / TCP Redundant V2?
What is the difference between "normal routing" and data record routing?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What should you watch out for when using the alarm numbering procedure?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
What is the maximum number of parameters that can be assigned to an FC and FB in the S7-300 CPU?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Why is only a warm start available for S7-300?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
Which entries deal with consistent data in conjunction with distributed I/O?
What properties, advantages and special features does the S7 Basis Communication offer?
What properties, advantages and special features does the global data communication offer?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which modules support the S7 routing function?
How can you obtain an overview of the memory concept of SIMATIC S7-300 CPUs and C7 devices?
Retentivity behavior of S7-300 CPU 31x and complete devices C7-6xx with MMC
Status of the run-time meter after overall reset
Why does the retentivity behavior of the S7-300 CPUs and C7 devices without MMC (Micro Memory Card) influence the contents of the variables?
Local data addressing with S7-300 / S7 400
S7 300 run-time meter doesn't give any value
S7-400 CPU 41x -- Product information -- Background and system information
How many devices can you connect to an S7-300/S7-400 using the Modbus/TCP protocol?
When compiling a CFC chart, why is the error message "Time stamp conflict" displayed in connection with the Modbus/TCP FBs for S7-400 CPUs?
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
All-round protection with Industrial Security - System Integrity
What are the differences between OPEN MODBUS / TCP Redundant V1 and OPEN MODBUS / TCP Redundant V2?
What is the difference between "normal routing" and data record routing?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What should you watch out for when adding components or changing their parameters using CiR (Configuration in Run)?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Behavior of the CPU after power off without back-up battery
I/O addressing with DP slaves
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
What is the difference between a restart (warm restart), cold restart and hot restart of a S7-400 CPU?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
What properties, advantages and special features does the S7 Basis Communication offer?
What properties, advantages and special features does the global data communication offer?
Which entries deal with consistent data in conjunction with distributed I/O?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which modules support the S7 routing function?
CPU does not work in RUN
What does "Correction factor" mean in the "Diagnostics/Clock" tab of the CPU's Properties dialog?
What is multicomputing mode and what are the differences to operating in the segmented subrack?
Differing information on the requirement of offline/ online memory
How can I get an overview of the S7-400 memory concept?
ET 200S (standard modules) -- Product information -- System description
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
Which modules of the Siemens portfolio support PROFIenergy functions?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which hardware and software components do you need to establish communication between SIMATIC S7 stations and third-party devices using the MODBUS RTU protocol?
Which memory cards are used in the interface modules in the ET 200 with CPU functionality?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Backing up the IM 151/CPU data on Micro Memory Card
What is the meaning of the terms "sinking" (German: "P-schaltend") and "sourcing" (German: "M-schaltend") in digital modules of SIMATIC?
ET 200pro -- Product information -- System description
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
Which labeling signs and lettering systems are available in IP65/IP67 for the distributed IO SIMATIC ET 200?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which connectors and cables can you order for the distributed IO systems ET 200eco, ET 200eco PN and ET 200pro?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
ET 200M (standard modules) -- Product information -- System description
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
Which accessories can you order for the distributed IO device ET 200M and for what do you need the accessories?
Which hardware and software components do you need to establish communication between SIMATIC S7 stations and third-party devices using the MODBUS RTU protocol?
How do you replace an IM153-2 FO?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
What degree of accuracy can you obtain for plant-wide and segment-wide time stamping?
NAMUR sensors on ET200 slaves
Starting up ET200-M with analog modules
Module failure with ET200-M
What do you need the Micro Memory Card (MMC) for in the ET 200M?
Time stamping of process signal changes with IM153-2BA00
Which manuals for ET 200M are available for downloading in A&D Product Support?
ET 200eco -- Product information -- System description
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
Which labeling signs and lettering systems are available in IP65/IP67 for the distributed IO SIMATIC ET 200?
Which connectors and cables can you order for the distributed IO systems ET 200eco, ET 200eco PN and ET 200pro?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
WinAC RTX -- Product information -- System description
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Which modules can you use when implementing software redundancy?
Which modules support the S7 routing function?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
WinAC RTX F -- Product information -- System description
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
Which IO controllers and IO devices support the following functions in STEP 7 V5.5: IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, I device, sochronous mode, System redundancy and Option handling?
Which modules support the S7 routing function?
Communications between WinAC RTX (with CP 5613) and OP
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
Network transitions and links (DP) -- Product information -- System description
What do the LEDs indicate on the standard repeater?
What is the difference between "normal routing" and data record routing?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What are the requirements for operating the DP/ASi-Link Advanced as DP master on a CP 443-5 Extended?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Which modules support the S7 routing function?
How do you set up the DP/PA link and how do you configure the DP/PA link and DP/PA coupler?
Unidirectional data transfer with the DP/DP coupler
Documentation for the DP/PA coupler in Dutch, Danish, Finnish, Swedish, Portuguese and Greek
ET 200SP -- Product information -- System description
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
Why is the menu item for starting S7-PCT in STEP 7 disabled in some IO Link master modules?
How do you load the 3D, CAx and ePLAN data for the SIMATIC products?
What is the meaning of the terms "sinking" (German: "P-schaltend") and "sourcing" (German: "M-schaltend") in digital modules of SIMATIC?
Which hardware and software components do you need to establish communication between SIMATIC S7 stations and third-party devices using the MODBUS RTU protocol?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
ET 200MP -- Product information -- System description
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, Isochronous mode, System redundancy and Option handling?
How do you load the 3D, CAx and ePLAN data for the SIMATIC products?
Which hardware and software components do you need to establish communication between SIMATIC S7 stations and third-party devices using the MODBUS RTU protocol?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Part number:

Configuration Notes
With the extended PROFINET diagnostics it is possible to have functions like the diagnostics and parameterization of integrated Ethernet interfaces (fiber-optic diagnostics and topology configuration, for example). The PROFINET IO devices that support extended PROFINET diagnostics are configured in the Hardware Configuration in STEP 7. They are available in the hardware catalog and have additional ports or interface modules as subslots in the module's slot. 

More information about PROFINET diagnostics and how to implement the PROFINET device module in SIMATIC is available in the manual "SIMATIC PROFINET with STEP 7 V12" in Entry ID 49948856.

Example
ET200S with extended PROFINET diagnostics


Fig. 01

The following IO controllers support the extended PROFINET diagnostics
 
Module Firmware Order number
PC CPs
CP1616 from V2.0 6GK1161-6AA00
CP1604 from V2.0 6GK1160-4AA00
SIMATIC NET PC software
SOFTNET PROFINET IO from V7.1
(Edition 2008)
6GK1704-1HW71-3AA0
Embedded and PC-based Automation
WinAC RTX 2008 V4.4 6ES7671-0RC06-0YA0
WinAC RTX (F) 2009 V4.5 6ES7671-0RC07-0YA0
6ES7671-1RC07-0YA0
WinAC RTX (F) 2010 V4.6 6ES7671-0RC08-0YA0
6ES7671-1RC08-0YA0
S7-mEC, EC31-RTX from V4.4 6ES7677-1DD00-0BB0
6ES7677-1DD10-0BB0
S7-400 CPUs
CPU412-2 PN from V6.0 6ES7412-2EK06-0AB0
CPU414-3 PN/DP from V5.0 6ES7414-3EM05-0AB0
CPU414-3 PN/DP from V6.0 6ES7414-3EM06-0AB0
CPU414F-3 PN/DP from V6.0 6ES7414-3FM06-0AB0
CPU416-3 PN/DP from V5.0 6ES7416-3ER05-0AB0
CPU416-3 PN/DP from V6.0 6ES7416-3ES06-0AB0
CPU416F-3 PN/DP from V5.0 6ES7416-3FR05-0AB0
CPU416F-3 PN/DP from V6.0 6ES7416-3FS06-0AB0
S7-300 CPUs
CPU315-2 PN/DP from V2.5 6ES7315-2EH13-0AB0
CPU315-2 PN/DP from V3.1 6ES7315-2EH14-0AB0
CPU315F-2PN/DP from V2.5 6ES7315-2FH13-0AB0
CPU315F-2PN/DP from V3.1 6ES7315-2FJ14-0AB0
CPU317-2 PN/DP from V2.5 6ES7317-2EK13-0AB0
CPU317-2 PN/DP from V3.1 6ES7317-2EK14-0AB0
CPU317F-2PN/DP from V2.5 6ES7317-2FK13-0AB0
CPU317F-2PN/DP from V3.1 6ES7317-2FK14-0AB0
CPU319-3 PN/DP from V2.5 6ES7318-3EL00-0AB0
CPU319-3 PN/DP from V3.2 6ES7318-3EL01-0AB0
CPU319F-3 PN/DP from V2.5 6ES7318-3FL00-0AB0
CPU319F-3 PN/DP from V3.2 6ES7318-3FL01-0AB0
S7-1500 CPUs
CPU1516-3 PN/DP from V1.0 6ES7516-3AN00-0AB0
CPU1513-1 PN from V1.0 6ES7513-1AL00-0AB0
CPU1511-1 PN from V1.0 6ES7511-1AK00-0AB0
S7-1200 CPUs
CPU 1211C from V1.0 6ES7211-1AD30-0XB0
6ES7211-1BD30-0XB0
6ES7211-1HD30-0XB0
  from V3.0 6ES7211-1AE31-0XB0
6ES7211-1BE31-0XB0
6ES7211-1HE31-0XB0
CPU 1212C from V1.0 6ES7212-1AD30-0XB0
6ES7212-1BD30-0XB0
6ES7212-1HD30-0XB0
  from V3.0 6ES7212-1AE31-0XB0
6ES7212-1BE31-0XB0
6ES7212-1HE31-0XB0
CPU 1214C from V1.0 6ES7214-1AE30-0XB0
6ES7214-1BE30-0XB0
6ES7214-1HE30-0XB0
  from V3.0 6ES7214-1AG31-0XB0
6ES7214-1BG31-0XB0
6ES7214-1HG31-0XB0
CPU 1215C from V3.0 6ES7215-1AG31-0XB0
6ES7215-1BG31-0XB0
6ES7215-1HG31-0XB0
Industrial Ethernet CPs
CP343-1 Standard from V2.2 6GK7343-1EX30-0XE0
CP343-1 Advanced from V1.0 6GK7343-1GX30-0XE0
CP343-1 Advanced from V3.0 6GK7343-1GX31-0XE0
CP443-1 Standard from V1.0 6GK7443-1EX20-0XE0
CP443-1 Standard from V3.0 6GK7443-1EX30-0XE0
CP443-1 Advanced from V2.0 6GK7443-1GX20-0XE0
CP443-1 Advanced from V3.0 6GK7443-1GX30-0XE0
ET 200S
IM151-8 PN/DP CPU from V2.7 6ES7151-8AB00-0AB0
IM151-8 PN/DP CPU from V3.2 6ES7151-8AB01-0AB0
IM151-8F PN/DP CPU from V2.7 6ES7151-8FB00-0AB0
IM151-8F PN/DP CPU from V3.2 6ES7151-8FB01-0AB0
ET 200pro
IM154-8 CPU from V2.5 6ES7154-8AB00-0AB0
IM154-8 CPU from V3.2 6ES7154-8AB01-0AB0
IM154-8F CPU from V3.2 6ES7154-8FB01-0AB0
IM154-8FX CPU from V3.2 6ES7154-8FX00-0AB0
Table 01

The following IO devices can use the extended PROFINET diagnostics:
 
Module Firmware Order number
PC CPs
CP1616 from V2.0 6GK1161-6AA00
CP1604 from V2.0 6GK1160-4AA00
S7-300 CPUs
CPU315-2 PN/DP from V3.2 6ES7315-2EH14-0AB0
CPU315F-2PN/DP from V3.2 6ES7315-2FJ14-0AB0
CPU317-2 PN/DP from V3.2 6ES7317-2EK14-0AB0
CPU317F-2PN/DP from V3.2 6ES7317-2FK14-0AB0
CPU319-3 PN/DP from V3.2 6ES7318-3EL01-0AB0
CPU319F-3 PN/DP from V3.2 6ES7318-3FL01-0AB0
S7-400 CPUs
CPU412-2 PN from V6.0 6ES7412-2EK06-0AB0
CPU414-3 PN/DP from V6.0 6ES7414-3EM06-0AB0
CPU414F-3 PN/DP from V6.0 6ES7414-3FM06-0AB0
CPU416-3 PN/DP from V6.0 6ES7416-3ES06-0AB0
CPU416F-3 PN/DP from V6.0 6ES7416-3FS06-0AB0
S7-1500 CPUs
CPU1516-3 PN/DP from V1.0 6ES7516-3AN00-0AB0
CPU1513-1 PN from V1.0 6ES7513-1AL00-0AB0
CPU1511-1 PN from V1.0 6ES7511-1AK00-0AB0
Industrial Ethernet CPs
CP343-1 Lean from V2.2 6GK7343-1CX10-0XE0
CP343-1 Standard from V2.2 6GK7343-1EX30-0XE0
CP343-1 Advanced from V1.0 6GK7343-1GX30-0XE0
CP343-1 Advanced from V3.0 6GK7343-1GX31-0XE0
ET 200S modules
IM151-3PN FO from V4.0 from 6ES7151-3BB21-0AB0
IM151-3PN ST from V4.0 from 6ES7151-3AA20-0AB0
IM151-3PN HF from V4.0 from 6ES7151-3BA20-0AB0
IM151-3PN HS from V1.0 from 6ES7151-3BA50-0AB0
IM151-8 PN/DP CPU from V3.2 6ES7151-8AB01-0AB0
IM151-8F PN/DP CPU from V3.2 6ES7151-8FB01-0AB0
ET 200M modules
IM153-4PN from V1.0 6ES7153-4AA00-0XB0
IM153-4PN from V2.0 6ES7153-4AA01-0XB0
ET 200pro modules
IM154-4PN HF from V2.0 from 6ES7154-4AB00-0AB0
IM154-8 CPU from V3.2 6ES7154-8AB01-0AB0
IM154-8F CPU from V3.2 6ES7154-8FB01-0AB0
IM154-8FX CPU from V3.2 6ES7154-8FX00-0AB0
ET 200eco PN from V6.0 6ES7141-6Bx00-0AB0
6ES7142-6Bx00-0AB0
6ES7142-6Bx50-0AB0
ET 200SP
IM155-6PN ST from V1.0 6ES7155-6AA00-0BN0
6ES7155-6AU00-0BN0
IM155-6PN HF from V2.0 6ES7155-6AA00-0CN0
6ES7155-6AU00-0CN0
ET 200MP
IM155-5PN ST from V1.0 6ES7155-5AA00-0AB0
Network components
PN/PN coupler from V1.0 6ES7158-3AD00-0XA0
SCALANCE X20x IRT products from V2.1 -
SCALANCE X200 products from V2.1 -
see Entry ID: 25472849
SCALANCE X300 products from V2.1 -
SCALANCE X414-3 E from V2.1.1 -
see Entry ID: 25355654
SCALANCE X408-2 from V2.0 -
SCALANCE X500 products from V3.0 -
Gateways
IE/AS Interface Link PN/IO from V2.0 Single AS-i master:
6GK1 411-2AB10

Double AS-i master:
6GK1 411-2AB20

Table 02

The PROFINET IO devices that support the extended PROFINET diagnostics can only be operated on PROFINET IO controllers that likewise support the extended PROFINET diagnostics.

There is a migration GSDML file for some of the PROFINET IO devices listed above for operating the PROFINET IO device on a PROFINET IO controller that does not yet support the extended PROFINET diagnostics.

Example
PN/PN coupler


Fig. 02

Note
The following applications provide a detailed description, including sample program, of the diagnostics options available in a PROFINET IO system.

  • "Diagnostic Methods for PROFINET Network Components (PROFINET IO, SNMP, WBM)" in Entry ID: 21566216
  • "PROFINET IO – Diagnostics Processing in the User Program"
    in Entry ID: 24000238

 Entry ID:23678970   Date:2013-07-22 
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
Topics
Help
Online Help
Guided Tour