show the entry list
PC/PG general -- Setting up systems -- Installing / setting up PC operating systems
How do you enable automatic logon with Microsoft Windows?
Which settings do you need to be able to use "Wake on LAN" on a SIMATIC IPC227D or IPC277D?
SIMATIC PG/PC does not revert to suspend mode after pcAnywhere installation 
Conflict between the internal interface for the memory card and the Ethernet card
Installing and managing partitions in Windows 2000
Changing the keyboard layout of the Windows logon mask
Creating a bootable system floppy disk for BIOS update
Definition of terms: FAT file system
BIOS password of PC forgotten
User with the name "Service" cannot be created
Rack PC -- Setting up systems -- Configuring systems
Why is a picture of the SIMATIC IPC not displayed when you access with the SIMATIC IPC Remote Manager by means of AMT?
Which slot do you have to configure when using the WinAC RTX 2010 with WinCC (TIA Portal)?
How do you enable automatic logon with Microsoft Windows?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How can you ensure operation of Windows 2000 with hard disks greater than 120 GB?
What can you do about the screen display sporadically freezing or the screen resolution switching to VGA mode with the Rack PC 840 V2?
Keyboard lock for WinCC Runtime with SIMATIC Rack PC IL 40 S and IL 40 S V2
Box PC -- Setting up systems -- Parameterizing systems
How do you configure the "Message Buffer Partition" with a SIMATIC IPC?
Why is a picture of the SIMATIC IPC not displayed when you access with the SIMATIC IPC Remote Manager by means of AMT?
Which slot do you have to configure when using the WinAC RTX 2010 with WinCC (TIA Portal)?
How do you enable automatic logon with Microsoft Windows?
Why does the installation of SQL Express 2005 on a SIMATIC IPC with embedded operating system abort?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How can you change the designation of the LAN interface in Windows so that the identification of the network interfaces matches between housing sticker and Windows (Box PC 627B and Box PC 827B)?
How can you ensure operation of Windows 2000 with hard disks greater than 120 GB?
Deactivation of fan monitoring in the SOM software
Computer crash when opening the diagnostics for the CP5611 in Windows 2000
Restart after installing MS Windows 98SE is not possible
Box PC 620 / Panel PC 670 - after installing a CP 1613 / CP 5611 Microsoft Win 2000 no longer starts or Windows shuts itself down
How can you avoid faults in the graphics display in Windows XP with the Box PC 840 V2?
Panel PC -- Setting up systems -- Configuring systems
How do you speed up the opening of the "Onscreen Keyboard" with SIMATIC IPCs?
How do you configure the "Message Buffer Partition" with a SIMATIC IPC?
How do you switch from landscape to portrait format with SIMATIC IPC277D?
Why is a picture of the SIMATIC IPC not displayed when you access with the SIMATIC IPC Remote Manager by means of AMT?
Which slot do you have to configure when using the WinAC RTX 2010 with WinCC (TIA Portal)?
How do you enable automatic logon with Microsoft Windows?
Why does the installation of SQL Express 2005 on a SIMATIC IPC with embedded operating system abort?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How can you ensure operation of Windows 2000 with hard disks greater than 120 GB?
How can I log in on a Windows 2000 computer without keyboard (e.g. Panel PC)?
Function "Change Operating Mode" with the parameter "Serial Transfer"
How can you implement Sm@rtAccess (HTTP communication) and Sm@rtServices (HTML pages) on a Panel PC 477B with WinCC flexible RT?
Changing the background lighting, the key code and triggering of function keys on the SIMATIC Panel PC 670/ 870 under WinNT
Restoring the touch functionality on the PC 670 after reinstalling the operating system
Softwaretools for SIMATIC Panel PCs 670 (with function keys)
Difficulties when Shutting Down Windows 98 Second Edition
Displayed Windows View turned by 180 degrees at IL70
Microsoft Windows 9x and memory extension of more than 512 MB
Field PG / Power PG -- Setting up systems -- Parameterizing systems
How do you enable automatic logon with Microsoft Windows?
How do you activate the Full Screen mode with STEP 5 on a Field PG running MS Windows operating systems?
How can you change the keyboard layout for STEP 5 to "QWERTY"?
Saving memory with parallel installation of Windows 9x / Windows ME or Windows NT / Windows 2000
Missing icons for network and dial-up connections in Windows 2000
How do you change the user interface language preinstalled in WinCC flexible on the Field PG M to a different language (German, French etc.)?
Why are the options "Standby mode" and "Power-down mode" not available in the "Power Schemes" tab of "Power Options Properties"?
Displayed size of the main memory during the boot procedure of Pentium IV Field or PowerPGs
How do you install Service Pack updates for Windows XP?
How do you install a more recent Service Pack for Windows 2000 MUI?
How do you switch the Windows XP MUI and the SIMATIC software to German after delivery of a Field PG?
WinCC -- Setting up development environments -- Parameterizing systems
How do you safely close WinCC by means of an external application?
How can you access WinCC stations remotely?
How do you reset the user interface of the WinCC Graphic Designer?
What should you watch out for when running SIMATIC WinCC or SIMATIC PCS 7 with Microsoft SQL Server 2005/2008 on PCs with multi-core or multiple processors?
How can you change the properties of the ToolTip text (font, font size, ...) in WinCC Runtime?
How do you enable automatic logon with Microsoft Windows?
WinCC: settings in the pcANYWHERE
Implementing WinCC V5.x on standalone computers (not applicable for V5.1 and higher) with Windows 2000
Symbol bars in the Graphics Designer can no longer be changed in size and location.
WinCC project information is not displayed correctly in the "WinCC Projects" folder in the Windows Explorer
Implementing WinCC V5.x on standalone computers (not applicable for V5.1 and higher) with Windows NT
How do you use the SIMATIC shell to configure the terminal bus of a WinCC station?
Why are WinCC pictures shown incorrectly or with margins in Runtime when using TFT and flat screens?
Which settings must you make in the WinCC-Explorer under "Computer > Properties" on each computer locally?
How can you make "lost" buttons visible again in the toolbar of the WinCC Explorer or the WinCC Graphics Designer?
Why after changing the resolution or installing a second monitor on my computer is the Properties dialog not displayed in the Graphics Designer?
WinCC (TIA Portal) -- Setting up development environments -- Installing / setting up operating systems
What settings must you make when installing a multiple station system in the SIMATIC WinCC Professional?
How do you do an "Operating system update" (OS update) or "Reset to factory settings" on operator panels?
How do you enable automatic logon with Microsoft Windows?
Why do other WinCC stations not appear in the network environment on the Windows 7 and Windows Server 2008 PCs?
Which SIMATIC software can you install in 64-bit operating systems?
How can you lock key combinations in WinCC V7.0 SP3 Update 3 and higher, and in WinCC (TIA Portal) with Windows 7 or Windows Server 2008?
How do you enable automatic logon with Microsoft Windows?
Part number:

Description
When a computer starts up (SIMATIC IPC, for example), you are asked which user name you want to use to log on to the system. This interrupts the automatic startup, which is undesirable, for example, after a power failure.

Validity
Microsoft Windows 2000
Microsoft Windows XP
Microsoft Windows Vista
Microsoft Windows 7
Microsoft Windows 8
Microsoft Windows XP Embedded
Microsoft Windows Embedded Standard 2009
Microsoft Windows Embedded Standard 7
Microsoft Windows Server 2003
Microsoft Windows Server 2008
Microsoft Windows Server 2012

Note
Refer to the versions of the Microsoft operating system released for your product in the Compatibility Tool here: Link.

Remedy
As a remedy we recommend you install automatic logon. Depending on whether your computer (SIMATIC IPC, for example) is member of a Windows working group or domain you have different options for installing automatic logon.

Automatic logon to a domain/working group using the Microsoft "Autologon for Windows" tool
To install automatic logon to a domain or working group we recommend you use the Microsoft "Autologon for Windows". The "Autologon for Windows" tool is available at this website:
http://technet.microsoft.com/en-us/sysinternals/bb963905.
The tool can be used with Microsoft Windows XP or Microsoft Windows Server 2003 onwards.

Automatic logon to a domain/working group using the Microsoft "Autologon for Windows" tool
If you wish to install automatic logon without an additional tool on your computer (SIMATIC IPC, for example), proceed as described in the table below.
 
No. Procedure
1

Open the "Run" dialog field with "Start > Run" or the key combination "Windows-Logo + R".

2

If you are using

  • Microsoft Windows 2000

you enter the command

"control userpasswords".

If you are using

  • Microsoft Windows XP

  • Microsoft Windows Vista

  • Microsoft Windows XP Embedded

  • Microsoft Windows Embedded Standard 2009

  • Microsoft Windows Embedded Standard 7

  • Microsoft Windows Server 2003

you enter the command

"control userpasswords2".

If you are using

  • Microsoft Windows 7

  • Microsoft Windows 8

  • Microsoft Windows Server 2008

  • Microsoft Windows Server 2012

you enter the command

"netplwiz.exe".


Fig. 01

Confirm your input by clicking the "OK" button. This opens the "User Accounts" dialog.

3

In the "User Accounts" dialog you open the "Users" tab.

Disable the "Users must enter a user name and password to use this computer" check box.


Fig. 02

Then click the "Apply" button. The "Automatically Log On" dialog window opens.

4

Note
If in a domain you cannot select "Users must enter a user name and password to use this computer", note the following.


Fig. 03

  • Close the "User Accounts" window.

5
  • Repeat steps 1 and 2 displayed in the table, then enter the "regedit.exe" command instead of "netplwiz.exe".


Fig. 04

  • In the "Registry Editor" window you open this Registry folder: "HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows NT\CurrentVersion\Winlogon\".

6
  • Right-click the Registry item "AutoAdminLogon" and then click "Modify...".


Fig. 05

7
  • Enter 1 in the "Value data:" field and then click "OK".


Fig. 06

Note
Restart the computer after this modification.

8

Note
If the Registry item "AutoAdminLogon" is not available, proceed as follows.

  • Right-click the Registry folder "Winlogon", then click "New" and then "String Value".


Fig. 07

9
  • Change the "String Value" to "AutoAdminLogon".


Fig. 08

  • Repeat steps 6 and 7 displayed in the table.

10

In the "Automatically Log On" dialog you specify the name and ID that is to be logged on automatically when the computer starts up.

Note
In a domain the following is to be entered as user name: "<Domain name>\user".


Fig. 09

Confirm your input by clicking the "OK" button.

11

Automatic Logon is now installed. After a restart or reboot of the computer (SIMATIC IPC, for example), the Windows logon is executed automatically and you can start using your application immediately.

Notes

  • The two passwords entered in the "Automatically Log On" window are checked for parity. However, the passwords are not checked for correctness. If two identical but incorrect passwords are preset, automatic logon does not work when you start the computer (SIMATIC IPC, for example).

  • You must disable the Enhanced Write Filter (EWF) before making changes in Microsoft Windows Embedded operating systems. See also Entry ID: 40108744.

  • If automatic logon is already configured, but you still want to make changes, then check the option check box "Users must enter a user name and password to use this computer" and then clear it again afterwards. Now you can click the "Accept" or "OK" button and the "Automatically Log On" window opens.

Important
This entry contains information for editing the registry. You should make a backup copy of the Registry before editing it. More information about making a backup copy, restoring and editing the Registry is available in the Microsoft Knowledge Base in Entry ID 256986. Incorrect use of the Registry editor can cause serious problems that affect the complete system and make it necessary to reinstall the operating system. You use the Registry editor at your own risk.

Additional Keywords
Auto, Start, User, Password, Logon, Login, 15390777

 Entry ID:23598260   Date:2014-11-17 
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
Topics
Help
Online Help
Guided Tour