show the entry list
Microbox -- Setting up systems -- Parameterizing systems
How do you configure the "Message Buffer Partition" with a SIMATIC IPC?
How do you configure WinAC RTX 2005 for implementation of a Microbox PC 420 with Windows XP Embedded?
How can you use the Teaming function in Windows XP to team two independent Gbit Ethernet interfaces?
How can you set up auto logon for SIMATIC IPCs?
How should I define the settings so as to ensure that my settings or programs that I have loaded are still available after restarting?
Rack PC -- Setting up systems -- Configuring systems
Why is a picture of the SIMATIC IPC not displayed when you access with the SIMATIC IPC Remote Manager by means of AMT?
Which slot do you have to configure when using the WinAC RTX 2010 with WinCC V11?
How can you set up auto logon for SIMATIC IPCs?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How can you ensure operation of Windows 2000 with hard disks greater than 120 GB?
What can you do about the screen display sporadically freezing or the screen resolution switching to VGA mode with the Rack PC 840 V2?
Keyboard lock for WinCC Runtime with SIMATIC Rack PC IL 40 S and IL 40 S V2
Box PC -- Setting up systems -- Parameterizing systems
Why is a picture of the SIMATIC IPC not displayed when you access with the SIMATIC IPC Remote Manager by means of AMT?
Which slot do you have to configure when using the WinAC RTX 2010 with WinCC V11?
How can you set up auto logon for SIMATIC IPCs?
Why does the installation of SQL Express 2005 on a SIMATIC IPC with embedded operating system abort?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How can you change the designation of the LAN interface in Windows so that the identification of the network interfaces matches between housing sticker and Windows (Box PC 627B and Box PC 827B)?
How can you ensure operation of Windows 2000 with hard disks greater than 120 GB?
Deactivation of fan monitoring in the SOM software
Computer crash when opening the diagnostics for the CP5611 in Windows 2000
Restart after installing MS Windows 98SE is not possible
Box PC 620 / Panel PC 670 - after installing a CP 1613 / CP 5611 Microsoft Win 2000 no longer starts or Windows shuts itself down
How can you avoid faults in the graphics display in Windows XP with the Box PC 840 V2?
Panel PC -- Setting up systems -- Configuring systems
How can you speed up the opening of the "Onscreen Keyboard" with SIMATIC IPC277D?
How do you configure the "Message Buffer Partition" with a SIMATIC IPC?
How do you switch from landscape to portrait format with SIMATIC IPC277D?
Why is a picture of the SIMATIC IPC not displayed when you access with the SIMATIC IPC Remote Manager by means of AMT?
Which slot do you have to configure when using the WinAC RTX 2010 with WinCC V11?
How can you set up auto logon for SIMATIC IPCs?
Why does the installation of SQL Express 2005 on a SIMATIC IPC with embedded operating system abort?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How can you ensure operation of Windows 2000 with hard disks greater than 120 GB?
How can I log in on a Windows 2000 computer without keyboard (e.g. Panel PC)?
Function "Change Operating Mode" with the parameter "Serial Transfer"
How can you implement Sm@rtAccess (HTTP communication) and Sm@rtServices (HTML pages) on a Panel PC 477B with WinCC flexible RT?
Changing the background lighting, the key code and triggering of function keys on the SIMATIC Panel PC 670/ 870 under WinNT
Restoring the touch functionality on the PC 670 after reinstalling the operating system
Which software tools are available for the SIMATIC Panel PCs 870 with function keys?
Softwaretools for SIMATIC Panel PCs 670 (with function keys)
Difficulties when Shutting Down Windows 98 Second Edition
Displayed Windows View turned by 180 degrees at IL70
Microsoft Windows 9x and memory extension of more than 512 MB
Field PG / Power PG -- Setting up systems -- Parameterizing systems
How can you set up auto logon for SIMATIC IPCs?
How do you activate the Full Screen mode with STEP 5 on a Field PG running MS Windows operating systems?
How can you change the keyboard layout for STEP 5 to "QWERTY"?
Saving memory with parallel installation of Windows 9x / Windows ME or Windows NT / Windows 2000
Missing icons for network and dial-up connections in Windows 2000
How do you change the user interface language preinstalled in WinCC flexible on the Field PG M to a different language (German, French etc.)?
Why are the options "Standby mode" and "Power-down mode" not available in the "Power Schemes" tab of "Power Options Properties"?
Displayed size of the main memory during the boot procedure of Pentium IV Field or PowerPGs
How do you install Service Pack updates for Windows XP?
How do you install a more recent Service Pack for Windows 2000 MUI?
How do you switch the Windows XP MUI and the SIMATIC software to German after delivery of a Field PG?
WinCC -- Setting up development environments -- Parameterizing systems
What should you watch out for when running SIMATIC WinCC or SIMATIC PCS 7 with Microsoft SQL Server 2005 on PCs with multi-core or multiple processors?
How can you change the properties of the ToolTip text (font, font size, ...) in WinCC Runtime?
How can you set up auto logon for SIMATIC IPCs?
WinCC: settings in the pcANYWHERE
Implementing WinCC V5.x on standalone computers (not applicable for V5.1 and higher) with Windows 2000
Symbol bars in the Graphics Designer can no longer be changed in size and location.
WinCC project information is not displayed correctly in the "WinCC Projects" folder in the Windows Explorer
Implementing WinCC V5.x on standalone computers (not applicable for V5.1 and higher) with Windows NT
How do you use the SIMATIC shell to configure the terminal bus of a WinCC station?
Why are WinCC pictures shown incorrectly or with margins in Runtime when using TFT and flat screens?
Which settings must you make in the WinCC-Explorer under "Computer > Properties" on each computer locally?
How can you make "lost" buttons visible again in the toolbar of the WinCC Explorer or the WinCC Graphics Designer?
Why after changing the resolution or installing a second monitor on my computer is the Properties dialog not displayed in the Graphics Designer?
OS - WinCC -- Creating HMI configurations -- Configuring User Administrator
How in PCS 7 can you prevent a user with "Monitor" rights from acknowledging messages?
How do user rights (authorizations) work in SIMATIC PCS 7 V7.1?
What is the standard password of the user "Administrator" in the WinCC User Administrator?
How can you set up auto logon for SIMATIC IPCs?
PCS 7 V6.0 / WinCC V6.0 operator right during Remote-access to Server
Executing actions depending on authorization level
Which setting options do I have when logging on with the chip-card reader (PCS 7 V4.x / V5.x)?
There are too many authorization levels in the User Administrator
Why doesn't the area-specific authorization work although it has been set in the User Administrator?
How can you realize login via chip card in PCS 7 with SIMATIC Logon?
How can you set up auto logon for SIMATIC IPCs?
Part number:

Instructions
When a SIMATIC IPC starts up, you are asked which user name you want to use to log on to the system. This interrupts the automatic startup, which is undesirable, for example, after a power failure. We recommend setting up auto logon as a remedy.

Setting up auto logon
The table below describes how to set up auto logon in various Windows operating systems on a SIMATIC IPC.
 
No. Procedure
1

In Windows XP you open the Run dialog via "Start > Run.
When using Windows 7, you open the Run dialog via "Start > All Programs > Accessories > Run"

2

Enter the "control userpasswords2" command in Windows XP / XP embedded / Windows embedded 2009 / Server 2003 / Vista or Windows 7.

In Microsoft Windows 2000, you use the "control userpasswords" command instead.


Fig. 01

Confirm with OK. The "User Accounts" dialog opens.

3

In the "Users" tab in the "User Accounts" dialog, you mark the relevant "User Name" (S_User, for example) and disable the function

  • "Users must enter a user name and password to use this computer".


Fig. 02

4

Then click the "Apply" button. The "Automatically Log On" dialog opens. Here you enter the password for the user name selected in the fields "Password:" and "Confirm Password:" and confirm with OK.

5

Click on "OK" to close the "User Accounts" dialog.

Auto logon has now been set up. After a restart or reboot of the SIMATIC IPC, the Windows logon is executed automatically and you can start using your application immediately.

Notes

  • You must disable the Enhanced Write Filter (EWF) before making changes in Windows embedded operating systems.

  • This method has the advantage that you avoid direct editing of the Windows Registry database and the password is stored in coded form.

  • The "Automatically Log On" window then opens only when you click on the "Apply" or "OK" button if the option check box "Users must enter a user name and password to use this computer" has been disabled just before.

  • If automatic logon is already configured, but you still want to make changes, then check the option check box "Users must enter a user name and password to use this computer" and then clear it again afterwards. Now you can click on the "Apply" or "OK" button and the "Automatically Log On" window opens.

  • The two passwords entered in the ""Automatically Log On" window are checked for parity. However, the passwords are not checked for validity. If two identical, but invalid passwords are preset, automatic logon does not work when you start the SIMATIC IPC.

  • The Auto-logon function is only available in Windows work groups. It is not possible to have automatic logon to a domain using the method described above.

  • In a SIMATIC IT environment you should make sure that in "Automatic Windows user logon" is checked in the management console under Settings --> System --> Security.

Keywords
Autostart, User password

 Entry ID:23598260   Date:2011-11-25 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour