show the entry list
S7-400 CPU 41x -- Configuring and programming communication -- Using communication blocks
What is the difference between the initialization and runtime parameters on the blocks for Modbus TCP?
Why is the status value A090 (hex) output for Modbus TCP although you have entered the correct license?
What are the differences between the licensed version and the downloadable demo version of the blocks for Modbus TCP?
Why is the value A083 (hex) output permanently at the STATUS output parameter of the block for Modbus TCP when the ENQ_ENR=true input parameter has been set?
Which blocks for Modbus TCP can you rename or re-wire when the block numbers of the Mode blocks are already being used in the user program?
How can you read out diagnostics data from a SIRIUS 3RK3 modular safety system using a S7-300/400 CPU?
Which communication options are there in SIMATIC S7?
How does data communication work between S7-300/S7- 400 and S7-200 via MPI using S7 basic communication?
Consistent data in S7-400, summary of mechanisms
Which ports are released for Modbus/TCP communication and how many Modbus clients can communicate with a SIMATIC S7 CPU as Modbus server?
How do you implement chronological messaging with S7-400 CPUs and WinCC?
How do you configure a specified and an unspecified S7 connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
How can you establish OPEN MODBUS / TCP communication from a SIMATIC S7 and where can you find further information?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What restrictions are there for active jobs when communicating with SFC 58 / SFC 59 and SFB 52 / SFB 53 via PROFIBUS DP and PROFINET IO?
How do you program the communication blocks FB63 "TSEND", FB64 "TRECV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange by way of the integrated PROFINET interface of a CPU or by way of the CP443-1 Advanced?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300 or S7-400 CPU?
How do you program the communication blocks FB67 "TUSEND", FB68 "TURCV", FB65 "TCON" and FB66 "TDISCON" in order to use the UDP protocol for data exchange by means of the integrated PROFINET interface of a CPU?
How can you access consistent data without SFC14/15 as part of the process image?
How great is data consistency in the PUT and GET S7 communication functions for the individual S7-400 CPUs?
How great is data consistency in the PUT and GET S7 communication functions for the individual S7-400 CPUs?
Part number:


Description:
In S7 communication with PUT and GET SFBs/FBs, data consistency is dependent on the individual servers (S7-400 CPU):
 
CPU Order no. Consistent data (bytes), max.
CPU 318-2DP 6ES7318-2AJ00-0AB0 1 Variable, max. 462 Byte
CPU 41x-1 6ES7412-1XF03-0AB0
CPU 41x-2 6ES7412-2XG00-0AB0
6ES7414-2XG03-0AB0
6ES7416-2XK02-0AB0
CPU 41x-3 6ES7414-3XJ00-0AB0
6ES7416-3XL00-0AB0
CPU 41x-4/H 6ES7417-4XL00-0AB0
6ES7414-4HJ00-0AB0
6ES7417-4HL01-0AB0
Table 1: Overview of the consistency ranges

Notes:

  • CPU 318-2DP behaves like a 41x series CPU.
  • The statements also apply to more recent order numbers:
    for example, for 6ES7412-2XG04-0AB0 instead of 6ES7412-2XG00-0AB0

You can find further information:

  • In the STEP 7 online help, 'Common parameters of the SFBs/FBs and of the SFC/FC for S7 communication')
  • In the "System software for S7-300/400 system and standard functions" manual, Entry ID 1214574:
    This contains a block-oriented overview of S7 communication and data consistency (Chap. 20). "Common parameters of the SFBs/FBs and of the SFC/FC for S7 communication" are described in Chap. 20.1.
     

 Entry ID:23522154   Date:2006-06-20 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour