show the entry list
S7-300 I/O Digital -- Product information -- Technical data
Which front connector do you need for S7-300 analog/digital modules and for S7-300 compact CPUs?
Collection and linking of documentation on digital input/output modules of SIMATIC S7 300 / ET 200M.
What should you pay attention to when selecting digital input modules if you want to control these with relay?
What is the meaning of the terms "sinking" (German: "P-schaltend") and "sourcing" (German: "M-schaltend") in digital modules of SIMATIC?
What is the meaning of the "Lamp load" specification in digital modules?
What is minimum voltage and minimum current required to ensure that the digital output module 6ES7322-1HF01-0AA0 switches through?
ET 200S (standard modules) -- Product information -- System description
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which hardware and software components do you need to establish communication between SIMATIC S7 stations and third-party devices using the MODBUS RTU protocol?
Which memory cards are used in the interface modules in the ET 200 with CPU functionality?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Which PROFINET nodes support automatic commissioning and the replace device without interchangeable medium function?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Backing up the IM 151/CPU data on Micro Memory Card
What is the meaning of the terms "sinking" (German: "P-schaltend") and "sourcing" (German: "M-schaltend") in digital modules of SIMATIC?
FM 350-1, 350-2, 450, SM338 -- Product information -- Technical data
What are the differences between the counter modules FM350-2, FM350-1 and ET200S1Count when determining measuring results?
What is the meaning of the terms "sinking" (German: "P-schaltend") and "sourcing" (German: "M-schaltend") in digital modules of SIMATIC?
FM 352-5 -- Product information -- Technical data
What is the meaning of the terms "sinking" (German: "P-schaltend") and "sourcing" (German: "M-schaltend") in digital modules of SIMATIC?
What is the meaning of the terms "sinking" (German: "P-schaltend") and "sourcing" (German: "M-schaltend") in digital modules of SIMATIC?
Part number:

Description:
There is a variety of terminologies for characterizing digital inputs and outputs,
e.g. "P-schaltend", "M-schaltend" (German) and "sinking", "sourcing" (English).

There are also assignment problems with

  • the logical status
  • the electrical signal
  • the wiring and switching

The two tables below show the relationship between terminology and assignment:

Digital inputs (24V)
 
Terminology Logical status Electrical signal

Switching

"P-lesend"

Sinking input

Switch is located between DC24V and the module

1 (true) 24V


Fig. 01

0 (false) 0V (or open)
"M-lesend"

Sourcing input

Switch is located between the module and ground

1 (true) 0V
Fig. 02
0 (false) 24V (or open)

Digital outputs (24V)
 
Terminology Logical status Electrical signal

Switching

"P-schaltend"

Sourcing output

PNP Transistor

Load located between the module and ground

1 (true) 24V


Fig. 03

0 (false) 0V (or open)
"M-schaltend"

Sinking output

NPN Transistor

Load located between DC24V and the module

1 (true) 0V
Fig. 04
0 (false) 24V (or open)

All S7-300, S7-400 and ET200S input modules and output modules are
"P-lesend" or "P-schaltend", except the modules listed in the table below.
 
SIMATIC S7-300 modules
6ES7 321-1BH50-0AB00 "M-lesend" inputs
6ES7 321-1BP00-0AB0 "P-lesend" or "M-lesend" inputs
6ES7 350-1AH03-0AB0 "P-lesend" or "M-lesend" encoder inputs
6ES7351-1AH02-0AE0 "P-lesend" or "M-lesend" encoder inputs
6ES7 322-1BP50-0AA0 "M-schaltend" outputs
6ES7 326-2BF40-0AB0 "P-schaltend" or "M-schaltend" inputs
6ES7 352-5AH00-0AE0 "M-schaltend" outputs
SIMATIC S7-400 modules
6ES7 421-7DH00-0AB0 "P-lesend" or "M-lesend" inputs
6ES7 450-1AP00-0AE0 "P-lesend" or "M-lesend" encoder inputs
SIMATIC ET200S modules
6ES7 131-4BD51-0AA0 "M-lesend" inputs
6ES7 131-4BF50-0AA0 "M-lesend" inputs
6ES7 138-4DA04-0AB0 "P-lesend" or "M-lesend" encoder inputs
6ES7 132-4BD50-0AA0 "M-schaltend" outputs
6ES7 132-4BF50-0AA0 "M-schaltend" outputs
6ES7 138-4FB02-0AB0 "P-schaltend" or "M-schaltend" inputs

 Entry ID:23451499   Date:2011-08-26 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour