show the entry list
WinCC -- Setting up development environments -- Installing and upgrading software
What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted?
Why do I receive errors during the upgrade installation to WinCC version V7.0 SP2?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC WinCC?
How can you switch the Microsoft SQL Server Management Studio Express to English on the bundle PC IPC 477C with WinCC V7.0 SP1?
Why does the installation of Microsoft SQL Server 2005 abort?
Why can't you install the SQL server from WinCC V6.2 or WinCC V6.2 SP2 after installing WinCC flexible 2008?
How do you install WinCC V7.0 on a MUI operating system if the language set in Windows is not English?
What can you do if installation of Security Patch KB929046 fails in the Windows Server 2003 R2 SP2?
Why is it not possible to activate the subcomponent "Common" while installing the "Microsoft Message Queuing" component?
How can you install WinCC while the computer is logged on to a domain?
Why does installation of the "Microsoft Message Queuing Services" abort with an error message?
What is the difference between an upgrade and an update?
How do you upgrade the WinCC Options V6.1?
How do you upgrade WinCC V6.0 to WinCC V6.0 SP3?
How do you migrate WinCC V4.x projects to WinCC V6.x and WinCC V7.x?
How can you regularly receive updates to the latest versions of WinCC?
Which settings do you have to make to set up a redundant single-user station in Microsoft Windows XP SP2?
How can you analyze errors when installing WinCC?
Why is the Setup of SIMATIC WinCC aborted at the ACE component (Active Communication Environment)?
How should you proceed if installation of the Microsoft SQL server fails?
Missing SQLUNIRL.dll when Installing SIMATIC WinCC V6
Why does the SQL server 2000 SP3 not appear as present during the installation of WinCC V6.0 SP3, even though it is installed?
What is the difference between an upgrade and an update?
Part number:

Configuration Notes:
An upgrade is an upgrade to a new version usually with additional functions. In this case one speaks of a new "major release". This upgrade package is usually billable and also includes a new license. An upgrade is from WinCC V5 to V6, for example.

An update is a further development within a program version (e.g. from WinCC V6.0 SP3 to SP4). Updates are always free of charge and provide no or only minor additional functions.

 Entry ID:23287238   Date:2006-05-15