show the entry list
SIMATIC NET SCALANCE S602 Industrial Security Component Released for Delivery
Part number:
Summary Internet document

The new SIMATIC NET SCALANCE S602 Industrial Security Component has been released for immediate delivery.

Internet document Summary
 

1. Product description

SCALANCE S602 is the basic version from the SCALANCE S family. It has the following features:

 ·        Stateful Inspection Firewall for access controll

·        Optional operation in Bridge or Router mode; It can thus be used directly on IP subnet boundaries

·       NAT or NAPT (Network Address and Port Translation) for the use of private IP addresses in an internal network, so that public IP addresses are saved

·        DHCP Server for devices in an internal (protected) network

·       Remote diagnostics via a protected channel with the SCALANCE S configuration tool; The evaluation of log files is supported by a connection to Syslog server

·        Global firewall rules can be assigned for simultaneous allocation to several  SCALANCE S devices

·       Symbolic names can be assigned to IP addresses for simple and quick configuration of the firewall.

 

2. Ordering data

  

Product Name

Order No.

SCALANCE S602

6GK5 602-0BA00-2AA3

  

Accessory:

Product Name

Order No.

C Plug

6GK1 900-0AB00

 

 

Here is your link to the Mall:

 

3. Application

The SCALANCE S602 Security Module permits protection of any devices in Ethernet networks. Subordinated networks are protected in accordance with the Industrial Security Concept. SCALANCE S is designed for mounting in switchboards.

 

4. Miscellaneous 

 

 

 Entry ID:23234996   Date:2006-05-08 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour