Instructions When generating module drivers, the following error message indicates that you are using blocks from a different library version to the one currently integrated: "Necessary files are missing for block CH_AI. Please note that you must install exactly that version of the library from which this block was imported."
Remedy Please refer to the detailed instructions for installing libraries in the manuals for the versions concerned. If you install according to these instructions, the above-mentioned error should no longer occur.
| Version |
Manual |
Chapter / Section |
Link |
| SIMATIC PCS 7 V6.0 |
"Software updates without using new functions (PCS 7 V5.x to V6.0)" |
4.2 |
Entry ID: 16518653 |
| SIMATIC PCS 7 V6.1 |
"Software updates without using new functions (PCS 7 V6.0 to V6.1)" |
3.5 |
Entry ID: 21407325 |
| SIMATIC PCS 7 V7.0 |
"PCS 7 V7.0 software updates without using new functions(PCS 7 V6.x to V7.0)" |
5.4 |
Entry ID: 24449025 |
| SIMATIC PCS 7 V7.0 SP1 |
"SIMATIC Process Control System PCS 7 V7.0 SP1 software updates without using new functions (PCS 7 V6.x to V7.0 SP1)" |
6.4 |
Entry ID: 27002507 |
| SIMATIC PCS 7 V7.1 |
"Software updates without using new functions (PCS 7 V6.x to V7.1)" |
5.3 |
Entry ID: 36191721 |
|