Instructions: Upon installation of WinCC different log files are created in the Windows directory, e.g. "C:\WINDOWS\". If installation problems occur, you can go through these log files to find error entries and thus determine a possible cause of the problem. Below is a list of some of the log files with path specifications.
Files up to and including WinCC V7.0:
| citamis.str |
C:\WINDOWS |
| HMI_*.log 1) |
C:\WINDOWS |
| HMI_*.TXT 2) |
C:\WINDOWS |
| RASetup*.LOG |
C:\ |
| WinCCInstallation.log |
C:\WINDOWS |
| sqlsp.log |
|
| sqlstp.log |
|
1) For example: HMI_CCInit_Master.log, HMI_WebNavigatorServer.log, HMI_WinCCSmartTools.log, HMI_RemotePublisher.log
2) For example: HMI_SC_ACE_LOG.TXT, HMI_SQLServerData.txt, HMI_SSC_ComArch_LOG.TXT
Files as from WinCC V7.0 SP1:
XP / 2003
| citamis.str |
C:\WINDOWS |
| HMI_SQLStarter.txt |
C:\Documents and Settings\All Users\Application Data\Siemens\Automation\Logfiles\Setup |
| RASetup*.LOG |
C:\ |
| WinCC_Configuration_Log.txt |
C:\WINDOWS |
| WinCC_Runtime_Log.txt |
C:\WINDOWS |
Vista:
| citamis.str |
C:\ProgramData\Siemens\Automation\Logfiles\Setup |
| HMI_SQLStarter.txt |
C:\ProgramData\Siemens\Automation\Logfiles\Setup |
| RASetup*.LOG |
C:\ProgramData\Siemens\Automation\Logfiles\Setup |
| WinCC_Configuration_Log.txt |
C:\ProgramData\Siemens\Automation\Logfiles\Setup |
| WinCC_Runtime_Log.txt |
C:\ProgramData\Siemens\Automation\Logfiles\Setup |
Note: You can quickly find the error entries by using specific full-text searches, e.g. a search for the character string "ERROR". Taking the time stamp, you can compare the entries with any entries in the Windows event display and thus establish further connections.
|