|
Lifting of the Delivery Stop for the Panel Options based on WinCC flexible 2005:
In the article with the ID 22926459 you were informed about the delivery stop affecting the WinCC flexible options SIMATIC WinCC flexible /Sm@rtAccess for SIMATIC Panels as well as WinCC flexible /Sm@rtService for SIMATIC Panels.
With the delivery release of WinCC flexible 2005 SP1 (article ID: 22927119), the delivery stop is being lifted effective immediately.
The products with the following order numbers are available for delivery again effective immediately:
Panel Options based on WinCC flexible 2005:
| WinCC flexible /Sm@rtAccess for SIMATIC Panels |
6AV6 618-7AB01-1AB0 |
| WinCC flexible /Sm@rtService for SIMATIC Panels |
6AV6 618-7BB01-1AB0 |
Note:
Both Panel options may only be used in connection with WinCC flexible 2005 SP1 following the scenarios formulated in the article with the ID 22926459. Please observe the following product information, which is also enclosed with the options.
Product Information.pdf ( 416 KB )
Discontinuation of the Panel Options based on WinCC flexible 2004 and WinCC flexible 2004 SP1:
The cause of the delivery stop was corrected with WinCC flexible 2005 SP1. The affected runtime options on the basis of WinCC flexible 2004 may no longer be used under the scenarios formulated in the article with the ID 22926459, or an upgrade to WinCC flexible 2005 SP1 has to be made.
The products with the following order numbers are therefore discontinued starting 05/01/2006.
Panel Options based on WinCC flexible 2004:
| WinCC flexible /Sm@rtAccess for SIMATIC Panels |
6AV6 618-7AB01-0AB0 |
| WinCC flexible /Sm@rtService for SIMATIC Panels |
6AV6 618-7BB01-0AB0 |
|