show the entry list

FM 350-1, 350-2, 450, SM338 -- Product information -- Determining performance and quantity frameworks 
Which modules can you use when implementing software redundancy? 
FM350-1: changing the updating time in measuring modes 

Which modules can you use when implementing software redundancy?Go to beginning
Part number:

Description
Software Redundancy (SWR) is a software package for configuring fault-tolerant controllers with standard components. The controller part consists of standard CPUs of the S7-300 and S7-400 series. The redundancy link for synchronizing the redundant CPUs is achieved with standard communication mechanisms like CPs or via an MPI interface. Connection to I/O devices is via two redundant PROFIBUS DP segments to the ET-200M stations with redundant IM 153-2 interface modules. You can also implement Software Redundancy on WinAC RTX as from version 2008.

Note
More information is available in the function manual "Software Redundancy for SIMATIC S7" in Entry ID 1137637.

The following table lists modules that support software redundancy. The lowercase letter x is a wildcard character in the order numbers.

S7-300 CPUs
 
Module Order number
CPU 313C-2 DP 6ES7313-6CE0x-0AB0
6ES7313-6CF03-0AB0
6ES7313-6CG04-0AB0
CPU 314C-2 DP 6ES7314-6CF0x-0AB0
6ES7314-6CG0x-0AB0
6ES7314-6EH04-0AB0
CPU 315-2 DP 6ES7315-2AFxx-0AB0
6ES7315-2AG10-0AB0
6ES7315-2AH14-0AB0
CPU 315F-2 DP 6ES7315-6FF0x-0AB0
CPU 315-2 PN/DP 6ES7315-2EG10-0AB0
6ES7315-2EH1x-0AB0
CPU 315F-2 PN/DP 6ES7315-2FH1x-0AB0
6ES7315-2FJ14-0AB0
CPU 315T-2 DP 6ES7315-6Tx1x-0AB0
CPU 316-2 DP 6ES7316-2AG0x-0AB0
CPU 317-2 DP 6ES7317-2AJ10-0AB0
6ES7317-2AK14-0AB0
CPU 317F-2 DP 6ES7317-6FF0x-0AB0
CPU 317-2 PN/DP 6ES7317-2Ex1x-0AB0
CPU 317F-2 PN/DP 6ES7317-2Fx1x-0AB0
CPU 317T-2 DP 6ES7317-6Tx1x-0AB0
CPU 318-2 DP 6ES7318-2AJ0x-0AB0
CPU 319-3 PN/DP 6ES7318-3EL0x-0AB0
CPU 319F-3 PN/DP 6ES7318-3FL0x-0AB0
Table 01

S7-400 CPUs
 
Module Order number
CPU 412-1 6ES7412-1XF0x-0AB0
6ES7412-1XJ05-0AB0
CPU 412-2 PN 6ES7412-2EK06-0AB0
CPU 412-2 6ES7412-2XG0x-0AB0
6ES7412-2XJ05-0AB0
CPU 413-1 6ES7413-1XG0x-0AB0
CPU 413-2 6ES7413-2XG0x-0AB0
CPU 414-1 6ES7414-1XG0x-0AB0
CPU 414-2 6ES7414-2XG0x-0AB0
6ES7414-2XJ0x-0AB0
6ES7414-2XK05-0AB0
CPU 414-3 6ES7414-3XJ0x-0AB0
6ES7414-3XM05-0AB0
CPU 414-3 PN/DP 6ES7414-3EM05-0AB0
6ES7414-3EM06-0AB0
CPU 414F-3 PN/DP 6ES7414-3FM06-0AB0
CPU 416-1 6ES7416-1XJ0x-0AB0
CPU 416-2 6ES7416-2XK0x-0AB0
6ES7416-2XL0x-0AB0
6ES7416-2XN05-0AB0
CPU 416F-2 6ES7416-2FN05-0AB0
CPU 416-3 6ES7416-3XL0x-0AB0
6ES7416-3XR05-0AB0
CPU 416-3 PN/DP 6ES7416-3ES06-0AB0
6ES7416-3ER05-0AB0
CPU 416F-3 PN/DP 6ES7416-3FR05-0AB0
6ES7416-3FR06-0AB0
CPU 417-4 6ES7417-4XL0x-0AB0
6ES7417-4XT05-0AB0
Table 02

Note
The SIMATIC S7-300/400 F-CPUs are to be used here without F program.

Communication modules with DP master function
 
Module Order number
CP 443-5 EXT
(connection to PROFIBUS network)
6GK7443-5DX04-0XE0
6GK7443-5DX05-0XE0
IM 467 and IM 467-FO
(can only be used in version V1.1)
6ES7467-5GJ0x-0AB0
6ES7467-5FJ00-0AB0
Table 03

Communication modules for linking the stations
 
Module Order number
CP 342-5 6GK7342-5DA00-0XE0
6GK7342-5DA02-0XE0
6GK7342-5DA03-0XE0
CP 343-1 6GK7343-1BA00-0XE0
6GK7343-1EX11-0XE0
6GK7343-1EX30-0XE0
6GK7343-1GX30-0XE0
CP 343-1 LEAN
(connection to Industrial Ethernet)
6GK7343-1CX10-0XE0
CP 443-5 EXT
(connection to PROFIBUS network)
6GK7443-5DX04-0XE0
6GK7443-5DX05-0XE0
CP 443-1 ISO1
(connection to Industrial Ethernet)
6GK7443-1EXxx-0XE0
6GK7443-1GXxx-0XE0
6GK7443-1BXxx-0XE0
Table 04

Modules for distributed I/O device ET 200M
 
Module Order number
IM 153-2 6ES7153-2BA0x-0XB0 as from release 2
(bus module 6ES7195-7HD10-0XA0)
FM 350-1 6ES7350-1AH0x-0AE0
CP 341
(20 mA TTY, RS232, RS422/485)
6ES7341-1xH01-0AE0
6ES7341-1xH02-0AE0
CP 341
(RS232C)
6ES7341-1AH02-0AE0
All digital and analog modules for ET 200M (see Catalog ST70)
Table 05

PC-based controller
 
Module Order number
Windows Logic Controller WinAC RTX F V4 6ES7611-4FB00-0YB7
You cannot order this MLFB separately but only as part of the products below.
  • WinAC RTX F as from version 2009 (6ES7 671-1RC0x-0YA0)
  • SIMATIC IPC427 Bundles (6ES7 675-1D...)
  • SIMATIC HMI IPC477C Bundles(6AV7 884-...)
Windows Logic Controller WinAC RTX V4 6ES7611-4SB00-0YB7
You cannot order this MLFB separately but only as part of the products below.
  • WinAC RTX as from version 4 (6ES7 671-0RC0x-0YA0)
  • Microbox 420-RTX (6ES7 675-1B...)
  • Microbox 427B Bundles (6ES7 675-1C...)
  • IPC427C Bundles (6ES7 675-1D...)
  • Panel PC 477 HMI/RTX (6AV7 84...)
  • Panel PC 477B Bundles (6AV7 85...)
  • HMI IPC477C Bundles (6AV7 884...)
Embedded Controller, EC31 6ES7677-1DD00-0BA0
6ES7677-1DD10-0BA0
Embedded Controller, EC31-RTX 6ES7677-1DD00-0BB0
6ES7677-1DD10-0BB0
Embedded Controller, EC31 HMI/RTX 6ES7677-1DD00-0BF0
6ES7677-1DD00-0BG0
6ES7677-1DD00-0BH0
6ES7677-1DD10-0BF0
6ES7677-1DD10-0BG0
6ES7677-1DD10-0BH0
Embedded Controller, EC31-RTX F 6ES7677-1FD00-0FB0
6ES7677-1FD10-0FB0
Table 06  

Note
The ET 200M stations must always be configured with active bus modules (6ES7195-7HB00-0XA0 or 6ES7195-7HC00-0XA0), even if the "Hot swapping of I/O modules" function is not possible with S7-300 CPUs.

FM350-1: changing the updating time in measuring modesGo to beginning
Part number:

QUESTION:  
How can I change the updating time in the measuring modes with an FM350-1?

ANSWER:  

Determining the updating time:

  • The updating time in synchronous mode with a PROFIBUS DP cycle ( TDP) of TDP < 10ms is n*TDP. You obtain the factor n via the following formula:

    n = 10ms/TDP[ms] + 1

    The digits after the decimal point are dropped after division.

    Example:
    TDP= 6ms and n = 2  results in an updating time of 12ms.

    The updating time in synchronous mode with a PROFIBUS DP cycle ( TDP) of TDP>=10ms is n*TDP  with nmin = 1.
  • The updating time in synchronous mode is n*10ms  with nmin = 1.

Entering the value determined in the DB:

You must enter the factor n in the DB for FC CNT_CTL1. The address 22 is parameterized in the WORD format, address 24 has the value zero.

Data type

Data block

BYTE 22 23 24 25
WORD 22
Factor n
 
24
---

More information on this module is available in the manual "SIMATIC FM 350-1 Function Module", section 8.4, in Entry ID: 1086726.


 Entry ID:23004410   Date:2012-09-03 
I regard this article....as helpfulas not helpful                                 






























related links
What are the requirements for usi ...
What is multicomputing mode and w ...
Manual Part B8 CP 343-1 Lean
Manual Part B3A CP 343-1 Advanced
How many communication instances ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour