show the entry list
New JAVA S7 Beans Library V.2.5.5 for Advanced CPs and IT CPs
Part number:
Summary Internet document

The updated version 2.5.5 of the JAVA S7 Beans class library is now available for downloading. It enables the creation of customized JAVA-based Web applications for SIMATIC NET communication processors.

 

Internet document Summary
 

 

In contrast to ready-made JAVA applets, that can only be included and parametrized in HTML pages, the JAVA beans permit the creation of customized applets.

The required JAVA class library version 2.5.5 features the following improvements:

·         Optimized use of the parameterization screenforms of the Borland Tools JBuilder

·         Size indication and label entry available for graphical representation of the "CLState3LED" and "CLStateLED" beans.

 

The beans have been tested with the following development tools:

·         JBuilder 7 Enterprise

·         JBuilder X Enterprise

·         JBuilder 2005 Enterprise

·         JBuilder 2006 Enterprise
 

The following browsers were tested:

·         MS Internet Explorer V6

·         Mozilla Firefox 1.0.7

·         Mozilla Firefox 1.5

 

The JAVA S7 beans library can be used for the following CPs:

·         CP 243-1IT

·         CP343-1IT

·         CP343-1Advanced

·         CP443-1IT

·         CP443-1Advanced

The library can be downloaded from entry ID 22964892

More information on the use of the JAVA beans library is available from the user manual "S7Beans / Applets for IT CPs" http://support.automation.siemens.com/WW/view/de/22260159

 

The file system V2.5.5 of the CP443-1Advanced, that is also available for downloading, already contains the the above JAVA S7 beans class library V2.5.5.
 

 

 Entry ID:22964982   Date:2006-04-20 
I regard this article....as helpfulas not helpful                                 
related links
Download of the JAVA S7 Beans Lib ...
MOBIC T8: running Java applications
Why don´t regulary work function ...
Web-Based Access to Process Varia ...
VS130-2 CAT Client
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour