|
Description: As from PCS 7 V6.0 SP3 you have the functionality that the acknowledging operator is entered in the operator message.
In order to be able to use this functionality after upgrading from PCS 7 V6.0 SP2, the OS project editor must be run once with the option "Complete configuration (loss of online delta load capability)".
Proceed as follows.
| No. |
Procedure |
| 1 |
Open the OS project editor in the WinCC Explorer. |
| 2 |
In the "General -> Activities when processed by project editor ...." tab you activate "Complete configuration (loss of support for online Delta Loading)". |
| 3 |
Click "OK" to close the OS project editor. |
This adapts the existing operator messages to the new functionality.
These instructions have been verified with PCS 7 V6.0 SP3.
|