show the entry list

S7-300 I/O Digital -- Setting up and parameterizing hardware -- Connecting and wiring modules 
Which 24V digital input modules need a power supply and to which pins must the power supply be connected? 
When do the digital outputs of modules 6ES7 322-1BL00-0AA0 and 6ES7 322-1BH..1-0AA0 have to be protected in addition? 
What should you watch out for when operating the digital output module 6ES7322-1HH01-0AA0 with a load voltage of 24V AC? 
What should you watch out for when replacing the digital output module 6ES7322-1HH00-0AA0 with the digital output module 6ES7 322-1HH01-0AA0? 
How do you connect a contactor with 24V AC to an SM 322 (MLFB 6ES7 322-1EL00-0AA0)? 

Which 24V digital input modules need a power supply and to which pins must the power supply be connected?Go to beginning
Part number:

Description
The table below shows the pins of the S7-300 24V digital input modules that need a power supply connections. It also shows the pins of the S7-300 24V digital input modules to which the power supply connections (L+ / M) are to be connected. The S7-300 digital input modules not listed do not need an external power supply.
 
Module

Power supply connections

L+

M

6ES7 321-1BH00-0AA0

Pin 1

Pin 20

6ES7 321-1BH01-0AA0 Pin 1 Pin 20
6ES7 321-1BH02-0AA0 --- Pin 20
6ES7 321-1BH81-0AA0 Pin 1 Pin 20
6ES7 321-7BH00-0AB0 Pin 1 Pin 20
6ES7 321-7BH01-0AB0 Pin 1 Pin 20
6ES7 321-7BH80-0AB0 Pin 1 Pin 20
6ES7 321-1BH50-0AA0 Pin 1 ---
6ES7 321-1BH02-0AA0 --- Pin 20
6ES7 321-1BH10-0AA0 --- Pin 20
6ES7 321-1BL00-0AB0 --- Pin 20
6ES7 321-1BL80-0AB0 --- Pin 40
6ES7326-1BK00-0AB0 Pin 1
Pin 21
 Pin 2
Pin 22
6ES7326-1BK01-0AB0 Pin 1
Pin 21
 Pin 2
Pin 22
6ES7326-1BK02-0AB0 Pin 1
Pin 21
 Pin 2
Pin 22
6ES7326-1RF00-0AB0 Pin 21 Pin 22
Table 1: Pin assignments of the power supply connections

Note
More information is available in the manual "S7-300 Module Data" in Entry ID: 8859629 and "SIMATIC Automation System S7-300 ET 200M Distributed I/O Device Fail-safe signal modules" in Entry ID: 19026151 .

Keywords
Signal modules

When do the digital outputs of modules 6ES7 322-1BL00-0AA0 and 6ES7 322-1BH..1-0AA0 have to be protected in addition?Go to beginning
Part number:

Description
If an additional manual operation or a manual switching on of the connected actuator is intended in parallel to the digital outputs of modules 6ES7 322-1BL00-0AA0 and 6ES7 322-1BH..1-0AA0, a blocking diode has to be connected in series to the output of the module. This blocking diode prevents regenerative feedback into the module and protects it against destruction.
The let-through current of the diode must be at least as high as the nominal current of the outputs.

Note
The digital outputs of these modules are not protected against reverse voltage. Configuration without this blocking diode might lead to regenerative feedback of the plant.

What should you watch out for when operating the digital output module 6ES7322-1HH01-0AA0 with a load voltage of 24V AC?Go to beginning
Part number:

Description
The digital output module 6ES7322-1HH01-0AA0 can also be operated with a load voltage of 24V AC. In this case, you must pay attention to the switching duration. Switching duration:

  • Ohmic load, 24 V AC at 1.5 A: typically 1.5 million switching cycles
  • Inductive load, 24 V AC, 1.5 A: typically 1.0 million switching cycles

What should you watch out for when replacing the digital output module 6ES7322-1HH00-0AA0 with the digital output module 6ES7 322-1HH01-0AA0?Go to beginning
Part number:

Description
Please remove the locking elements in the front connector if you want to use the front connector of the 6ES7322-1HH00-0AA0 as the front connector for successor module 6ES7322-1HH01-0AA0. These light gray coding elements prevent you inadvertently plugging in a front connector on a different module (Fig. 1) and must be removed in this case.


Fig. 1: Locking elements - back of connector

Use a screwdriver to press the elements out backwards:


Fig. 2: Front of connector

Note
Since the digital output module 6ES7322-1HH01-0AA0 can be used up to a rated voltage of 230V AC, it needs to be locked against use with the older digital output module 6ES7322-1HH00-0AA0, because this can only be used up to a rated voltage of 120V AC.

How do you connect a contactor with 24V AC to an SM 322 (MLFB 6ES7 322-1EL00-0AA0)?Go to beginning
Part number:

Instructions:
It is not possible to connect contactors with 24V AC to this module. A voltage of 24V AC is not sufficient of the sensor to recognize a blown fuse. The minimum load voltage for this module is 120V AC minus 20%.

Note: 
24V AC contactors can be connector to module 6ES7 322-5GH00-0AB0. This module is designed for load voltages of up to 48V AC/DC and does not need a minimum load voltage.


 Entry ID:22950349   Date:2011-09-26