show the entry list
ProTool -- Creating HMI configurations -- Creating pictures
Configuring headers of OP3 pictures in ProTool V5.2 /SP2
Programming the "Set_Bit" function by pressing a button on Windows-based devices
Picture change on the TP170A as tag function
CPU functions for S7-300 with OP7/OP17
Entering an S5TIME" variable in ProTool/Pro to provide values for a timer in the SIMATIC controller
Showing an "S5TIME" variable from a SIMATIC logic control with ProTool/Pro
Configuring the TAB order ProTool
Subsequent insertion of pictures in the configuration
Graying in the OP display of bitmap graphics
Description of the default name "PIC_xx" for a ProTool/Pro screen
Can I also program function keys in the message image?
Special characters and language-specific characters
How can you register unknown ActiveX objects on a PC and then incorporate them in ProTool/Pro?
Settings required for implementation of the ProTool function "Start Program"
Display of help texts for a certain image object on a Touch Panel
How can you start specific items in the Control Panel directly from the Runtime on an operator panel?
How do you implement the "Clean Screen" function for cleaning the touch screen on Mobile Panel 170?
How do you configure screen selection on a line or graphics operator panel via controller job 51?
How do you configure screen selection on a Windows-based operator panel via controller job 51?
How can you make a screen selection on an OP3 via the controller?
How can you make a screen selection on a Windows-based operator panel via the controller without using a controller job?
How can you make a screen selection on a Windows-based operator panel by entering a screen number?
How can the display for the danger and warning area of an analog display be made in color?
How can you optimize the response time when changing screens via the controller?
How do you monitor and control tags on panels on which the status/control object is not available?
How can the display for the danger and warning area of an analog display be made in color?
Part number:

Instructions:
At the moment it is not possible to have the display for the normal, danger and warning area made in color on a Windows CE-based operator panel.

However you can do this manually by using a graphical representation laid behind an analog display that is switched to transparent.
 
No. Procedure
1

Insert analog display:

First insert an XGauge Control in your configuration and define the size of the display.

Tip:
You can define the height and width of the display in the Properties under XGauge Control > Position > Size. 

2

Set parameters:

In the Properties of the display under "General" you define the relevant parameters for the SMark Width, Danger, Warning etc.

Under "Labeling" you select the "Display" (Danger Display, Warning Display, Normal Display) that is to be displayed later on the analog display.

3 Create screen shot:

Make a "screen shot" of the picture/page with the analog display (e.g. via the key combination Ctrl + Print).

Insert this screen shot in a graphics processing program (e.g. Microsoft Paint).

4 Edit screen shot:

From the screen shot you remove all the details such as labels and scales. Below is an example of the original and the edited screen shot.

Original 


Fig. 01

Edited


Fig. 02

 5 Incorporate graphical representation:
  • First open the Properties of the analog display.
    Under "General > Back Style:" you select the "Transparent" entry.
  • Switch to the "Labeling" menu item. There you clear the check marks for the Danger, Warning and Normal displays.
  • Insert a new graphical representation. In this case you use the screen shot you have edited as the graphical representation.
  • Place the two elements one over the other (analog display and graphical representation). The analog display must be set to "Foreground".

This completes the analog display.

6 Overview:


Fig. 03

Runnability and test environment:
The following table lists the components that have been used to create this entry and verify the functions described.
 
Component Product and version
PC operating system Microsoft Windows XP SP2
Standard Tools -
Engineering Tools -
HMI Software ProTool V6.0 SP3
HMI devices MP370 Touch 12"
Controllers -
Table 1: Creation environment of the download attached

The attached download contains the archived ProTool project with the example described above.

  Attachment 1: Project_1 ( 15 KB )

 Entry ID:22832504   Date:2006-05-09 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour