show the entry list

ET 200S (standard modules) -- Product information -- Technical data  
What are the requirements for using the S7 routing function and which modules can you implement? 
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet? 
Which PROFIBUS connectors can you use in Zone 1 or 2? 
What are the system limits in an F CPU for safe bidirectional data communication via S7 Communication? 
Which SIMATIC S7 components and which drives support clock-synchronicity functionality? 
ET 200S: Are there special requirements for ET200S when mounted on sheet metal plates? 
ET200S: How many motor starters can be allocated to a power module? 
ET 200S: How many motor starters can be allocated to a power module? 
ET 200S: How many load feeders may be connected? 
Calculating the maximum absolute error of the counter module 1Count24V/100kHz (6ES7 138-4DA02-0AB0) when measuring rotational speed  
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas 
Baud rates for ET200S FO modules 
Maximum power load for digital output modules 
Minimum distance to the ET 200S front 
How do you assign and identify thermocouples? 
How long does the input signal have to be present before an analog input module identifies this signal as a process alarm? 

What are the requirements for using the S7 routing function and which modules can you implement?Go to beginning
Part number:

Description
From STEP 7 V5.0 SP3 HF3 onwards you can reach ST stations online over and beyond subnet limits with the PG/PC, in order, for example, to load user programs or a hardware configuration or in order to execute test and diagnostic functions. You can connect a PG/PC at any place within the network and connect online to any stations which are reached through gateways.

Gateway
The gateway from a subnet to one or more other subnets is in a SIMATIC station that has interfaces to the subnets concerned.

Requirements

  • At least STEP 7 V5.0 SP3 HF3 is installed on the PG/PC for configuration and use of the S7 routing function.
  • An interface (Industrial Ethernet or PROFIBUS PC CP) is installed in the PG/PC to establish a connection to the gateway. You can use PROFIBUS PC CPs 55xx and 56xx. You can use any NDIS-compatible Ethernet network card (3COM, CP1613, for example) as Industrial Ethernet interface in the PG/PC.
  • The associated communications modules of the station support the S7 routing function.
  • The network configuration does not go across project boundaries.
  • Both the modules and the PG or PC are loaded with the configuration information that contains the latest "knowledge" about the complete network configuration of the project.
    Technical background
    All the modules associated with the gateway must receive information about which subnets can be reached over which routes (= routing information).

Note
The lists below have been updated with the modules of the hardware catalog of STEP 7 V5.4 SP2. This means that older modules which support the S7 routing function are listed in the tables, but are not necessarily included in the hardware catalog of the latest versions of STEP 7.

SIMATIC S7-CPUs
The list below gives an overview of the SIMATIC S7 CPUs that support the S7 Routing function.

584459_Overview_CPUs_en.pdf ( 43 KB )

Communications processors (CPs)
The list below gives an overview of the PROFIBUS and Industrial Ethernet CPs that support the S7 Routing function.

584459_Overview_CPs_en.pdf ( 41 KB )

SIMATIC S7 FM modules
The list below gives an overview of the SIMATIC S7 FM modules that support the S7 Routing function.
 

FM

Version

Order number

FM 356-4 V5.0 V5.0 6ES7356-4BM00-0AE0
FM 356-4 V5.0 V5.0 6ES7356-4BN00-0AE0
FM 456-2 V5.0 6ES7456-2AA00-0AB0
Table 01

Gateways
The list below gives an overview of the gateways that support the S7 Routing function.
 

Link

Version

Order number

IE/PB Link as from V1.0 6GK1411-5AA00
IE/PB Link PNIO as from V1.0 6GK1411-5AB00
IWLAN/PB Link PNIO as from V1.1 6GK1417-5AB00
IWLAN/PB Link PNIO as from V1.1 6GK1417-5AB01
Table 02

SIMATIC S7 IM modules
The list below gives an overview of the SIMATIC S7 IM modules that support the S7 Routing function.
 

IM

Version

Order number

IM 467 as of V2.0 6ES7467-5GJ02-0AB0
IM 467 FO as of V2.0 6ES7467-5FJ00-0AB0
Table 03

SIMATIC WinAC RTX, WinAC Slot and WinAC MP
The list below gives an overview of SIMATIC WinAC RTX, WinAC Slot and WinAC MP that support the S7 Routing function.
 
WinAC Version Order number
WinAC RTX as from V4.0 6ES7671-0R...
WinAC Slot 412 as from V3.2 6ES7673-2C...
WinAC Slot 416 as from V3.2 6ES7673-6C...
WinAC MP as from V4.1 6ES7671-4EE00-0YA0
6ES7671-5EF01-0YA0
6ES7671-7EG01-0YA0
Table 04

SINAUT communications modules
The list below gives an overview of SIMATIC WinAC RTX, WinAC Slot and WinAC MP that support the S7 Routing function.
 
TIM Version Order number
TIM 3V-IE as from V1.0 6NH7800-3BA00
TIM 3V-IE Advanced as from V1.1 6NH7800-3CA00
TIM 4R-IE as from V1.0 6NH7800-4BA00
TIM 4RD as from V3.x 6NH7 800-4AD90
Table 05

Note
The target station does not have to support the S7 Routing function.

Additional Keywords
Module function

Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?Go to beginning
Part number:

Description
The table below gives you an overview of the communication services that are supported by the CPUs with integrated PROFINET interface and by the WinAC RTX (F) via Industrial Ethernet.

18909487_CPUs_overview_e.pdf ( 16 KB )

The following entries include the manuals for the above-mentioned CPUs, which provide more information on the Technical Data, Communication Services and Quantity Frameworks.
 
CPU Entry ID
S7-300 12996906
S7-400 44444467
IM151-8 PN/DP CPU 47409312
IM154-8 CPU 44251850
WinAC RTX (F) 2010 43715176

The following entries give you an overview of the communication services that are supported by the S7-300 and S7-400 Industrial Ethernet CPs: Entry IDs  16767769 and 15368142.

Keywords
S7 communication, Open communication services, PROFINET IO, TCP, ISO-on-TCP, UDP, IO device, IO controller, PROFINET CBA

Which PROFIBUS connectors can you use in Zone 1 or 2?Go to beginning
Part number:

Description
The ET 200S and ET 200M distributed I/O systems may be used right into Zone 2. The ET 200iSP intrinsically safe distributed I/O system may be used right into Zone 1.

You can use the following PROFIBUS connectors for connecting the PROFIBUS network in Zone 2 (non-intrinsically safe PROFIBUS network).
 
30° outgoing cable unit
(max. 1.5Mbit/s)
35° outgoing cable unit
(max. 12Mbit/s)
90° outgoing cable unit
(max. 12Mbit/s)
6ES7 972-0BA30-0XA0 6ES7 972-0BA41-0XA0 6ES7 972-0BA52-0XA0
- 6ES7 972-0BB41-0XA01) 6ES7 972-0BB52-0XA01)
- 6ES7 972-0BA60-0XA0 6ES7 972-0BA12-0XA0
- 6ES7 972-0BB60-0XA01) 6ES7 972-0BB12-0XA01)
1) PROFIBUS connector has a PG socket

For connecting an ET200iS in Zone 1, you must configure the PROFIBUS network in this area as intrinsically safe. Therefore, the above-listed PROFIBUS connectors are not suitable.

Use the PB FC Standard Cable IS GP (order number: 6XV1831-2A) and the PROFIBUS connector 6ES7 972-0DA60-0XA0 to connect the ET 200iSP intrinsically safe remote I/O system to the PROFIBUS network.

The IK PI catalog ("PROFIBUS" chapter) contains the technical data, order data and the order numbers of other PROFIBUS bus cables and bus connectors.

IK PI Catalog

Warning
In order to set up an intrinsically safe PROFIBUS segment, it is imperative to use the RS 485-IS coupler.
The manual for the RS 485-IS coupler is available in Entry ID 29306413.

What are the system limits in an F CPU for safe bidirectional data communication via S7 Communication?Go to beginning
Part number:

Description:
This entry gives you an overview of the system limits of S7 Communication.

The following figures show the basic configuration of S7 Communication between F CPUs via Industrial Ethernet. Bidirectional data communication is via an S7 connection.


Fig. 01

Alternatively, bidirectional data communication can be via two separate S7 connections. In this way, you can structurally separate the send and receive channels, for example.


Fig. 02

The system limit of S7 Communication is determined by the following parameters:

  • Max. number of connections supported by the CPU.
  • Max. number of S7 connections that can be configured per interface.
  • Max. number of instances supported by the CPU.

Max. number of connections supported by the CPU
The following table shows the maximum number of connections supported by the F CPUs.
 
F CPU Max. number of connections 
IM 151-8F CPU 12
CPU 315F-2 PN/DP 16
CPU 317F-2 PN/DP 32
CPU 319F-3 PN/DP 32
CPU 416F-2 DP 64
CPU 416F-3 PN/DP 64
WinAC RTX F 2009 64

Max. number of S7 connections that can be configured
The following table shows the maximum number of S7 connections supported by the F CPUs.
 
F CPU Max. number of S7 connections that can be configured 
IM 151-8F CPU 10
CPU 315F-2 PN/DP 14
CPU 317F-2 PN/DP 16
CPU 319F-3 PN/DP 16
CPU 416F-2 DP with CP443-1 Adv. 62
CPU 416F-3 PN/DP 30
WinAC RTX F 2009 Via CP5611: 6
Via CP5613: 48
Via CP1616: 30
Via IE general: 14

Max. number of instances
The following table shows the maximum number of instances supported by the F CPUs.
 
F CPU Max. number of instances
IM 151-8F CPU 32
CPU 315F-2 PN/DP 32
CPU 317F-2 PN/DP 32
CPU 319F-3 PN/DP 32
CPU 416F-2 DP with CP443-1 Adv. Firmware version < V5.2: 1800 (can be configured: 600 preset)
Firmware version V5.2 onwards: 4000 (can be configured: 600 preset)
CPU 416F-3 PN/DP 600 (internal interface)
CPU 416F-3 PN/DP with CP443-1 Adv. Firmware version < V5.2: 1800 (can be configured: 600 preset)
Firmware version V5.2 onwards: 4000 (can be configured: 600 preset)
WinAC RTX F 2009 600 (can be configured: 300 preset)

Example:
In a CPU 319F-3 PN/DP, you select S7 Communication via TCP/IP for safe bidirectional data communication. Depending on whether the data communication is via one or two configured S7 connections, you can configure another 15 or 14 S7 connections.

The fail-safe communication blocks "F_SENDS7" and "F_RCVS7" are called in the CPU user program for safe bidirectional data communication via S7 connections. These blocks internally call the system function blocks SFB8 "USEND" and SFB9 "URCV" respectively. In this way, the user data and associated acknowledgments are sent and received. An instance data block is assigned to each SFB8 "USEND" and SFB9 "URCV" system function block. Thus, the number of instance data blocks (= instances) is identical to the number of communication jobs.

This means that in the case of safe bidirectional data communication, at least four communication jobs are executed and four instances are needed. In this case, with the CPU 319F-3 PN/DP there remain 28 free instances.

In the user program of the CPU 319F-3 PN/DP, you can call a maximum of 16 fail-safe communication blocks "F_SENDS7" or F_RCVS7", because the maximum of instances is limited to 32.
In the case of safe bidirectional data communication, the CPU 319F-3 PN/DP can communicate with a maximum of 8 F CPUs.

Calculation for safe bidirectional data communication in the CPU 319F-3 PN/DP:
8  "F_SENDS7" + 8 "F_RCVS7" = 16 fail-safe communication blocks
8*("USEND" + "URCV") + 8*("USEND" + "URCV")
= 16 "USEND" + 16 "URCV" = 32 communication jobs or instances

Note:
The safety function is foremost with F CPUs. Therefore, the system limit of S7 Communication is determined not only by the number of communication connections, but also by the response times achieved. If the required response times are not achieved because of the number of communication connections, the remedy is to

  • Reduce the number of communication connections.
  • Use a larger and faster CPU.

Which SIMATIC S7 components and which drives support clock-synchronicity functionality?Go to beginning
Part number:

Configuration notes:
Clock synchronicity is used to establish a direct connection between the equidistant DP cycle, the I/O modules and the user program.

The following SIMATIC components support clock-synchronicity functionality:

  • S7-300 CPUs
    • CPU 315 and CPU317 as DP masters from FW 2.5
    • CPU 319 as DP masters from FW2.4
  • S7-400 standard and S7-400F CPUs as DP masters from FW 3.1
  • ET 200M with selected modules
  • ET 200S with selected modules
  • Repeaters and diagnostics repeaters

Please note that only the internal DP interfaces on the CPUs can be used for clock-synchronicity communication.
STEP 7 V5.2 or higher is required for configuration purposes. 

The drives which support the clock-synchronicity functionality are the entire product group comprising "SIMODRIVE 611U", "SINAMICS" and "MASTERDRIVE MC".

The following are required in order to configure the drives: Drive ES Basic V5.2 or higher, STEP 7 V5.2 or higher and one of the CPUs mentioned above.

You can find a list with the precise designations of the SIMATIC modules, which support clock-synchronicity functionality, in the manual SIMATIC Clock Synchronicity in subsection 2.2.1 of Entry ID 15218045

Keywords:
Constant bus cycle time, Compatibility list

ET 200S: Are there special requirements for ET200S when mounted on sheet metal plates?Go to beginning
Part number:
Request : Are there special requirements for ET 200S when
   mounted on sheet metal plates?
   May standard mounting plates and DIN rails (mounting rails) be used? Are 
   yellow passivated sheet metal plates permitted?

Suggestion : There is no special requirements regarding surface or 
   material of mounting plates and DIN rails. Our factory does not use yellow 
   passivated steel plates anymore due to hazardous substances beeing emitted 
   during passivation process. 
   The only requirement for the mounting rail is a fixing screw at every 200 mm 
   for stability reasons.
                                                                                
ET200S: How many motor starters can be allocated to a power module?Go to beginning
Part number:
Request : What is the criteria in an application of power
   modules with regard to amount of motor starters and distribution of 
   potential?

Suggestion : A power mudule serves to supply load power to motor 
   starters.
   It is possible to configure load groups and potential groups. 
   A potential group always requires its own power module.
   One power module can be used for several load groups with a rated current of 
   max. 40 A each (at common potential)
   From the electrical point of view, up to 20 motor feeders can be allocated to
   one power modul.
   A total maximum physical length of 100 cm of an ET200S station is permitted.
                                                                                
ET 200S: How many motor starters can be allocated to a power module?Go to beginning
Part number:
Request : What is the criteria in an application of power
   modules with regard to amount of motor starters and distribution of 
   potential?

Suggestion : A power mudule serves to supply load power to motor 
   starters.
   It is possible to configure load groups and potential groups. 
   A potential group always requires its own power module.
   One power module can be used for several load groups with a rated current of 
   max. 40 A each (at common potential)
   From the electrical point of view, up to 20 motor feeders can be allocated to
   one power modul.
   A total maximum physical length of 100 cm of an ET200S station is permitted.
                                                                                
ET 200S: How many load feeders may be connected?Go to beginning
Part number:
Request : ET 200S: How many load feeders may be 
   connected? What must be observed?

Suggestion : The maximum amount of load feeders depends on the total 
   current per load group/ potential group and the maximum bus length.
   The maximum total current per group is 40 A, the maximum bus length of an 
   ET200S station is 100 m.
   The space requirements of all other modules (interface-, electronic-, power-,
   distance modules, etc.) must be taken into consideration.
   Are more feeders required as possible acc. to the above, one more ET200S 
   station must be used. A multi-tier installation is not possible at the 
   moment.
   At vertical mounting, simultaneity factor, ambient temperature and load must 
   be observed. Important is the maximum bus length of 100 m.
   DOL starters for one direction of rotation and reversing starters may be 
   mixed.
                                                                                
Calculating the maximum absolute error of the counter module 1Count24V/100kHz (6ES7 138-4DA02-0AB0) when measuring rotational speed Go to beginning
Part number:

QUESTION:
How can you calculate the maximum absolute error of the counter module 1Count24V/100kHz (6ES7 138-4DA02-0AB0) when measuring rotational speed?

ANSWER:
If the information in the manual about the error when measuring rotational speed is not sufficient for your purposes, you can use the following formula to calculate the maximum absolute error:

Example:

Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gasGo to beginning
Part number:

SIMATIC modules of the product families

  • S7-300
  • S7-400
  • ET 200M
  • ET 200S
  • ET 200iSP
  • TDC

are also approved for implementation in environments with high concentrations of corrosive gas in compliance with ISA–S71.04 severity level G1; G2; G3.

The relevant information is given in the manuals of the product families S7-300, S7-400, ET 200M, ET 200S, ET 200iSP and TDC.
Please refer to the relevant manuals for more information on climatic environmental conditions.

Baud rates for ET200S FO modulesGo to beginning
Part number:

QUESTION:
Which PROFIBUS DP baud rates can I use for the communication to my ET200S FO module?

ANSWER:  
The module supports the following baud rates:

  • 12 Mbit/s
  • 1.5 Mbit/s
  • 500 Kbit/s
  • 187 Kbit/s
  • 93.7 Kbit/s
  • 19.2 Kbit/s
  • 9.6 Kbit/s

If you try to set a different baud rate, then in STEP 7 V5.2 you get the error message shown in Fig. 1.

Fig 1: Error message in STEP 7 V5.2

Important:
In STEP 7 V5.1 it is also possible to set transmission rates of 3 Mbit/s and 6 Mbit/s. But these baud rates are not suitable for secure communications.

Maximum power load for digital output modulesGo to beginning
Part number:

QUESTION:
Can a digital output module with a nominal current of e.g. 0,5A be loaded in the range of the threshold value of the short circuit protection (0,7 to 1,8A)?

ANSWER:
Power monitoring is done thermic. The reached value - except for the circuit allowance - depends on the slope control speed and the temperature, which increases rapidly for a power supply of more than 0.5A. The module can only temporarily be loaded with an slope increase between 0.5 to about 1.7A without activating the thermal monitoring.

Note:
While activating the thermal monitoring the module will not be damaged.

Minimum distance to the ET 200S frontGo to beginning
Part number:

QUESTION:
What is the minimum distance to be kept to the front door when mounting an ET 200S in a control cabinet?

ANSWER:  
There is no minimum distance specified, for example for heat dissipation. However, a distance of about 2mm should be kept to accommodate any tolerances in the components which might prevent the front door of the control cabinet from closing properly.

Note:
Please pay attention to the different sizes of the various ET200S modules.

How do you assign and identify thermocouples?Go to beginning
Part number:

Principle:
According to the Seebeck effect, when two different metals are combined there is touch voltage at the points of contact, which depends on the temperature.

The thermo material combinations are standardized. The different material properties of a thermocouple determine the different application cases.

The following table shows the assignment of thermocouple types to the various material compositions:
 

Type

Material composition

Temperature range

T

Cu-CuNi (IEC 584) -270 °C - 400 °C

K

NiCr-Ni (IEC 584) -270 °C - 1372 °C

B

PtRh-PtRh (IEC 584) 200 °C - 1820 °C

N

NiCrSi-NiSi (IEC 584) -270 °C - 1300 °C

E

NiCr-CuNi (IEC 584) -200 °C - 900 °C

R

PtRh-Pt (Pt 13%) (IEC 584) -50 °C - 1769 °C

S

PtRh-Pt (Pt 10%) (IEC 584) -50 °C - 1769 °C

J

Fe-CuNi (IEC 584) -210 °C - 1200 °C

C

W-Re(IEC 584) 0 °C - 2320 °C

L

Fe-CuNi (DIN 43714) 0 °C - 760 °C

U

Cu-CuNi (DIN 43714) -200 °C - 600 °C

TXK / TXK (L)

NiCr-CuCr (P8.585-2001) -200 °C - -150 °C

The following table gives an overview of which modules the thermocouples can be connected to.

ET 200S:
 
Type T K B N E R S J C L U TXK
2AI TC ST X X X X X X X X   X    
2AI TC HF X X X X X X X X X X    

ET 200M:
 
Type T K B N E R S J C L U TXK
SM 331 AI 8 x TC X X X X X X X X X X X  
SM 331 AI 8 x TC 16 Bit X X X X X X X X X X X X
SM331 AI 2 x 12 Bit   X   X X     X   X    
SM331 AI 8 x 12 Bit   X   X X     X   X    

ET 200iSP:
 
Type T K B N E R S J C L U TXK
4 AI TC X X X X X X X X   X X  

Note:
Pay attention to the polarity of the thermocouple wires.

Compensating circuit and thermocouple conductors:

Type T (IEC 584)   Type T (IEC 584 EX)

Fig. 01

  • The color of the insulating sleeve and the positive conductor is brown.
  • The color of the negative conductor is white.
  • The color of the insulating sleeve for intrinsically safe circuits is always blue.

Type K (IEC 584)   Type K (IEC 584 EX)

Fig. 02

  • The color of the insulating sleeve and the positive conductor is green.
  • The color of the negative conductor is white.
  • The color of the insulating sleeve for intrinsically safe circuits is always blue.

Type B (IEC 584)   Type B (IEC 584 EX)

Fig. 03

  • The color of the insulating sleeve and the positive conductor is gray.
  • The color of the negative conductor is white.
  • The color of the insulating sleeve for intrinsically safe circuits is always blue.

Type N (IEC 584)  Type N (IEC 584 EX)

Fig. 04

  • The color of the insulating sleeve and the positive conductor is pink.
  • The color of the negative conductor is white.
  • The color of the insulating sleeve for intrinsically safe circuits is always blue.

Type E (IEC 584)   Type E (IEC 584 EX)

Fig. 05

  • The color of the insulating sleeve and the positive conductor is purple.
  • The color of the negative conductor is white.
  • The color of the insulating sleeve for intrinsically safe circuits is always blue.

Type R / S (IEC 584)  Type R / S (IEC 584 EX)

Fig. 06

  • The color of the insulating sleeve and the positive conductor is orange.
  • The color of the negative conductor is white.
  • The color of the insulating sleeve for intrinsically safe circuits is always blue.

Type J (IEC 584)    Type J (IEC 584 EX)

Fig. 07

  • The color of the insulating sleeve and the positive conductor is black.
  • The color of the negative conductor is white.
  • The color of the insulating sleeve for intrinsically safe circuits is always blue.

Type C (IEC 584)  Type C (IEC 584 EX)

Fig. 08

  • The color of the insulating sleeve and the positive conductor is red.
  • The color of the negative conductor is white.
  • The color of the insulating sleeve for intrinsically safe circuits is always blue.

Type L (DIN 43714)

Fig. 09

  • The color of the insulating sleeve is blue.
  • The color of the positive conductor is red.
  • The color of the negative conductor is blue.

Type U (DIN 43714)

Fig. 10

  • The color of the insulating sleeve is brown.
  • The color of the positive conductor is red.
  • The color of the negative conductor is white.

Note:
When you use thermocouples, you must run a temperature compensation. More information on the temperature compensation options when using thermocouples is available in Entry IDs: 19164525; 19163406; 19164641; 19243010

How long does the input signal have to be present before an analog input module identifies this signal as a process alarm?Go to beginning
Part number:

Instructions
This value is dependent on the conversion time, the type of measurement (current, voltage and resistance measurement) and the number of active channels.

The total conversion time determined (basic conversion time + additional conversion times) for a channel has to be multiplied by the number of active channels. This gives you the cycle time for a module. A signal must be present for at least this time to ensure that it is recognized as a process alarm.

The following manuals give information on the length of the basic conversion times of the various modules and on any additional conversion times that might have to be taken into account 
 
Modules Manual

Entry ID

ET200M  SIMATIC S7-300 programmable logic
controller, module data
8859629
ET200S  SIMATIC ET 200S distributed I/O system 
1144348
ET 200iSP SIMATIC ET 200iSP distributed I/O device 28930789
ET 200pro SIMATIC ET 200pro distributed IO system 21210852
ET 200eco PN SIMATIC ET 200eco PN distributed I/O device 29999018

If smoothing of the input signals has also been configured, the smoothing level which has been parameterized has to be taken into account. The smoothing levels (weak, medium and strong) are multiples of the cycle time and vary depending on the module used. 
The smoothing level attenuates the rise of an input signal. The specification in cycles indicates in how many cycles an input signal with 63% of its maximum value is recognized

Note
Refer to the manuals listed above to find out the number of cycles per smoothing level for your module.

 Entry ID:22742904   Date:2013-03-26 
I regard this article....as helpfulas not helpful                                 






























related links
ET 200S: Motorstarters: Maximum c ...
ET 200S: How many motor starters ...
ET 200S: How many load feeders ma ...
Which modules can you use when im ...
ET 200S: Motorstarter standard: C ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour