show the entry list

ES - SIMATIC Manager -- Product information -- Checking compatibility 
Compatibility Tool for Automation and Drive Technology 
What are the basic requirements for data exchange between COMOS and SIMATIC PCS 7? 
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11? 
How can you find out which Microsoft Patches are installed on the PC? 
Why can different versions of PCS 7 not be operated in mixed mode? 
Which modules and their firmware versions are released for PCS 7 and how can you update them? 
With what are SIMATIC PCS 7 V8.x, V7.x, V 6.x, V5.x and V4.x compatible? 
Why can't you use Service Packs for Microsoft Windows, the MS SQL Server or the Internet Explorer if they do not originate from the CDs/DVD provided with the PCS 7 software? 
What support does Microsoft provide for Microsoft products (operating systems and Internet Explorer) implemented with PCS 7? 
Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC PCS 7? 
Important note on Microsoft Patches KB 943459 and KB 971468 
Important note when using Microsoft's automatic update service in PCS 7. 
Additional information on the compatibility of PCS 7 V6.x and Microsoft products 

Compatibility Tool for Automation and Drive TechnologyGo to beginning
Part number:

Compatibility Tool
Compatibility information for Automation and Drive Technology is available in the Compatibility Tool of the Industry Online Support.
The tool is designed to support you in questions about the compatibility of various hardware and software products.
The database is constantly being revised and extended. In addition, you can use the tool centrally to download the compatibility lists of the separate product lines as Excel files.

The table below contains the links to the Compatibility Tool.

Brief Instructions
To query the compatibility information you require, you must first choose a "master component" (WinCC, PCS 7, STEP 7, ...). To these "master components" you can add more components (such as operating systems, virus scanners, ...). Once you have chosen the components you require, you can have the compatibility list shown by clicking the "Show compatibility" button. A detailed description of the tool is available in the Online_Help.pdf file in the table below.

 
Compatibility Tool Manual compatibility check
This video shows you the ways of manually checking compatibility using an example.
In this example we use WinCC, STEP 7, an operating system and a virus scanner. You can extend the list to suit your requirements.
  Download (ZIP) ( 68307 KB )

 
Compatibility Tool Updates in January 2014
This video introduces you to the new functions in the Compatibility Tool. (download of the compatibility lists, for example).
  Download (ZIP) ( 64912 KB )

 
Contents
Short Link to Compatibility Tool
German: http://www.siemens.de/kompatool
English: http://www.siemens.com/kompatool
Language-dependent link to the Compatibility Tool
https://support.automation.siemens.com/kompatool/index.html?lang=en&camid=K000003
Documentation
Online_Help.pdf
Table 01

Compatibility Tool revision history
The table below shows you the changes made in the past three months (data status and software functions).
 
Edition Data Update Software Update
12/2014 New compatibility information for: 
  • Openness (TIA Portal): V12.0
  • SIMATIC NET PC Software: V12.0 SP1, V12.0 SP2
  • SINAUT ST7 Engineering: V5.3
  • SINEMA Server: V12
  • STEP 7: V5.4 SP3.1, V5.4 SP5, V5.5, V5.5 SP1, V5.5 SP2, V5.5 SP3, V5.5 SP4
  • STEP 7 Basic (TIA Portal): V11.0, V11.0 SP1, V11.0 SP2, V12.0, V12.0 SP1, V13.0
  • STEP 7 Professional: 2010, 2010 SR1, 2010 SR2, 2010 SR3, 2010 SR4
  • STEP 7 Professional (TIA Portal): V12.0 SP1, V13.0
  • WinAC ODK: V4.2, V4.2 SP1
  • WinCC: V6.2, V6.2 SP2, V6.2 SP3, V7.0, V7.0 SP1, V7.0 SP2, V7.0 SP3, V7.2, V7.3, V7.3 SE Upd1
  • WinCC (TIA Portal)/ControlDevelopment: V12.0, V13.0
  • WinCC Advanced (TIA Portal): V11.0, V11.0 SP1, V11.0 SP2, V12.0, V12.0 SP1, V13.0
  • WinCC Basic (TIA Portal): V11.0, V11.0 SP1, V11.0 SP2, V12.0, V12.0 SP1, V13.0
  • WinCC Comfort (TIA Portal): V11.0, V11.0 SP1, V11.0 SP2, V12.0, V12.0 SP1, V13.0
  • WinCC flexible: 2008, 2008 SP1, 2008 SP2, 2008 SP3
  • WinCC Professional (TIA Portal): V11.0, V11.0 SP1, V11.0 SP2, V12.0, V12.0 SP1, V13.0
  • WinCC RT Advanced (TIA Portal): V11.0, V11.0 SP1, V11.0 SP2, V12.0, V12.0 SP1, V13.0
  • WinCC RT Professional (TIA Portal): V11.0, V11.0 SP1, V11.0 SP2, V12.0, V12.0 SP1, V13.0
 
11/2014 New compatibility information for: 
  • Drive ES PCS 7: V7.0 SP1
  • Openness (TIA Portal): V13.0
  • PCS 7: V7.0, V7.0 SP1, V7.0 SP2, V7.0 SP3, V7.1 SP3, V8.0, V8.0 Upd1, V8.0 SP1, V8.0 SP1 Upd1, V8.0 SP2, V8.1
  • SIMATIC Information Server: 2014
  • SIMATIC NET PC Software: V12.0 SP1, V12.0 SP2
  • SIMATIC Process Historian: 2014
  • STEP 7: V5.4, V5.4 SP1, V5.4 SP2, V5.4 SP3, V5.4 SP3.1, V5.4 SP4, V5.4 SP5, V5.5, V5.5 SP1, V5.5 SP2, V5.5 SP3, V5.5 SP4
  • STEP 7 Professional: 2010 SR4
  • WinCC: V7.2, V7.3
  • WinCC Advanced (TIA Portal): V13.0
  • WinCC Basic (TIA Portal): V13.0
  • WinCC Comfort (TIA Portal): V13.0
  • WinCC Professional (TIA Portal): V13.0
  • WinCC RT Advanced (TIA Portal): V13.0
  • WinCC RT Professional (TIA Portal): V13.0
 
10/2014 New compatibility information for: 
  • Drive ES Basic: V5.4 SP4, V5.4 SP5, V5.5, V5.5 SP1
  • Drive ES PCS 7: V7.1 SP1
  • PCS 7: V6.1, V6.1 SP1, V6.1 SP3, V7.0, V7.0 SP1, V7.0 SP2, V7.0 SP3, V7.1 SP4, V8.0, V8.0 SP1, V8.0 SP1 Upd1, V8.0 SP2, V8.0 Upd1, V8.1
  • SIMATIC NET PC Software: V6.4 (Edition 2006), V6.4 (Edition 2006) HF1, V6.4 (Edition 2006) HF11, V6.4 (Edition 2006) HF6
  • SIMOTION Scout: V4.4
  • STEP 7: V5.4 SP5, V5.5, V5.5 SP1, V5.5 SP2, V5.5 SP3, V5.5 SP4
  • STEP 7 Basic (TIA Portal): V12.0, V12.0 SP1, V13.0
  • STEP 7 Professional (TIA Portal): V12.0, V12.0 SP1, V13.0
  • TIA Openness: V13.0
  • WinCC: V7.0 SP3, V7.2, V7.3
  • WinCC (TIA Portal)/ControlDevelopment: V13.0
  • WinCC Advanced (TIA Portal): V12.0 SP1, V13.0
  • WinCC Basic (TIA Portal): V12.0 SP1, V13.0
  • WinCC Comfort (TIA Portal): V12.0 SP1, V13.0
  • WinCC flexible: 2004, 2004 SP1, 2005, 2005 SP1, 2007, 2008, 2008 SP1, 2008 SP2, 2008 SP3
  • WinCC Professional (TIA Portal): V12.0 SP1, V13.0
  • WinCC RT Advanced (TIA Portal): V11.0, V11.0 SP1, V11.0 SP2, V12.0 SP1, V13.0
  • WinCC RT Professional (TIA Portal): V11.0, V11.0 SP1, V11.0 SP2, V12.0 SP1, V13.0
 
Table 02

Additional Keywords
2334224, 5895889, 6248329, 8250891, 8795716, 9061581, 9859007, 10154608, 11703924, 15082268, 15082926, 15093580, 15227707, 18734363, 19378505, 21169761, 21649775, 21852809, 21927667, 21927773, 21954341, 22055368, 22055716, 22056585, 24122009, 24254820, 25092587, 26998997, 31592453, 33912473, 37208360, 37571060, 40357341, 41306596, 49382005, 49382338, 49383047, 49385278, 49452605, 49453265, 49455057, 51120883, 51694087, 52255904, 67653438, .NET Framework, 05/2000+SP2, 07/2001, 11/2002, 11/2003+SP1, Operating systems, Compact Flash, DOT NET, DOTNET Framework, Drive ES, Drive ES Basic, Drive ES SIMATIC, Drive ES PCS 7, Edition 2005+HF1, Edition 2006, Edition 2007, Edition 2008, FDA 21 CFR Part 11, Remote diagnostics, Remote control, Remote servicing, Releases, Third-party software, GMP, Upgrade, IE, iMAP, Internet Explorer, Communication requirements, Comparison Tool, Compatible, Compatibility, Compatibility list, Compatibility matrix, Compatibility tool, CompaTool, Life Science, McAfee VirusScan, Migration, MS .NET, PCS 7 Migration OS Options, Pharma, ProTool, RAID System, S7, SIMATIC PC BIOS Manager, SIMATIC PC DiagMonitor, SIMATIC PC Image & Partition Creator, SIMOTION Scout, SmartTools, SSD, PCS7, STEP7, Symantec AntiVirus, SIMATIC NET, System requirements, TIA Portal, Trend Micro Office Scan, Overview, V12, V8.0, V8.1, V8.2, Validation, Version, Virus scanner, Vista, WebNavigator, Win7, Win8, WinAC RTX, Windows 2000 Professional, Windows 2003 Server, Windows 2008 Server, Windows 7, Windows 8, Windows 98, Windows operating system, Windows ME, Windows NT, Windows Seven, Windows Vista, Windows XP, Windows version, XP, Additional software

What are the basic requirements for data exchange between COMOS and SIMATIC PCS 7?Go to beginning
Part number:

Description
You must install the systems below to be able to exchange data between COMOS V10.0 SP1 and SIMATIC PCS 7.
 
Requirements
COMOS and PCS 7 on one computer
Install
  • COMOS V10.0 SP1 (or higher version) and the Automation Interface component
  • SIMATIC PCS 7 V7.1 SP2 (or higher version)

Note
Here you must note that with PCS 7 V7.1 SP2 you can only exchange data that PCS 7 V7.1 SP2 can handle. For example, the newly added control module types in PCS 7 V8.0 can only be exchanged in conjunction with PCS 7 V8.0.

COMOS and PCS 7 on different computers
Install:

Computer 1:

  • SIMATIC PCS 7 V7.1 SP2 (or higher version)
  • SIMATIC XML Transfer from the COMOS V10.0 SP1 DVD (or higher version)

Computer 2:

  • COMOS V10.0 SP1 (or higher version)
  • SIMATIC XML Transfer from the COMOS V10.0 SP1 DVD (or higher version)
  • SIMATIC PCS 7 V7.1 SP2 or higher with the programs below from the PCS 7 Installation DVD:
    - STEP 7
    - CFC
    - TH and IEA-PO

Notes

  • XML Transfer requires a SIMATIC PCS 7 installation. Using the trial licenses supplied with PCS 7 is sufficient because PCS 7 does not need to be started on the second computer.
  • Here you must note that with PCS 7 V7.1 SP2 you can only exchange data that PCS 7 V7.1 SP2 can handle. For example, the newly added control module types in PCS 7 V8.0 can only be exchanged in conjunction with PCS 7 V8.0.
Table 01

Additional Keywords
Integrated Engineering

Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?Go to beginning
Part number:

Description
Installation of one of the Microsoft security patches KB2467174, KB2467175, KB2465361 or KB2465367 causes a massive drain on resources (increase in handles) in WinCC Runtime (OS Runtime, WinCC Runtime Professional V11). This consumption of resources can lead to a standstill of WinCC Runtime.
It is strongly recommended not to install any of the Microsoft security patches KB2467174, KB2467175, KB2465361 or KB2465367.

Detailed information about these Microsoft security patches is available at these links:

A remedy is given in the entries below under the corresponding KB numbers.

Note
Refer also to
"Which Microsoft Security Patches have been tested for compatibility with SIMATIC WinCC?" in Entry ID: 18752994 and
"Which Microsoft Security Patches have been tested for compatibility with SIMATIC PCS 7?" in Entry ID: 18490004.

How can you find out which Microsoft Patches are installed on the PC?Go to beginning
Part number:

Description
Microsoft provides the option by means of WMI for determining which patches are installed.

What is WMI/WMIC?
WMI is the abbreviation for "Windows Management Instrumentation".
WMIC (Windows Management Instrumentation Command Line) extends WMI for operation by way of multiple command line interfaces and batch processing script files.

More information about WMI is available from Microsoft in the internet at
http://technet.microsoft.com/en-us/library/bb742610.aspx (English)

Procedure
 
No. Procedure
1 In the Windows Start menu you select the "Ausführen" menu item and enter the command "cmd". (German version)
In the Windows Start menu you select the "Run..." menu item and enter the command "cmd". (English version)


Fig. 01

2 In the DOS command window that opens you enter the command below:
wmic qfe list full /format:htable >C:\Temp\hotfixes.htm


Fig. 02

This command creates an HTM list with the installed patches of Microsoft  Windows.

3 Go to the path specified (here C:\Temp) and find the file Hotfixes.htm.
This file contains a list of all the Microsoft Windows patches installed on the SIMATIC PC.


Fig. 03

4 In this list you can find the patches required using the Search command.


Fig. 04

Further information
It is also possible to use Microsoft MBSA (Microsoft Baseline Security Analyzer).
http://technet.microsoft.com/en-us/security/cc184924 (English)
http://technet.microsoft.com/de-de/security/cc184924 (German)

Information about which Microsoft patches are released for WinCC is available in Entry ID: 18752994.

Information about which Microsoft patches are released for PCS 7 is available in Entry ID: 18490004.

Additional Keywords
Hotfix, KB

Why can different versions of PCS 7 not be operated in mixed mode?Go to beginning
Part number:

Description:
PCS 7 projects only support the use of a single version of PCS 7 products. Any mixed combinations of PCS 7 versions (e.g. PCS 7 V 4.02, V5.x, V6.0 and V6.1) are not supported.

Furthermore, stand-alone versions of standard SIMATIC software (SFC, CFC etc.) cannot be used for work on PCS 7 projects. There are important PCS 7-specific functions in the engineering station (ES) which are only active if PCS 7 ES is installed.

In addition, in the case of WinCC multi-client/client-server systems, the same WinCC service packs and hotfixes must be installed on the computers affected.

Note:
However, you can leave the blocks and firmware unchanged on the controller side (e.g. PCS 7 V5.0) but upgrade the engineering station and the operating station (e.g. to  PCS 7 V5.2, V6.0 or V6.1 ). There is detailed information available in the release notes for the version compatibility (Upgrading without new functionality).

Keywords:
Engineering toolset, Compatibility


Which modules and their firmware versions are released for PCS 7 and how can you update them?Go to beginning
Part number:

Description
The following manuals give an overview of which modules are released for which versions of PCS 7:
 
PCS 7 version -- Released modules Entry ID
PCS 7 V8.1 106210481
PCS 7 V8.0 SP1 68157377
PCS 7 V8.0 61187475
PCS 7 V7.1 SP3 (also valid for PCS 7 V7.1 SP4) 79719965
PCS 7 V7.0 SP1 28739248
PCS 7 V7.0 24831707
PCS 7 V6.1 21406213
PCS 7 V6.0 15229053
PCS 7 V5.2 8774030
PCS 7 V5.1  7174990
Table 01

Note
If other modules have been released with a service pack (SP) of a PCS 7 version, this is documented in the "Readme" file for that service pack.

Reading out the firmware version
You can determine the current firmware version of your module in the SIMATIC Manager or in the HW Config through the menu:
"PLC > Diagnostics/Settings > Module Status" or "PLC > Module Status". You must select the module required beforehand. In the hardware configuration, you can use this function to determine all the modules with loadable firmware (including I/O modules).


Fig. 01

The current firmware versions with a description of how to update from S7-400 CPUs are available in Entry ID 40945038

The current firmware versions to update from CP 443-1 are available at the following link:
 
CP used Link
Firmware updates for CP 443-1  CP443-1 firmware update *)
Firmware updates for CP 443-5 Extended  CP443-5 Extended firmware update *)
Table 02
*)
Change the language in the header to receive the downloads in the language of your choice.

As from PCS 7 V6.0, detailed notes on Upgrading and determining modules are available in the "Service Support and Diagnostics" manual. Links to the manuals are shown in the following table.
 
Manual Entry ID
Service Support and Diagnostics V8.1 sections 3.3 and 7.18.7 90682682
Service Support and Diagnostics V8.0 SP1 sections 3.3 and 7.18.7 68157287
Service Support and Diagnostics V8.0 sections 3.3 and 7.18.7 61187456
Service Support and Diagnostics V7.1 sections 2.3 and 6.16.7 36195904
Service Support and Diagnostics V7.0 sections 1.3 and 5.16.7 24449644
Service Support and Diagnostics V6.0 section 1.3 and chapter 5 15236128
Table 03

Notes

  • Since the IM 467 does not support CiR (Configuration in Run) and cannot be used for an H system, this module is not released for PCS 7. The IM 467 can be considered as a simplified version of the CP443-5 Extended. The IM 467 functions are also available with CP443-5 Extended, which is why CP443-5 Extended is to be used and a CP443-5 Extended is to be configured in HW Config.
  • The benefits of PCS 7, such as plant hierarchy, PCS 7 libraries, SFC and PCS 7 message system (Alarm_8P block. for instance), are not supported by S7-300 CPUs. The range of functions of the S7-300 CPUs is not sufficient for this. The S7-300 CPUs can be edited without using PCS 7 blocks and functions (libraries) with the SIMATIC Manager (including HW Config) and be programmed with CFC. The sample application "Integration of S7-300 Package Units into SIMATIC PCS 7 with the PCS 7 Industry Library" describes, among other things, the configuration steps for the integration of S7-300 CPUs in the form of package units into PCS 7.

Additional Keywords
Hardware update, Updates, FW 10447706, 20383858, 6932456

With what are SIMATIC PCS 7 V8.x, V7.x, V 6.x, V5.x and V4.x compatible?Go to beginning

Compatibility Tool
Compatibility information for PCS 7 is available in the Compatibility Tool of the Industry Online Support.
The tool is designed to support you in questions about the compatibility of various hardware and software products.
The database is constantly being revised and extended. In addition, you can use the tool centrally to download the compatibility lists of the separate product lines as Excel files.

We would appreciate your feedback on the new Compatibility Tool.
For this, we would kindly ask you to fill in and return the feedback form.

The table below contains the links to the Compatibility Tool and the feedback form.

Brief Instructions
To query the compatibility information you require, you must first choose a "master component" (WinCC, PCS 7, STEP 7, ...). To these "master components" you add more components (such as operating systems, virus scanners, other SIMATIC products, ...). Once you have chosen the components you require, you can have the compatibility list shown by hitting the "Show compatibility" button. A detailed description of the tool is available in the Online_Help.pdf file in the table below.
 
Contents

Link/Download

Link to Compatibility Tool
Documentation
Online_Help.pdf
Feedback Form
Your feedback to assist in the further development of the Compatibility Tool.
Table 01

Why can't you use Service Packs for Microsoft Windows, the MS SQL Server or the Internet Explorer if they do not originate from the CDs/DVD provided with the PCS 7 software?Go to beginning
Part number:

Description:
The PCS 7 OS software always includes by default a Microsoft Windows Service Pack, the MS SQL Server and the software for the Internet Explorer. This software has been specially put together and matched for PCS 7. It also includes components that are not available on the software CDs supplied by Microsoft.
Thus it is not possible use a Service Pack downloaded from the Microsoft Support pages, for example, even if it apparently has the identical version number. 

So you must use only the software packages supplied with the PCS 7 software.

Notes:

  • This applies only for Service Packs and not for Security Patches. If it is necessary to install a Microsoft Security Patch from the Microsoft Support pages, then an explicit release for this will not be issued. Details are explained in Entry ID 18490004 .
  • The statements above do not apply for the pcAnywhere software. You can use the original from Symantec with the relevant version number. More information on the compatibility of versions of pcAnywhere with versions of PCS 7 is available in Entry ID: 2334224 .

What support does Microsoft provide for Microsoft products (operating systems and Internet Explorer) implemented with PCS 7?Go to beginning
Part number:

Support phases
Support for Microsoft products is divided into 3 phases.


Fig. 01

General
Microsoft provides support for security updates for at least 10 years for business and developer products (not valid for XP Home, for example, for which support is provided for only 5 years).

In the Mainstream Support Phase and in the first two years of the Extended Support Phase security updates are provided via "Microsoft Updates".

In the last three years of the Extended Support Phase, very important or critical security updates are published on the Microsoft Download Center website.

Support for service packs ends either 12 months after release of the next service pack or at the end of support for the basic product, whichever is first the case.

1. Mainstream Support Phase (for all products)
Microsoft provides a Mainstream Support Phase of at least 5 years from the time the product becomes generally available.

Security Update Support:

  • General Hotfixes
  • Free Incident Support
  • Billable Support by Telephone or Internet
  • Support Services on Hourly Basis
  • Support for Warranty Claims
2. Extended Support Phase (not for all products)
For specific products Microsoft provides an Extended Support Phase for 5 years as of the end of the Mainstream Support Phase.
  • Security-related hotfix support provided free of charge.
  • All billable support options.
  • The general hotfix support requires a separate contract.
  • During the Extended Support Phase, Microsoft does not accept any requests for warranty support, changes to the design or new features.

3. Self Help Online Support (for all products)
The Online Support is available for at least 10 years as of release of the product. Online Support provides customers the opportunity of finding solutions to their technical problems themselves round the clock and free of charge via the Knowledge Base, FAQs and News Groups.

  • Accompanying support upon release of the product.

Note
The information you can find here is not exhaustive. You will find the latest information about Microsoft Support Lifecycle at this link:
http://support.microsoft.com/lifecycle/.

Further information

  • The compatibility of SIMATIC PCS 7 and the Microsoft Windows operating systems and the Internet Explorer is given in Entry ID: 2334224.
  • Install only those Service Packs that are on the CD/DVD. For further details, go to Entry ID: 19142000.
  • What you should watch out for when implementing Microsoft Security Patches in SIMATIC PCS 7 is described in Entry ID: 18490004.

Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC PCS 7?Go to beginning
Part number:

Instructions
Microsoft regularly rectifies security gaps in its products and makes these fixes available to its customers in the form of official patches. This usually happens every second Tuesday in the month, on so-called "Patch Tuesday". Microsoft divides up the updates into numerous different classifications
(http://support.microsoft.com/kb/824684/EN-US/
and
http://support.microsoft.com/kb/824684/de).

However, you only have to install "Security Patches" and "Critical Patches" to ensure that SIMATIC PCS 7 operation is secure and stable. For this reason, a PCS 7 test configuration has been set up in order to test the compatibility of the PCS 7 software with the above-mentioned patch classifications ("Security Patches" and "Critical Patches"). This system always features the very latest of the released versions of PCS 7 and Microsoft products released for operating these versions of PCS 7. Keeping pace with the updates published by Microsoft, compatibility tests with the latest released versions of PCS 7 are performed on the test system.
The attached table in xls format provides precise information about the Microsoft "Security Patches" and "Critical Patches" which are tested for compatibility. As far as possible, this is updated within two weeks after publication of the latest updates of the classification designated.
If reflects the Microsoft products installed in the PCS 7 test configuration. Therefore, a discrepancy between this list and the products installed in the project cannot be excluded. If a system requires more updates than contained in the published list, these updates are requested according to the additional installed products / software components. In this case, it is up to the user to install these updates.
We recommend installing all the available updates of both the named classifications to ensure that the system is protected.
However, we cannot say anything about the compatibility of such updates that we have not tested. Therefore, we recommend installing all the updates in separate project-specific test environment prior to rolling out the updates in the productive environment.

Download
 
Description Download
Excel file Security_Patches.xls ( 774 KB )
packed XML and model files Security_Patches_XML.zip ( 67 KB )
Table 01

In rare cases an update might have a negative effect on our software in our tests. This is noted in the "Comment" field in the list above. Furthermore, we inform you as fast as possible by newsletter of any indications and the resulting remedies.

Recommended procedure for patch management with the Microsoft Windows Server Update Service (WSUS)
These instructions assume that you have a WSUS installed for your PCS 7 system. How to proceed with the WSUS is described in Entry ID: 38621083.
 
No. Procedure
1 WSUS configuration:
In the "Products and Classifications" dialog you select the "Products" tab and then all the Microsoft products relevant for the system.
2 WSUS configuration:
In the "Products and Classifications" dialog you select the "Classifications" tab and then "Definition Updates", "Security Updates" and "Critical Updates".


Fig. 01

3 WSUS configuration:
Create the project-specific groups for distribution of the updates in the system.
4 Download the "Security_Patches.xls" Excel table above onto your computer.
5 Open the table and set the filter to "Failed" in the "Test Result" column.
6 Check the "Comments" column to see whether these updates have been replaced.
7 WSUS administration:
Select all the available updates in the "Critical Updates" and "Security Updates" categories and then deselect the non-released patches as in the list above. Release the patches for installation in the groups created.
8 Log in on the clients connected to the WSUS using an administrative account (the clients were configured to receive the updates from the WSUS).
9 Execute the updates offered.
Table 02

You can find more precise information about Industrial Security in connection with PCS 7 software in the PCS 7 Security Concept in Entry ID: 60119725.
For more detailed explanations about Microsoft Updates and the WSUS visit the following Microsoft sites.

Notes

  • To find out which Microsoft Patches are installed on the PC, refer to Entry ID: 48844294.
  • These guidelines apply only for version PCS 7 V6.1 SP1 and higher.

Warning
The procedure described above does not apply for new Microsoft Service Packs which still require an explicit release for use. If the patches require a higher version of the Microsoft software, then refer to the "PCS 7 readme" file or Entry ID: 2334224 to check whether these higher versions of the software or Service Packs are released for SIMATIC PCS 7.

Additional Keywords
Windows Update Service, Security Patch

Important note on Microsoft Patches KB 943459 and KB 971468Go to beginning
Part number:

Description
When using Microsoft operating system Windows Server 2003 SP1 or SP2, there can be rare cases of blocking on the OS clients if two clients (one after another) access the same runtime screen (*.pdl). Operation of the OS client is disrupted (hour glass) during this blocking.
The error that leads to this behavior is in the Kerberos ticket handling of the Microsoft operating system Windows Server 2003.

KB 943459 has been updated by Microsoft for Windows Server 2003 SP2 with KB 971468 (also available via WSUS).

More detailed information about Microsoft Patches is available in the entries below.

  • "Which Microsoft Security Patches have been tested for compatibility with SIMATIC WinCC?" in Entry ID: 18752994
  • "Which Microsoft Security Patches have been tested for compatibility with SIMATIC PCS 7?" in Entry ID: 18490004

A correction is provided by Microsoft in KB 943459 and KB 971468 at the following links.

We therefore recommend that you install Microsoft Patch KB 943459 or KB971468 as soon as possible.

German Link
http://support.microsoft.com/kb/943459/de

http://support.microsoft.com/kb/971468/de

English link
http://support.microsoft.com/kb/943459/en-us

http://support.microsoft.com/kb/971468/en-us

Installation notes
You have to restart the computer after installing this hotfix.
Close all SIMATIC applications beforehand.

Note
Patch KB 943459 modifies the following code in the Registry: HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Services\LanmanServer\Parameters OplockBreakWait. Do not change the default time of 35 seconds set in the parameter OplockBreakWait. 

Important note when using Microsoft's automatic update service in PCS 7.Go to beginning
Part number:

Instructions:

Important note when using Microsoft's automatic update service in PCS 7.

The automatic update service must be disabled with SIMATIC PCS 7!

If the update service is enabled, there is a danger that new software packages, service packs, hotfixes etc. will be installed by Windows components, which under certain circumstances might cause problems with PCS 7 if the constellation has not yet been tested and officially released.
New packages issued by Microsoft should only be installed after thorough testing for compatibility (e.g. with reference to the PCS 7 Release Notes).

Option 1 for disabling:
You can disable the automatic update service if necessary in the Control Panel by double-clicking on the "Automatic Updates" icon and deselecting the relevant option.

Option 2 for disabling:
By disabling the "Automatic Updates" service under:

  • "Computer Management > Services and Applications > Services" or
  • "Start > Settings > Control Panel > Administration > Services > "Automatic Updates"

Note:
The SIMATIC Rack PC IL 40 S was supplied for a time with "Restore" Images in which the Microsoft automatic update service is enabled. You must disable this after a "Restore".

You must make special arrangements for the following system configurations:
 
No. System configuration
1 Central software update server for office and system networks
If you are using a common SUS for your office network and the PCS 7 system network, which automatically receives the updates from the Microsoft servers and automatically distributes these to the PCs in the office and PCS 7 system networks, you must make sure that the PCS 7 system PCs do not receive these software updates!
2 Automatic update service enabled on the PCS 7 system PCs upon access to the Internet
If your PCS 7 system PCs have a direct Internet access and the automatic update service is started on these PCs, then please disable the automatic update service or make sure that the PCS 7 system PCs do not have a direct Internet access!

Therefore we recommend that either you install the Microsoft Security Patches manually or you assign the updates to the various networks via a dedicated software update server.

Note:
In the case of the PC bundles released for PCS 7 V6.1 in the ST PCS 7 catalog, the automatic update service is disabled by default for security reasons. Please note that this automatic update service is switched on in most other PCs!

Keywords:
Upgrading, Hotfix, Service Pack, SP, HF

Additional information on the compatibility of PCS 7 V6.x and Microsoft productsGo to beginning
Part number:

The information below applies only to PCS 7 V6.x. More cross-version information is available in Entry ID: 2334224.

Which settings must be made before installing SIMATIC PCS 7 V6.x on the Microsoft Windows 2000 operating system?

Configuration Notes:
After successfully installing the required version of MS Windows you must make the following settings on the PC before installing SIMATIC PCS 7 version V6.x.  
 
No. Step Note
1 If necessary, install Service Pack for version of MS Windows operating system
(for whether and which Service Pack is required see Entry ID: 2334224)
CD/DVD is included in the delivery package SIMATIC PCS 7 V6.
2 Install Microsoft Internet Explorer 6.0 SP1                                    
(Exception: Windows Server 2003 Standard Edition and Windows XP, see Entry ID: 2334224)
CD/DVD is included in the delivery package SIMATIC PCS 7 V6.
3 Install Microsoft SQL Server 2000 incl. SP3 or  SP3a (as from SIMATIC PCS 7 V6.1 SP1) CD/DVD is included in the delivery package SIMATIC PCS 7 V6.
4 Install Message Queuing Services  
5 Disable Index Service  
6 Disable Internet Information Service (IIS)
(Exceptions: Central Archive Server, StoragePlus Server, OS Web Server).
 
7 If necessary, install other MS Security Patches and Hotfixes
(for whether and which Security Pack or Hotfix is required see Entry ID: 2334224 - footnotes)
 

If these requirements are not met, installation of PCS 7 V6 does not start or is aborted later.

Note:
Please note the following when installing a computer that is to be integrated into a domain:

  • The Message Queuing Services may only be installed once the computer has been incorporated in the domain.
  • If you incorporate the computer into the domain subsequently, then you must reinstall the Message Queuing Services.

Detailed information on the installation, in particular of the IIS (with Central Archive Server or StoragePlus) and Message Queuing (especially with Windows 2000 Server) is available in the documents "PCS 7 - PC Configuration and Authorization", "PCS 7 - System Documentation - Readme" and in the Readme.wri file.

By way of example, we have listed the procedure for installing the Message Queuing Services for MS Windows 2000 Professional. When installing a Microsoft Windows 2000 Server, you can make the setting during Setup.
 
No. Procedure
1 Open the Control Panel via "Start > Settings > Control Panel".
2 Open "Software" with a double-click.
 3 In the "Software" dialog window you select the setting "Add/Remove Windows Components".


Fig. 01

4 In the dialog window that opens you set a check mark for "Message Queuing Services" and close the dialog with "Next".

Note: 
You need the MS Windows 2000 installation CD.


Fig. 02

Repeat steps 1 to 3 to disable/check the system settings of the Index Service and the Internet Information Service (IIS). Then depending on the current computer settings you disable the two options as shown in the figure below.


Fig. 03

Which language versions of Microsoft Windows are released for SIMATIC PCS 7 V6.x?

Valid up to and including SIMATIC PCS 7 V6.1

The language versions MUI (Multilingual User Interface (tested with German, English and French)), German, English and French of the Microsoft Windows operating systems have been released and tested for SIMATIC PCS 7 V6.x. As per the SIMATIC PCS 7 Catalog, MUI versions are supplied by default with Bundle PCs. Please also note the correlation between PCS 7 and the Windows operating system in Entry ID: 2334224.

Valid up as from SIMATIC PCS 7 V6.1 SP1
The language versions MUI (Multilingual User Interface (tested with German, English, French, Italian, Spanish and (simplified) Chinese)), German, English and French of the Microsoft Windows operating systems have been released and tested for SIMATIC PCS 7 V6.1 SP1 and higher. As per the SIMATIC PCS 7 Catalog, MUI versions are supplied by default with Bundle PCs. Please also note the correlation between PCS 7 and the Windows operating system in Entry ID: 2334224.
Note:
With the Chinese language setting of the MUI version, please refer to the notes in "Readme.wri", section 1.4.

Which Microsoft Windows 2000 MUI updates are released for PCS 7 V6.x?

The Microsoft Windows 2000 MUI Update is released for SIMATIC PCS 7 V6.0 + SP1 and higher.

In Windows 2000 with Multilingual User Interface (MUI), menus, window bars and the Internet Explorer contain English texts although the setting has been changed in the Regional and Language Options to menus and dialogs in German. The localization coverage by Microsoft is only about 90% in Windows 2000, as described in English at http://www.microsoft.com/globaldev/DrIntl/faqs/MUIFaq.mspx#MUIques4.

"..The percentage of localization coverage in Windows 2000 with MUI is about 90%. In Windows 2000 with MUI, there are many visible strings that appear in English. One of the most noticeable areas is the Start Menu. This is because the Start Menu is populated directly using the file names of folders and link files created at setup time. They appear in English even if you are running on a MUI system with Japanese User Interface, as English was the original installation language."

A solution for Internet Explorer 6 is also available. This is described in an article in the Microsoft Knowledge Base.

http://support.microsoft.com/default.aspx?scid=kb;en-us;264550 (English)

http://support.microsoft.com/default.aspx?scid=kb;de;264550 (German)

Which operating system is required for which type of computer (ES/OS) with PCS 7 V6.x?
he following Microsoft operating systems are required for the various PCS 7 computers depending on their implementation:
  
SIMATIC PCS 7 V6.x Microsoft Installation
Engineering Station Windows 2000 Professional 1)
Windows XP Professional 1)
Windows 2000 Server
(Multiproject Engineering) 2)
Windows Server 2003 Standard Edition
(Multiproject Engineering) 2)
Operator System - Single-user Windows 2000 Professional
Windows XP Professional
Operator System - Terminal (client) Windows 2000 Professional
Windows XP Professional
Operator System - Server Windows 2000 Server
Windows Server 2003 Standard Edition
SIMATIC Batch - Single-user Windows 2000 Professional
Windows XP Professional
SIMATIC Batch - Terminal (client) Windows 2000 Professional
Windows XP Professional
SIMATIC Batch - Server Windows 2000 Server
Windows Server 2003 Standard Edition
Central Archive Server (as from V6.1) Windows Server 2003 Standard Edition
1) Also for Multiproject Engineering with distributed storage of subprojects
2) Multiproject Engineering with central storage of the project on a server

Note:
This table only shows the general requirements. More details regarding which versions of PCS 7 are compatible with which versions of Windows operating systems are available in Entry ID: 2334224 .

Only the ES (ES server) on which the project is located must have a Windows 2000 Server or Windows Server 2003 Standard Edition license. For those Engineering Stations that access the projects stored on the ES server it is sufficient to have a Windows 2000 Professional or Windows XP Professional license.

More information on this is available in the appendix of the manual "PCS 7 - PC Configuration and Authorization" in Entry ID: 21406001 and Entry ID: 15236125.

Important information on the Microsoft Patches KB829019 (Microsoft .NET Framework 2.0) and KB887616 (Office 2003 Service Pack 2)
We would like to point out that in our PCS 7 system test incompatibilities were discovered with the following Microsoft Patches in conjunction with CAS (Central Archive Server) and Storage Plus in the PCS 7 V6.1 + SP1 software environment.
Patch KB829019 contains a newer version (V2.0) of .NET Framework and Patch KB887616 contains the Service Pack 2 of Office 2003.
The incompatibility is caused by .NET Framework V2.0 and impairs the trend display in the StoragePlus WebViewer.
Therefore, do not install these Microsoft patches and generally prevent installation of .NET Framework V2.0 on PCS 7 V6.1 + SP1 systems.

Please note when implementing a Windows Software Update Server that under certain circumstances the patches are installed automatically in the PCS 7 system by the Microsoft Windows Software Update Service if you do not configure the Windows Software Update Service accordingly.
Therefore you should make the necessary technical arrangements so that Microsoft patches KB829019 and KB887616 cannot be installed automatically and also not manually in PCS 7 systems.

Note:
In the case of the IL 43 PC bundles released for PCS 7 V6.1 + SP1 in the ST PCS 7 catalog, the Automatic Update service is disabled by default for security reasons. Please note that this Automatic Update service is switched on in most other PCs!

Keywords:
System requirements, Software compatibility, W2K, 17497957, 17695539, 16503796, 23791870

 Entry ID:22681689   Date:2015-01-16 
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
Topics
Help
Online Help
Guided Tour