show the entry list

STEP 7 -- Product information -- Checking compatibility  
Compatibility Tool for Automation and Drive Technology 
Which SIMATIC software can you install in 64-bit operating systems? 
Which virus scanner versions can you use for STEP 7 V5.3, V5.4 and V5.5? 
Tips and tricks to check STEP 7- compatibility 
Information on the topic of "Checking compatibility" 
How do you check a STEP 7 project for the software packages required to edit the STEP 7 project? 
Why does a message appear indicating that a foreign language has to be installed in the operating system when a project is opened from STEP 7 version V5.3 SP2? 
Are there lists for the compatibility of Microsoft operating systems and SIMATIC Software products? 
Which version of STEP 7 is compatible with which version of Internet Explorer? 
Which foreign language character sets and special characters can be used in STEP 7? 
Which version of STEP 7 is compatible with which version of Microsoft Windows operating system? 
Which SIMATIC software packages are compatible with which Microsoft Windows operating system and with STEP 7 V5.5? 

Compatibility Tool for Automation and Drive TechnologyGo to beginning
Part number:

Compatibility Tool
Compatibility information for Automation and Drive Technology is available in the Compatibility Tool of the Industry Online Support.
The tool is designed to support you in questions about the compatibility of various hardware and software products. The database is constantly being extended.
The database is constantly being revised and extended. In addition, you can use the tool centrally to download the compatibility lists of the separate product lines as Excel files.

We would appreciate your feedback on the Compatibility Tool.
For this, please fill in and return the feedback form to assist us in the continuous development of the Compatibility Tool.

The table below contains the links to the Compatibility Tool and the feedback form.

Brief Instructions
To query the compatibility information you require, you must first choose a "master component" (WinCC, PCS 7, STEP 7, ...). To these "master components" you can add more components (such as operating systems, virus scanners, ...). Once you have chosen the components you require, you can have the compatibility list shown by hitting the "Show compatibility" button. A detailed description of the tool is available in the Online_Help.pdf file in the table below.
 
Contents

Link/Download

Link to Compatibility Tool
https://support.automation.siemens.com/kompatool/index.html?lang=en
Documentation
Online_Help.pdf
Feedback Form
Your feedback to assist in the further development of the Compatibility Tool.
Table 01

Compatibility Tool revision history
The table below shows you the changes made in the past three months (data status and software functions).
 
Edition Data Update Software Update
04/2013 New compatibility information for:
  • PCS 7: V6.1 SPx, V7.0 SPx, V7.1 SPx, V8.0 Upd1, V8.1
  • WinCC: V7.2, V12 
  • STEP 7: V5.5 SP3
  • SIMATIC NET: V7.1 SP6, V8.2 SP1, V8.2 SP2

New software functions:

  • "Suggestion for the entry" directly from the tool through the Feedback function on the results pages.

  • General note texts on the single products now also in the Compatibility Tool.

  • Download of the compatibility data from the tool in Excel format over the menu item "Tools".

03/2013 New compatibility information for:
  • PCS 7: V6.1 SPx, V7.0 SPx V7.1 SPx, V8.0 Upd1, V8.1
  • WinCC: V7.2, V12 
  • WinCC flexible: 2008 SP2, 2008 SP3
  • STEP 7: V12
--
02/2013 New compatibility information for:
  • PCS 7: V6.1 SP4,V7.1, V7.1 SP1,V7.1 SP2, V7.1 SP3, V7.1 SP4, V8.0 Upd1
  • WinCC: V7.0 SP3, V12
  • WinCC flexible: 2008 SP3
  • STEP 7: V12
--
Table 02

Additional Keywords
Operating systems, Windows NT, Windows 98, Windows 2000, Windows ME, Windows XP, Windows 2003 Server, Windows Vista, Windows 2008 Server, Windows 7, Win 7, Windows 8, Win 8, Internet Explorer, IE, Migration, Upgrade, Additional software, Third-party software, GMP, Pharma, Life Science, Validation, FDA 21 CFR Part 11, .NET Framework, DOTNET Framework, Dotnetframework, MS .NET, Virus scanner, Compatibility matrix, Compatibility list, Compatibility Tool, CompaTool, Compa Tool, Symantec AntiVirus, Trend Micro Office Scan, McAfee VirusScan, 10154608, 25092587, 21649775, 5895889, 6248329, 19378505, 21954341, 21852809, 40357341, 49382005, WinBDE, SmartTools, 21927667, 15227707, 24122009, 33912473, 8795716, 11703924, 49382338, 15082926, 15093580, 41306596, 22055716, 22056585, 26998997, 31592453, 49383047, 49452605, 49453265, 49455057, 9859007 , 49385278

Which SIMATIC software can you install in 64-bit operating systems?Go to beginning
Part number:

Note
More information about the compatibility of SIMATIC products is available in the Compatibility Tool in Entry ID: 56699648.

Description
This entry describes which SIMATIC software you can install on a 64-bit operating system. The products below are described:

LOGO! Soft Comfort
As from LOGO! Soft Comfort V7.0 LOGO! Soft Comfort is enabled for a 64-bit operating system in the Windows 7 operating system.
Please also refer to the following entries:
 
Description Entry
For which operating systems is LOGO! Soft Comfort released? 25447431
Update installation of LOGO! Soft Comfort without installed LOGO! Software. 17164153
Release for LOGO! 12/24RCE, LOGO! 230RCE and LOGO! Soft Comfort V7. 51401590
Table 01

STEP 7 Micro/WIN
As from version STEP 7 Micro/WIN V4.0.9, STEP 7 Micro/WIN is enabled in the Windows 7 operating system for a 64-bit operating system.
Please also refer to the following entries:
 
Description Entry
Which version of STEP 7 Micro/WIN or S7-200 PC Access is compatible with which version of MS Windows? 8675614
Download STEP 7 MicroWIN V4.0 SP8 and SP9 58523240
New Service Packs available for STEP 7 MicroWIN V4.0 and S7-200 PC Access V1.0 60035301
Table 02

S7-200 PC Access
As from version S7-200 PC Access V1.0 SP6, S7-200 PC Access is enabled in the Windows 7 operating system for a 64-bit operating system.
Please also refer to the following entries:
 
Description Entry
Which version of STEP 7 Micro/WIN or S7-200 PC Access is compatible with which version of MS Windows? 8675614
Download S7-200 PC Access V1.0 SP5 and SP6 58495870
New Service Packs available for STEP 7 MicroWIN V4.0 and S7-200 PC Access V1.0 60035301
Table 03

STEP 7
As from version STEP 7 V5.5 SP1, STEP 7 is enabled for a 64-bit operating system in the Windows 7 and Windows Server 2008 R2 operating systems.
You need the full version of STEP 7 V5.5 SP1 or higher for the installation. A service pack or an update/hotfix is only for upgrading an existing installation.
Please also refer to the following entries:
 
Description Entry
Service Pack 2 for STEP 7 V5.5 and STEP 7 Professional Edition 2010 57026032
Download Service Pack 2 for STEP 7 V5.5 and STEP 7 Professional 2010 57026339
Compatibility Tool -- Operating systems released for STEP 7 56699648
Table 04

S7 Distributed Safety
S7 Distributed Safety version V5.4 Service Pack 5 and higher is enabled for operation in the Windows 7 and Windows Server 2008 R2 Standard Server Edition 64-bit operating systems.
Please also refer to the following entries:
 
Description Entry
S7 Distributed Safety V5.4 + Service Pack 5 available for downloading 37593103
Download S7 Distributed Safety V5.4 + Service Pack 5 37592670
Table 05

Motor Starter
Motor Starter ES version 2007 Service Pack 5 and higher is enabled for operation in the Windows 7 64-bit operating system.
Please also refer to the following entries:
 
Description Entry
Delivery release for the parameterizing software Motor Starter ES 2007 + SP5 61499792
Motor Starter ES 2007 Premium download (14-day Trial Version) including Service Pack 5 58098734
Windows compatibility of the SIRIUS ES software for Motor Starter? 61842339
Table 06  

WinCC flexible
As from version WinCC flexible 2008 SP3, WinCC flexible is enabled in Windows 7 for the 64-bit operating system.
You need the full version of WinCC flexible 2008 SP3 for the installation. A service pack or an update/hotfix is only for upgrading an existing installation.
Please also refer to the following entries:
 
Description Entry
With what are SIMATIC WinCC flexible 2008, 2007, 2005 and 2004 compatible? 22055368
Delivery release: Service Pack 3 for SIMATIC WinCC flexible 2008 57267466
Update (Hotfix) for WinCC flexible 2008 Service Pack 3 58860033
Compatibility Tool 56699648
Table 07

WinCC
As from version WinCC V7.0 SP3, WinCC is enabled for a 64-bit operating system in the Windows 7 and Windows Server 2008 R2 operating systems.
You need the full version of WinCC V7.0 SP3 for the installation. A service pack or an update/hotfix is only for upgrading an existing installation.
Please also refer to the following entries:
 
Description Entry
With what are SIMATIC WinCC V7.x, V 6.x and V5.x compatible? 21927773
Delivery release of SIMATIC WinCC V7.0 SP3 and WinCC V7.0 SP3 ASIA 55987264
Update 2 for WinCC V7.0 SP3 and WinCC V7.0 SP3 ASIA 60984587
Compatibility Tool 56699648
Table 08

STEP 7 Basic V10.5
The STEP 7 Basic V10.5 software is not enabled for any 64-bit operating system.

Note
More information and notes about installing STEP 7 Basic V10.5 are available in Entry ID: 42100716  

STEP 7 Basic and Professional V11/V12
As from version STEP 7 V11 SP2, STEP 7 V11 is enabled for a 64-bit operating system in the Windows 7 and Windows Server 2008 R2 operating systems.
You need the full version of STEP 7 V11 SP2 or STEP 7 V12 for the installation on a 64-bit operating system. If you already have a full version for a 32-bit operating system, you can use one of the packages below for installation on a 64-bit operating system:

  • STEP 7 Basic
    STEP7 Basic Single ->
    Floating License Package (6ES7822-0AA01-0YC5)
  • STEP 7 Professional
    Trial DVD STEP 7 Professional V11 SP2 (6ES7822-1AA01-0YA7)
  • STEP 7 Professional / Basic V12
    The order numbers are available in the delivery release in Entry ID: 67851956.

Please also refer to the following entries:
 
Description Entry
Which version of STEP 7 (TIA portal) is compatible with which version of the Microsoft Windows operating system? 51120883
Delivery release of Service Pack 2 for STEP 7 V11 56771572
Updates for STEP 7 V11 SP2 and WinCC V11 SP2 58112582
Delivery release of SIMATIC STEP 7 Professional / Basic V12 67851956
Compatibility Tool 56699648
Table 09

WinCC Basic, Comfort, Advanced and Professional V11/V12 (incl. Runtime)
As from version WinCC V11 SP2, WinCC V11 is enabled for a 64-bit operating system in the Windows 7 and Windows Server 2008 R2 operating systems.
You need the full version of WinCC V11 SP2 or WinCC V12 for the installation on a 64-bit operating system. If you already have a full version for a 32-bit operating system, you can use one of the packages below for installation on a 64-bit operating system:

  • WinCC Basic
    WinCC Basic V11 SP2 Single ->
    Floating License Package (6AV2100-0AA01-0AE5)
  • WinCC Comfort/Advanced
    WinCC Comfort/Advanced V11 SP2, TRIAL (6AV2102-0AA01-0AA7)
  • WinCC Professional
    WinCC Professional V11 SP2, TRIAL (6AV2103-0AA01-0AA7)
  • WinCC Runtime Advanced
    WinCC Runtime Advanced Update/Hotfix V11, V11 SP1 ->
    V11 SP2 (6AV2104-0XX01-0DU8)
  • WinCC Runtime Professional
    WinCC Runtime Professional Update/Hotfix V11, V11 SP1 ->
    V11 SP2 (6AV2105-0XX01-0DU8)
  • WinCC V12
    The order numbers are available in the delivery release in Entry ID: 67797516.

Please also refer to the following entries:
 
Description Entry
With what is SIMATIC WinCC V11 compatible? 51694087
Delivery release of Service Pack 2 for WinCC V11 56899318
Updates for STEP 7 V11 SP2 and WinCC V11 SP2 58112582
Delivery release of SIMATIC WinCC V12 67797516
Compatibility Tool 56699648
Table 10

SIMATIC NET
As from version SIMATIC NET DVD V8.1, operation is enabled for a 64-bit operating system in the Windows 7 and Windows Server 2008 R2 operating systems.
Please also refer to the following entries:
 
Description Entry
Which SIMATIC NET CD is released for which Microsoft Windows operating system? 9859007
Which SIMATIC NET PROFIBUS PC CP is compatible with which Microsoft Windows operating system? 22611503
Which SIMATIC NET Industrial Ethernet PC CP is compatible with which Microsoft Windows operating system? 23785421
Sales/delivery release of SIMATIC NET DVD V8.2 63098071
Sales/delivery release of SIMATIC NET DVD V8.1 52566921
Sales/delivery release of SIMATIC NET DVD V8.1 + SP1 and SIMATIC NET CD V7.1 + SP4 57989792
Download SIMATIC NET CD V8.0 SP1 HF1 12660737
Compatibility Tool 56699648
Table 11

STARTER
STARTER V4.3 and higher is enabled for operation in the Windows 7 and Windows Server 2008 R2 64-bit operating system. It is imperative to note the restriction for Windows Server 2008 R2 in the following delivery releases. 
Please also refer to the following entries:
 
Description Entry
Delivery release for SINAMICS MICROMASTER STARTER V4.3 SP1 and additional SSPs 59441514
Delivery release for SINAMICS MICROMASTER STARTER V4.3 SP1 incl. HF2 and additional SSPs 61585426
Download SINAMICS MICROMASTER STARTER 26233208
Table 12

Drive ES V5.5
As from version Drive ES Basic V5.5 SP1 operation is enabled in the Windows 7 64-bit operating system.
Please also refer to the following entries:
 
Description Entry
Delivery release for Drive ES Basic V5.5 SP1 60148716
Compatibility lists for Drive ES products 18495518
Table 13

SINAMICS Startdrive V12
As from SINAMICS Startdrive V12 operation is enabled in the Windows 7 64-bit operating system.
Please also refer to the following entry:
 
Description Entry
Delivery release for SINAMICS Startdrive V12 67271250
Table 14

TeleService V6.1 incl. SP5
As from TeleService V6.1 incl. SP5 operation is released for a 64-bit operating system in the Windows 7 and Windows Server 2008 R2 operating systems.
Please also refer to the following entry:
 
Description Entry
Delivery release for TeleService V6.1 incl. SP5 56906611
Table 15

D7-SYS V8.0
As from version D7-SYS V8.0, operation is enabled for a 64-bit operating system in the Windows 7 and Windows Server 2008 operating systems.
Please also refer to the following entry:
 
Description Entry
D7-SYS V8.0 delivery release 59257503
Table 16

Which virus scanner versions can you use for STEP 7 V5.3, V5.4 and V5.5?Go to beginning
Part number:

Compatibility Tool
A new Compatibility Tool is available for you at the Service & Support site.
It is designed to support you in questions of the compatibility of various SIMATIC software products.

The contents are due to be included in the Compatibility Tool.
We would appreciate your feedback on the new Compatibility Tool.
For this, please fill in and return the feedback form.

The table below contains the link to the Compatibility Tool and the feedback form.

Brief Instructions
To query the compatibility information you require, you must first choose a "master component" (WinCC, PCS 7, STEP 7, ...). To these "master components" you add more components (such as operating systems, virus scanners, other SIMATIC products, ...). Once you have chosen the components you require, you can have the compatibility list shown by hitting the "Show compatibility" button. A detailed description of the tool is available in the Online_Help.pdf file in the table below.
 
Contents

Link/Download

Link to Compatibility Tool
https://support.automation.siemens.com/kompatool/index.html?lang=en
Documentation
Online_Help.pdf
Feedback Form
Your feedback to assist in the further development of the Compatibility Tool.

Description
The file below lists the versions of the virus scanners released for STEP 7 versions V5.3, V5.4 and V5.5.
 
Contents

Link/Download

STEP7_Virenscanner_e.pdf

( 21 KB )

More information is available in the STEP 7 readme, section 6.2 General - Using virus scanners.

Note
The virus scanner versions specified are for STEP 7. We cannot make an valid statements about other virus scanners not in the list.

Keywords
Symantec AntiVirus, Trend Micro Office Scan, McAfee VirusScan, 49452605

Tips and tricks to check STEP 7- compatibilityGo to beginning
Part number:

Configuration Notes:
This entry includes tips and tricks on STEP 7 compatibility.

  1. Can a STEP 7 project from a current version be edited in a previous version?
  2. Can the communication cards CP5511 and CP5512 be used with STEP 7 V5.4 in MS Windows Vista?
  3. Which version of STEP 7 fully supports the scroll wheel functions of the Microsoft wheel mice?
  4. Why are the symbolic names not available if a program created with STEP 7 V5.4 is downloaded from the CPU into the PG with STEP 7 V5.3?

The table below provides information and remedies for the above.
 
No. Procedure:
1 Can a STEP 7 project from a current version be edited in a previous version?
STEP 7 projects are downwards compatible to the previous versions. Projects created in version 5.4 can also be edited in version 5.3. A prerequisite is that the project created in STEP 7 V5.4 cannot contain any components and functions not supported by the previous version, such as new CPU modules or new functions (such as access protection or SIMATIC Version Trail).
  • If a STEP 7 V5.4 project is to be processed, for example with STEP 7 V5.3, then you can only use module order numbers that are known in version V5.3 in the V5.4 project. If necessary, you should configure new modules with the "predecessor order number".
  • In future you will be able to "retroload" new modules as of STEP 7 V5.2 .

Refer also to the note in the readme file in section 6.6 "Changing between the different versions of STEP 7", "New modules in old versions of STEP 7". If you open or dearchive a project in STEP 7 version V5.2 that has been created in version V5.3 or V5.4, the following messages might be displayed. As a consequence, you can only read the hardware configuration.

  • S7 Hardware Update options package not available.
  • The project includes objects of the "Hardware Update" options package that cannot be processed because the options package is not installed or an obsolete version of it is installed.
2 Can the communication cards CP5511 and CP5512 be used with STEP 7 V5.4 in MS Windows Vista?
STEP 7 is released in Windows Vista Ultimate and Business as of version V5.4 SP3. STEP 7 is not released in Windows Vista Home Basic or Premium. To use the communication cards, note that the
  • CP5512 is released in Windows Vista, the driver is integrated in STEP 7,
  • CP5511 is not released in Windows Vista.

More information is available in the readme file under "Notes on using communication cards in PCs/PGs (section 4.4.2).

3 Which version of STEP 7 fully supports the scroll wheel functions of the Microsoft wheel mice?
As of version 5.2, STEP 7 supports the scroll wheel function of the Microsoft wheel mice. However, you must install the driver for your mouse separately (the Windows default driver is not sufficient here). The driver is supplied by your mouse manufacturer, usually on a separate CD.

Once you have installed the mouse driver, restart the computer and a mouse icon is displayed in the task bar (next to the clock). Open the Control Panel via "Start > Settings > Control Panel" and double-click on the "Mouse" icon. You can make additional mouse settings in the dialog window "Mouse Properties".


Fig. 01

4 Why are the symbolic names not available if a program created with STEP 7 V5.4 is downloaded from the CPU into the PG with STEP 7 V5.3?
Please refer to the information in the STEP 7 Online Help under
  • "Downloading from the PLC into the PG",
  • "Load station into PG..."

The blocks are stored in the CPU irrespective of the STEP 7 version without symbols and comments. To keep the assignment of the symbols and comments for your program, load the program back into the associated project.

Information on the topic of "Checking compatibility"Go to beginning
Part number:

Instructions:
Information on the topic of "Checking compatibility" is available in the following manuals and chapters / sections and in the Online Help.
 
Document

Edition

Chapter / Section Entry ID
Configuring Hardware and Communication Connections with STEP 7 V5.5 05/2010 01: "Basics of Configuring Hardware with STEP 7"
03  "Configuring the Distributed I/O (DP)"
11  "Configuring Connections"
45531110
Programming with STEP 7 V5.5 05/2010 08: "Defining Symbols"
26: "Tips and Tricks"
45531107
STEP 7 Online Help V5.5 "Compatibility"
"SIMATIC PC - Use configuration from previous versions"
 

 

How do you check a STEP 7 project for the software packages required to edit the STEP 7 project?Go to beginning
Part number:

Instructions:
If you edit a project that contains objects which have been created with software package, then you need that software package for editing the project. When you open a project it is automatically checked for the software packages required. Then the software packages missing on your system are displayed.

First you get the message indicating that one or more objects of a type cannot be displayed and that the server S7 ... could not be loaded. Acknowledge this message with OK. You are then presented with a list of the names of the missing software packages (e.g. S7-HiGraph - Fig. 01).


Fig. 01

Mark the project name in the SIMATIC Manager and select the Project Properties dialog via Edit > Object Properties. In the dialog that opens you select the Required software packages tab. This displays a list of all the software packages used for this STEP 7 project and whether or not they are installed on your PC.


Fig. 02

For example, if you wish to forward projects you have created yourself to other persons (e.g. colleagues / business partners), then for project editing it is useful to know which software packages are required. In this way you can adapt your project to your colleagues' STEP 7 installation, which might not be as extended as yours.

For this you select the project in the SIMATIC Manager and then the menu command Edit > Object Properties > Tab: Required software packages". Here you will find an overview of the software packages required for editing this project.


Fig. 03

The information on the software packages required is complete if:

  • the project (or all the projects in a multiproject) or the library have been created with STEP 7 V5.2 or higher
  • the project has been checked for software packages used - the check is made automatically when you open or dearchive an S7 project.

 

Why does a message appear indicating that a foreign language has to be installed in the operating system when a project is opened from STEP 7 version V5.3 SP2?Go to beginning
Part number:

 

Description:
From STEP 7 version V5.3 SP2, the system outputs a message indicating that the project can only be opened in the Windows language specified;

  • in projects which have been newly created from STEP 7 V5.3 SP2 and
  • which have been created in an operating system language which does not correspond to one of the STEP 7 languages or
  • the current Windows language, and
  • if the project has not been set to be language-neutral.

Please follow the instructions in the Readme file (section 2.26 Information about using foreign-language character sets). From STEP 7 V5.3 SP2 you can use foreign language character sets other than the STEP 7 language set. However, the setting for this requested character set must be defined in the operating system.

If you wish to open your STEP 7 project or your library under any language setting, you have to activate the option

  • "Can be opened in any language in the Windows Regional and Language Option (l. neutral)"

in the project's object properties. Follow the procedure described in the table below.  
No. Procedure
1 Set the operating system to the language which has been used to create the project. To switch the operating system to another language, you must change the settings for the menus and dialogs in the Control Panel. You can find information about this setting procedure in our FAQ
  • "How to switch the operating system to English"
    , which you can find on the Internet in Entry ID 22309945 .
2 Then, in order to back up your STEP 7 project, make a copy of your project via "File > Save as...".
3 Highlight the name of the project in the SIMATIC Manager and right-click it. Then select "Object properties" in the pop-up menu that opens.


Fig. 01

4 Go to the "General" tab in the "Properties - Project" dialog and enable the following option:
  • "Can be opened in any language in the Windows Regional and Language Option (l. neutral)"

and click OK to confirm the message which appears then.


Fig. 02

After saving with OK, you can use the project or library in different language-speaking areas with different character sets. Multiple projects are always created on a language-neutral basis.

Note:
A project should only be set to be language-neutral if the programmer is sure that no language-specific characters have been used in this project (which would lead to nonsensical characters in another operating system language).

These instructions have been verified with STEP 7 V5.3.

Are there lists for the compatibility of Microsoft operating systems and SIMATIC Software products?Go to beginning
Part number:

Configuration Notes
The following  table provides those Entries on SIMATIC Software Products that are compatible with Microsoft Operating Systems:
 

SIMATIC Software

Entry-ID

COM PROFIBUS

8460601

LOGO! Soft Comfort

25447431

ProAgent

9264513

Prodave MPI

8755573

S7-200 PC Access

8675614

SIMATIC PCS 7

2334224

SIMATIC ProTool Lite, ProTool, ProTool Pro

8795248

SIMATIC WinCC flexible

22055368

SIMATIC STEP 5

6002243

SIMATIC STEP 7

8250891

SIMATIC STEP 7 Lite

23642592

SIMATIC STEP 7 MicroWin

8675614

SIMATIC WinCC

21927773

SIMATIC NET-CD

9859007

SIMATIC WinCC/Web Navigator

6944907

SIMATIC STEP 7 (TIA Portal)

51120883

SIMATIC WinCC V11

51694087

Keywords
System Requirement, Windows, Windows Version

Which version of STEP 7 is compatible with which version of Internet Explorer?Go to beginning
Part number:

Configuration notes:
In the table below we can see which version of STEP 7 is compatible with which version of Internet Explorer?
 

STEP 7 version

Internet Explorer

  V4.01 V5.0 V6.0 V7.0 V8.0

V3.1

-

-

-

- -

V3.2

-

-

-

- -

V4.01

-

-

-

- -

V4.02

-

-

-

- -

from V4.02.5

-

-

-

- -

V5.0 incl. SPs

X

-

-

- -

V5.1

X

-

-

- -

V5.1 incl. SPs

X

-

-

- -

V5.2 incl. SPs

-

X

-

- -
V5.3 incl. SPs

-

-

X

- -

V5.4 incl. SPs

-

-

X

X X

V5.5 incl. SPs

- - X X X

In the case of versions of STEP 7 from V5.0 to V5.1 including SP 1, the Internet Explorer is required for the cross-function Online Help.
The Internet Explorer is required in general from STEP 7 V5.1 including SP2.

Keywords:
Compatibility

Which foreign language character sets and special characters can be used in STEP 7?Go to beginning
Part number:

Configuration Notes:
The following table contains some information on the foreign language character sets and special characters in STEP 7:
 
No. Foreign language character sets and special characters in STEP 7:
1 Foreign language character sets:
From STEP 7 V5.3 SP2 you can use foreign language character sets in projects and libraries other than the STEP 7 language set. Requirements:
  • You must have Windows Multilingual User Interface (e.g. MS Windows XP MUI) installed on your PC and
  • The setting for this requested character set must be defined in the operating system.

More information is available in the STEP 7 Online Help under "Note on Using Foreign-Language Character Sets" and under "Settings the Windows Language." The following foreign language character sets are released under MS Windows MUI:

  • Japanese
  • Chinese (Simplified)
  • Korean
  • Russian
  • Greek

Also note the "Note on Using Foreign-Language Character Sets" (section 6) in the STEP 7 readme file.

2 Special characters in STEP 7:
From STEP 7 V5.2 you can enter special characters for documentation purposes or as a comment without any restrictions.

If you are using a version of STEP 7 < V5.2, then it might not be possible to enter special characters directly in every STEP 7 application. For example, in STEP 7 V5.1 it is possible to enter special characters directly in comment fields in the HW Config, but not in block or network comment fields in the LAD/FBD/STL editor.
In this case you can enter the special characters via the relevant ASCII codes. To enter characters via their ASCII codes you must press and hold the ALT key and enter the relevant code via the numbers keypad.

Please note that you cannot use special characters in every input field. For example, special characters are not usually permitted in tag names.

@  <ALT> + <64>
[  <ALT> + <91>
\  <ALT> + <92>
]  <ALT> + <93>
{  <ALT> + <123>
|   <ALT> + <124>
}  <ALT> + <125>
~  <ALT> + <126>

The download contains the complete ASCII table in PDF format.

ASCII_char_map.pdf ( 20 KB )

Which version of STEP 7 is compatible with which version of Microsoft Windows operating system?Go to beginning
Part number:

Compatibility Tool
A new Compatibility Tool is available for you at the Service & Support site.
It is designed to support you in questions of the compatibility of various SIMATIC software products.

The contents are due to be included in the Compatibility Tool.
We would appreciate your feedback on the new Compatibility Tool.
For this, please fill in and return the feedback form.

The table below contains the link to the Compatibility Tool and the feedback form.

Brief Instructions
To query the compatibility information you require, you must first choose a "master component" (WinCC, PCS 7, STEP 7, ...). To these "master components" you add more components (such as operating systems, virus scanners, other SIMATIC products, ...). Once you have chosen the components you require, you can have the compatibility list shown by hitting the "Show compatibility" button. A detailed description of the tool is available in the Online_Help.pdf file in the table below.
 
Contents

Link/Download

Link to Compatibility Tool
https://support.automation.siemens.com/kompatool/index.html?lang=en
Documentation
Online_Help.pdf
Feedback Form
Your feedback to assist in the further development of the Compatibility Tool.

Configuration Notes
Definitively the only operating systems that are released are those which are explicitly listed in the readme file. The table below shows the compatibility between the last two versions of STEP 7 and the current Windows operating systems. The compatibility list of the previous versions of STEP 7 is available as a PDF at the link.
 
STEP 7 version

Windows
2003 server

Windows XP
Professional 3)
Windows Vista 32 Bit
Ultimate and Business
Windows
Server 2008
(64-bit)
Windows 7
(32-bit)
Windows 7
(64-bit)

V5.4 incl. SPs

X1) X2) X3) - - -

V5.5

X5) X4) - - X6) -

V5.5+SP1

X9) X10) - X8) X7) X7)

1) MS Windows Server 2003 standard edition and MS Windows Server 2003 SP1 standard edition as workstation computer.
     For STEP 7 V5.4 SP4 Windows Server 2003 SP2 is required.
2) MS Windows XP Professional SP1 (or SP1a) or SP2 required.
    For MS Windows XP Professional SP3 you require STEP 7 V5.3 SP2.
    Not released under MS Windows XP SP2c.
3) As of STEP 7 V5.4 SP3. STEP 7 is not released for MS Windows Vista Home Basic and Premium.
4) MS Windows XP Professional SP2 or SP3.
5)
MS Windows Server 2003 SP2 / R2 SP2 standard edition as workstation computer.
6) MS Windows 7 Ultimate, Professional and Enterprise (standard installation). Windows XP mode in Windows 7 is not released.
    STEP 7 V5.5+SP1 is required for Windows 7+SP1.
7) MS Windows 7 Ultimate, Professional and Enterprise (standard installation) with or without SP1.
    Windows XP mode in Windows 7 is not released.
8) MS Windows Server 2008 R2 (64-bit), with or without SP1.
9) MS Windows Server 2003 R2 SP2 standard edition as workstation computer.
10) MS Windows XP Professional SP2 or SP3.

The PDF below shows the compatibility between the previous versions of STEP 7 and the Windows operating systems.
 
Contents

Link/Download

 Kompat_STEP7_Win.pdf

( 9 KB )

Further information
Information on other STEP 7 products is available in the compatibility list of your STEP 7 installation in Entry ID: 18734363 .
Information on the compatibility of Windows languages is available in Entry ID: 23568401 (Point 4) and 22635865.

Note on Windows 2000 Server
STEP 7 is not released for MS Windows 2000 Server.

Note on Windows XP
STEP 7 is not compatible with the 64-bit version of MS Windows XP Professional.

Keywords
Compatibility matrix , 49455057

Which SIMATIC software packages are compatible with which Microsoft Windows operating system and with STEP 7 V5.5?Go to beginning
Part number:

Compatibility Tool
A new Compatibility Tool is available for you at the Service & Support site.
It is designed to support you in questions of the compatibility of various SIMATIC software products.

The contents are due to be included in the Compatibility Tool.
We would appreciate your feedback on the new Compatibility Tool.
For this, please fill in and return the feedback form.

The table below contains the link to the Compatibility Tool and the feedback form.

Brief Instructions
To query the compatibility information you require, you must first choose a "master component" (WinCC, PCS 7, STEP 7, ...). To these "master components" you add more components (such as operating systems, virus scanners, other SIMATIC products, ...). Once you have chosen the components you require, you can have the compatibility list shown by hitting the "Show compatibility" button. A detailed description of the tool is available in the Online_Help.pdf file in the table below.
 
Contents

Link/Download

Link to Compatibility Tool
https://support.automation.siemens.com/kompatool/index.html?lang=en
Documentation
Online_Help.pdf
Feedback Form
Your feedback to assist in the further development of the Compatibility Tool.

Configuration Notes
The following compatibility list gives the compatibility of the different versions of the SIMATIC software packages with the last two versions of STEP 7 and with the various Microsoft Windows operating systems. The list is valid only for the versions given in these files.
 
Contents

Link/Download

German (release 12/2012-05a)
STEP7_Compatibility_de.pdf

( 305 KB )

English (release 12/2012-05b)
STEP7_Compatibility_en.pdf

( 321 KB )

French (release 12/2012-05c)
STEP7_Compatibility_fr.pdf

( 231 KB )

Italian (release 12/2012-05e)
STEP7_Compatibility_it.pdf

( 307 KB )

Spanish (release 12/2012-05d)
STEP7_Compatibility_es.pdf

( 309 KB )

The compatibility list for STEP 7 V5.5 is available on the STEP 7 installation CD under:
<CD-ROM drive>:\_Manuals\English\STEP7 - Compatibility List.pdf

After installing STEP 7 the latest compatibility list is also available in the Start bar under:
Start > SIMATIC > Information > English > STEP 7 - Compatibility List
.

Additional Keywords
Compatibility list, 49453265

 Entry ID:22636619   Date:2013-05-03 
I regard this article....as helpfulas not helpful                                 






























related links
How can you clear the error messa ...
Why can projects, blocks or the H ...
SIMATIC HMI Communication for Win ...
SIMATIC Windows Automation Center ...
DiagMonitor Getting Started
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour