show the entry list
S7-200 CPUs -- Configuring and programming communication -- Configuring communication to PCs
How do you establish a TeleService connection to an S7-200 via a TC65 terminal as remote modem with PIN transfer by PC/PPI cable?
How should you parameterize a GSM modem to set up a connection from an analog modem for teleservicing an S7-200?
How do you set up a teleservice connection based on MAS 21 to an S7-200 with MD720-3 via STEP 7 Micro/WIN?
How can you graphically display a variable of the PLC via EXCEL as OPC client with PC Access as OPC server?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Communicating with an S7-200 PLC via PPI using a CP5611 Card with Protool/Pro version 5.10
PPI connection of ProTool/Pro and S7-200
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
ProTool/ProRT and S7-200 with PC/PPI-Cable
Why do you get an error message when program downloading in various S7-S7-21x CPUs via USB/PPI or RS-232/ PPI Multi Master cable?
How do you set the network-related parameters for multimaster mode in STEP 7 Micro/WIN?
Which network configuration is typical when implementing the multimaster function?
Which cables do you use for communication in multimaster mode via the COM interface on the PC side?
How can you clear faults in Multimaster mode by parameterizing the COM communications interface on the PC side?
What alternatives are there to connecting to the multimaster network on the PC side?
Which cables do you use for communication in multimaster mode via the COM interface on the PC side?
Part number:

 

Configuration Notes:

Using the following PC/PPI cables together with STEP 7 Micro/WIN as from V 3.2 SP4 provides multimaster mode functionality.  
Product MLFB
Intelligent RS232/PPI cable with built-in RS232/RS485 converter 6ES7 901-3CB30-0XA0
Intelligent USB/PPI cable with built-in USB/RS485 converter 6ES7 901-3DB30-0XA0

The "M Master" setting must be enabled on the cable in order to be able to implement multimaster mode with RS232/PPI cables.

 Entry ID:22633270   Date:2006-02-17 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour