Instructions You can use the open communication through TCP connections for data exchange by way of the Industrial Ethernet CPs.
Below we describe how to configure a TCP connection for sending and receiving data by way of an Industrial Ethernet CP of S7-300 and S7-400.
TCP_Connection_en.pdf ( 2169 KB )
The functions below are called in the user program of the CPU for sending and receiving data by way of configured TCP connections.
- FC5 "AG_SEND" and FC6 "AG_RECV" for the S7-300
- FC50 "AG_LSEND" and FC60 "AG_LRECV" for the S7-400
The entries below contain sample programs and instructions for programming the above-mentioned functions in the user programs of S7-300 and S7-400: 17853532 and 18513371.
Note More information on communication over the Industrial Ethernet with S7-300 and S7-400 is available in the entries below.
| Entry ID |
Description |
| 26171811 |
What properties, advantages and special features does the TCP protocol offer? |
| 47885440 |
How do you configure an ISO-on-TCP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs? |
| 47885893 |
How do you configure a UDP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs? |
| 47885244 |
How do you configure an ISO transport connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs? |
| 29737950 |
How do you program the communication blocks FB63 "TSEND", FB64 "TRECV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by way of the integrated PROFINET interface of a CPU or by way of the CP443-1 Advanced? |
| 30564821 |
Functions (FC) and Function Blocks (FB) for SIMATIC NET S7 CPs Programming Manual |
|