Configuration Notes: The MAC addresses of CPU 317 PN/DP and CPU 315-2 PN/DP are preset and cannot be changed in the STEP 7 Hardware Configuration. You can identify the MAC address of the CPU via "PLC > Assign Ethernet address...".
  Fig. C3-01
The MAC address of CP 343-1 is preset, but depending on the system it can be changed for some CPs in the STEP 7 Hardware Configuration.
Warning:
This does not apply for the versions 6GK7343-1CX00-0EX0 (CP343-1 Lean), 6GK7343-1EX20-0XE0 and 6GK7343-1GX20-0XE0 (CP343-1 IT).
  Fig. C3-02
|