show the entry list
Industrial Ethernet S7-300/400 CPs -- Setting up and parameterizing hardware -- Synchronizing time
How do you configure the SIMATIC S7-300 as time master or time slave for time-of-day synchronization via Industrial Ethernet in SIMATIC mode?
How do you configure time synchronization?
Where can you find information on the Siclock system?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
How can you calculate the actual local time (summer time or winter time) in the S7-300/400 CPU and then use it on the panel as system time?
How do you configure the SIMATIC S7-400 as time master or time slave for time-of-day synchronization via Industrial Ethernet in SIMATIC mode?
How do you configure a PC as NTP server?
Why can't you use the IEEE Standard 1588 for synchronizing SIMATIC controllers?
Why can't you use the IEEE Standard 1588 for synchronizing SIMATIC controllers?
Part number:

Description:
The IEEE standard 1588 is entitled "Standard for a Precision Clock Synchronization Protocol for Networked Measurement and Control Systems", in short Precision Time Protocol (PTP). It defines a method and procedure for synchronizing multiple distributed real-time clocks that are linked via a package-relaying network. PTP is designed for implementation via Ethernet, but not limited to this. In principle any other package-relaying protocol that supports multicast addresses can also be used. The concept isolates the CSMA/CD layer from the upper application layer. In practice control of a process can thus be decoupled from the data transfer protocol.

However, this function is not supported by SIMATIC controllers or CP343-1/CP443-1.


 Entry ID:22144689   Date:2005-10-27 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour