Description: SQL Server 2000 SP3 has to be installed
in order to install WinCC V6.0 SP3.
The SQL server installation is supplied in WinCC.
There are two different SQL server CDs for WinCC V6.0 and WinCC
V6.0 SP3. The CD for WinCC V6.0 is marked "Siemens AG, Copyright
2003" and the CD for WinCC V6.0 SP3 is marked "Siemens AG,
Copyright 2004".
In order to install WinCC V6.0 SP3, ensure that you use the SQL
server CD marked "Siemens AG, Copyright 2004".
|