show the entry list
WinCC -- Setting up development environments -- Installing / transferring licenses
Why is the license not recognized when opening STEP 7?
How can you recover defective licenses and authorizations?
In SIMATIC WinCC V6.0 and higher there is no need for a license for "Basic Process Control"
Why is a WinCC server license demanded although the project has only been started on a single-user station?
Why was the software update WinCC V6.0 SP3 delivered without a license disk?
How do you perform a WinCC V6.0 SP3 license upgrade?
How do you perform a WinCC V6.0 license upgrade?
Why is there a license error message displayed with regard to storage even though storage is not in use?
Which license is required for communication via PROFIBUS FMS?
Which license do the archive servers require?
Which SIMATIC WinCC software package contains the S7 Lean license?
Which licenses do you require on which station when you use the different WinCC options?
What are the different types of tags available under licensing law?
Which license do you require in order to configure on a client?
Which SIMATIC WinCC software package contains the S7 Lean license?
Part number:

Configuration Notes
The Softnet S7 Lean license for 8 connections is supplied with new purchases of WinCC V6.0 SP3 and higher. When you order an upgrade package of WinCC, the Softnet S7 Lean licenses are not supplied or are supplied with the packages below:

  • Upgrades from V5.x to V6.x do not include the Softnet S7 Lean licenses.
  • Upgrades from V6.x to V6.2 or to V7.0 include the full license for Softnet S7 Lean.

 Entry ID:22083978   Date:2011-03-28 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour