show the entry list
MICROMASTER 4: PID filling level control with bumpless operating mode changeover
Part number:

Exclusion:

This application only applies to MICROMASTER 4 with Firmware < V4.0

 

Description:

PID controllers are used to control a wide range of process quantities. A typical application is a closed-loop level control for a cooling water reservoir. With this application, the water level must be kept constant in the reservoir, independent of the amount of water flowing into the reservoir. This means that the speed of the pump must be adapted according to the quantity of the water that flows into the reservoir order to pump-out the appropriate quantity of water. The actual water level in the reservoir is detected using a filling level sensor. Two pump operating modes should be provided - "automatic" and "manual". The mode is selected using a digital input, whereby the changeover between the operating modes is to be realized flying without shutting down the pump.

Downloads
Content of Downloads

Download

Documentation (German) tipps_tricks_011_PID-Fuelstandsregelung_de.pdf ( 133 KB )
Documentation (English) tipps_tricks_011_PID_Filling_level_control_en.pdf ( 132 KB )

 

History
Version

Modification

11/2005 first edition

 

Filter criteria:
Hardware platform: MICROMASTER
Software: none
Entry contents: Application Examples
 Entry ID:22079222   Date:2005-09-17 
I regard this article....as helpfulas not helpful                                 
related links
MICROMASTER 4: “Crane master sw ...
MICROMASTER 4- Torque Load Monitoring
MICROMASTER 440: manually determi ...
MICROMASTER: Working with differe ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
Contact
Support Request
Contacts worldwide
Technical Forum
QuickLinks
Compatibility tool 
Performance Data 
Micro Automation Sets
Help
Online Help
Guided Tour