|
Description: A project has been configured in German using WinCC flexible.
English has then been added as a second language. The languages have been exported, adapted and reimported.
Following import, the English texts are only visible on the engineering station, but not on the operating station.
Instructions: Compile the project with "Rebuilt All" and load this new compile project afterwards onto the operation station (panel) again.
| No. |
Procedure |
| 1 |
Start the compile process via "Project > Compiler > Rebuild All":
 ( 20 KB )
Fig. 01
A confirmation query then appears. Click "YES" to confirm.
The project is built. |
| 2 |
In preparation for the transfer, start "Project > Transfer > Transfer settings".
 ( 18 KB )
Fig. 02
The "Select devices for transfer" dialog is opened. |
| 3 |
Check the transfer settings and ensure that they match the device settings.
Click "Transfer" to perform the transfer.
 ( 24 KB )
Fig. 03
The newly created project is transferred to the operating station. |
|