show the entry list
WinCC -- Product information -- Checking compatibility
Compatibility Tool for Automation and Drive Technology
Important note on Microsoft Patches KB 943459 and KB 971468
Which licenses do you need to upgrade from WinCC flexible 2008 or WinCC V7 to WinCC V11 and in WinCC V11?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
With what are SIMATIC WinCC V7.x, V 6.x and V5.x compatible?
Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC WinCC?
How can you find out which Microsoft Patches are installed on the PC?
Further information on the Catalog ST80 with regard to WinCC Communication
Which operating system and software do you require for the SIMATIC WinCC Web Navigator V1.x, V6.x and V7.x?
With which Microsoft Windows operating systems is SIMATIC WinCC/ProAgent compatible?
Which security patch do you need for installing SIMATIC WinCC V6.0?
Drivers on the SIMATIC NET CD 07/2001 and WinCC
Notes on using WinCC V5.1 with "SIMATIC NET 7/2001 SP4"
Microsoft Windows language versions released for SIMATIC WinCC V5.1
WinCC -- Product information -- Information on WinCC Smart Tools
Compatibility Tool for Automation and Drive Technology
With what are SIMATIC WinCC V7.x, V 6.x and V5.x compatible?
EasyLanguage adds a 'T' to empty ToolTips upon export
Display/mask out first page/final page of the Dynamic wizard
Warning "Object has no or empty type property" when using the Export Wizard
Changing communication between WinCC server and client in WinCC V5 SP2
WinCC Configuration Tool: Error message while reading large WinCC-Projects
How can you make the menu item "WinCC" visible again in MS Excel when using the "WinCC Configuration Tool"?
Presetting the maximum number of lines in the WinCC Configuration Tool
How do you install the WinCC Smart Tools?
What Smart Tools are there for WinCC?
WinCC -- Configuring Tag Logging -- Importing and exporting archives
Compatibility Tool for Automation and Drive Technology
Can I save an archive cyclically anywhere?
In WinCC, how can exported archive segments of Alarm Logging or Tag Logging be connected/removed in Runtime?
With what are SIMATIC WinCC V7.x, V 6.x and V5.x compatible?
What Smart Tools are there for WinCC?
What options do you have for exporting a database in SIMATIC WinCC?
Why aren't any files created when exporting curve archives?
With what are SIMATIC WinCC V7.x, V 6.x and V5.x compatible?

Compatibility Tool
Compatibility information for WinCC is available in the Compatibility Tool of the Industry Online Support.
The tool is designed to support you in questions about the compatibility of various hardware and software products.
The database is constantly being revised and extended. In addition, you can use the tool centrally to download the compatibility lists of the separate product lines as Excel files.

We would appreciate your feedback on the new Compatibility Tool.
For this, please fill in and return the feedback form.

The table below contains the link to the Compatibility Tool and the feedback form.

Brief Instructions
To query the compatibility information you require, you must first choose a "master component" (WinCC, PCS 7, STEP 7, ...). To these "master components" you add more components (such as operating systems, virus scanners, other SIMATIC products, ...). Once you have chosen the components you require, you can have the compatibility list shown by hitting the "Show compatibility" button. A detailed description of the tool is available in the Online_Help.pdf file in the table below.
 
Contents

Link/Download

Link to Compatibility Tool
Documentation
Online_Help.pdf
Feedback form
Your feedback to assist in the further development of the Compatibility Tool.

 Entry ID:21927773   Date:2014-02-20