show the entry list
ProTool -- Creating HMI configurations -- Loading and testing configurations
Which settings do you have to make so that a ProTool project or WinCC flexible project can be transferred via TeleService Adapter IE?
Transferring the ProTool/Pro Runtime file (*.fwd) from the configuration computer to the visualization PC with the ProTool/Pro RT Loader
Automatic reset to serial transfer mode when the project download in ProTool V6.0 SP1 failed
ProTool Lite - Error when transferring a project
How can you transfer a ProTool project via MPI/PROFIBUS to a Windows-based panel?
How is an OP3 connected for the serial transfer of the configuration to the configuration PC?
What is the pin assignment for the adapter cable 6XV1440 - 2DE32 (TTY/V24)?
What is the serial cable assignment for transferring the configuration to an RMOS operator panel?
How do you make an MPI cable extension for an OP3?
What is the pin assignment for the plug-in connecting cable TD/OP <-> CP521 SI (V24)?
What is the serial cable assignment for transferring the configuration to a Windows-based device?
How do you load a project onto the operator panel with ProTool?
How do you use ProTool/Pro to configure the communication between a Windows-based operator panel and an S7 station via routing?
Why is the connection interrupted while transferring a project with ProTool to an OP?
Why can you not transfer the configuration from the PC to the Windows CE-based panel?
Using serial ports as of COM3 for ProTool project transfer from the PC to the panel
What is the serial cable assignment for transferring the configuration to an RMOS operator panel?
Part number:

Instructions:
For serial transfer via the V24 interface you should use only the cable TAG 6XV1 440 - 2K ... . The following length code applies:

6XV1 440 - 2K x ab

x = multiplier
x = E => 0.01m
x = H => 0.1m
x = N => 1.0m

ab = length code
ab = 10
ab = 12
ab = 15
ab = 16
ab = 20
ab = 25
ab = 32
ab = 40
ab = 50
ab = 60
ab = 63
ab = 80

Resulting length = Multiplier * Length code

Example:
Placing an order for a cable with a length of 1.5 meters.
The following order number results: 6XV1 440 - 2KH15
Multiplier H => 0.1m, length code = 15 => resulting length = 0.1m * 15 = 1.5m

When ordering, please note that the maximum cable length of 15 meters must not be exceeded.

If need be, for test purposes you can also use a cable that is wired as shown in the following figure.

Connector 1: 15-pin Sub-D male, V24
Connector 2: 9-pin Sub-D female, V24

Notes:

  1. Cable: 5 x 0.14 mm²; shielded; max. length 15 m.
  2. Shield connected on both sides over a wide area.
  3. This and other pin assignments are available in the manual "SIMATIC HMI Communication", in the chapter entitled "Interface Assignment", Entry ID: 1137086


Fig. 1      
 


 Entry ID:21923977   Date:2005-08-29 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour