Instructions: SIMATIC HMI Windows-based panels do not possess a TTY (20mA) interface which is needed for communication with a SIMATIC S5 PLC.
Exception:
The MP 370 operator panel possesses a TTY interface. Furthermore, the interface can be switched between V24 and TTY on a panel PC in the BIOS.
For all other Windows-based panels you need an adapter (9-pin female to 25-pin male) and an RS232/TTY converter cable for connecting to a SIMATIC S5.
Note:
The AS511 driver is no longer available for some operator panels for connecting to a SIMATIC S5 controller.
The latest information about which devices support the AS511 driver is available in the Online Help of WinCC flexible and ProTool, in the relevant manual of each operator panel, in the communication manual and in the ST80 catalog.
Below is an excerpt from the WinCC flexible Online Help.
  Fig. 01
There are two possible options:
Option 1: for a maximum distance of 3.2 meters
Siemens TTY/RS232 converter cable and an adapter (9-pin female to 25-pin male)

Fig. 02
| Article/description |
Order number |
Supplier |
Siemens TTY/RS232 converter cable
PLC 15-pin / PC 25-pin |
6ES5 734-1BD20 |
Siemens AG |
Adapter (9-pin female to
25-pin male). |
982075-14 |
Conrad Elektronik www.conrad.de |
Option 2: for a maximum distance of 1000 meters ELV TTY/RS232 converter.
  Fig. 03
| Article/description |
Order number |
Supplier |
| ELV AT adapter cable Sub-B 9-pin female to Sub-D 25-pin male |
68-078-86 |
ELV
www.elv.de |
ELV V24-20mA interface converter, ready-made device
Do-it-yourself instructions and description are available for downloading in a PDF file from the supplier. |
68-176-10 |
Note:
For connecting the ELV interface converter to the SIMATIC S5 you need an adapter cable (ELV interface converter Sub-D 25-pin male connector to S5 PLC Sub-D 15-pin male connector) wired according to the following pin assignment:
|
ELV interface converter
25-pin Sub-D male connector |
|
PLC / IP / CP
15-pin Sub-D male connector |
| Signal |
Pin |
|
Pin |
Signal |
| + 20 mA |
11 |
< jumper from
pin 11 to pin 18 |
|
|
| Sender + |
18 |
< jumper from
pin 18 to pin 11 |
|
|
| Sender - |
21 |
< to > |
9 |
TTY IN + |
| GND |
13 |
< to > |
2 |
TTY IN - |
| + 20 mA |
12 |
< to > |
6 |
TTY OUT + |
| Recipient + |
9 |
< to > |
7 |
TTY OUT - |
| Recipient - |
10 |
< jumper from
pin 10 to pin 14 |
|
|
| GND |
14 |
< jumper from
pin 14 to pin 10 |
|
|
Further Information:
| Connecting a Windows-based panel to an IM308C (SIMATIC S5) via PROFIBUS DP |
Entry ID:
17053153 |
| Connecting a Windows-based panel to the SIMATIC S5 (CP5431) via PROFIBUS DP |
Entry ID:
16640044 |
| Which program changes have to be made in an S5 controller if a line or graphics operator panel with PROFIBUS connection is replaced by a Windows-based operator panel? |
Entry ID:
21688871 |
| WinCC flexible Communication Manual |
Entry ID:
18797552 |
| ProTool Communication Manual |
Entry ID:
1405528 |
|