show the entry list
ProTool -- Configuring and programming communication -- Configuring communication to S5
Which program changes have to be made in an S5 controller if a line or graphics operator panel with PROFIBUS connection is replaced by a Windows-based operator panel?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Connecting a Windows-based panel to the SIMATIC S5 (CP5431) via PROFIBUS DP
Connecting a Windows-based panel to an IM308C (SIMATIC S5) via PROFIBUS DP
Which communication options exist for the different controllers / CPs, and how are they configured?
Which program changes have to be made in an S5 controller if a line or graphics operator panel with PROFIBUS connection is replaced by a Windows-based operator panel?
ProTool RT -- Configuring and programming communication -- Configuring communication to S5
Connecting a Windows-based panel to the SIMATIC S5 (CP5431) via PROFIBUS DP
Connecting a Windows-based panel to an IM308C (SIMATIC S5) via PROFIBUS DP
Which program changes have to be made in an S5 controller if a line or graphics operator panel with PROFIBUS connection is replaced by a Windows-based operator panel?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Which communication options exist for the different controllers / CPs, and how are they configured?
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to S5
Which program changes have to be made in an S5 controller if a line or graphics operator panel with PROFIBUS connection is replaced by a Windows-based operator panel?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Which communication options exist for the different controllers / CPs, and how are they configured?
Touch Panel / Operator Panel -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Which hardware can be connected to the USB port on Windows-based panels?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
What connecting cables are there for connections between the operator panels and the different controllers?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Connection of an OP3 on the MPI interface
OP3 - Transfer mode
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
Multi Panel -- Setting up and parameterizing hardware -- Setting up connections
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?
Why can you not access an enabled folder in Windows XP SP3 on a panel?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you integrate an HMI operator panel into a local network?
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
Microsoft ActiveSync connection for MP270, MP370
Which hardware can be connected to the USB port on Windows-based panels?
How do you transfer data from a server to a Windows-based panel via the FTP protocol?
Updating tags when a controller fails
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What connecting cables are there for connections between the operator panels and the different controllers?
How do you connect a panel to a SIMATIC H station?
Which GSDML files are there for the operator panels for Profinet IO?
Which GSD files are there for the Profibus DP operator panels?
How can you access a Microsoft Windows 2003 server with a panel / PC?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)?
How you change / save the size and position of the keyboard on Windows-based operator panels?
How do you read the current MPI / PROFIBUS address on a Windows CE panel?
How is the connection between a Windows-based panel and a SIMATIC S5 set up?
Part number:

Instructions:
SIMATIC HMI Windows-based panels do not possess a TTY (20mA) interface which is needed for communication with a SIMATIC S5 PLC.

Exception:
The MP 370 operator panel possesses a TTY interface. Furthermore, the interface can be switched between V24 and TTY on a panel PC in the BIOS.

For all other Windows-based panels you need an adapter (9-pin female to 25-pin male) and an RS232/TTY converter cable for connecting to a SIMATIC S5.

Note:
The AS511 driver is no longer available for some operator panels for connecting to a SIMATIC S5 controller.
The latest information about which devices support the AS511 driver is available in the Online Help of WinCC flexible and ProTool, in the relevant manual of each operator panel, in the communication manual and in the ST80 catalog.
Below is an excerpt from the WinCC flexible Online Help.


Fig. 01
 

There are two possible options:

Option 1: for a maximum distance of 3.2 meters

Siemens TTY/RS232 converter cable and an adapter (9-pin female to 25-pin male)


Fig. 02

 
Article/description Order number Supplier
Siemens TTY/RS232 converter cable
PLC 15-pin / PC 25-pin
6ES5 734-1BD20 Siemens AG
Adapter (9-pin female to
25-pin male).
982075-14 Conrad Elektronik www.conrad.de

Option 2: for a maximum distance of 1000 meters
ELV TTY/RS232 converter.


Fig. 03

 
Article/description Order number Supplier
ELV AT adapter cable Sub-B 9-pin female to Sub-D 25-pin male 68-078-86 ELV
www.elv.de
ELV V24-20mA interface converter, ready-made device
Do-it-yourself instructions and description are available for downloading in a PDF file from the supplier.
68-176-10

Note:
For connecting the ELV interface converter to the SIMATIC S5 you need an adapter cable (ELV interface converter Sub-D 25-pin male connector to S5 PLC Sub-D 15-pin male connector) wired according to the following pin assignment:
 

ELV interface converter
25-pin Sub-D male connector

  PLC / IP / CP
15-pin Sub-D male connector
Signal Pin   Pin Signal
+ 20 mA 11

< jumper from 
pin 11 to pin 18

   
Sender + 18

< jumper from 
pin 18 to pin 11

   
Sender - 21 < to > 9 TTY IN +
GND 13 < to > 2 TTY IN -
+ 20 mA 12 < to > 6 TTY OUT +
Recipient + 9 < to > 7 TTY OUT -
Recipient - 10 < jumper from 
pin 10 to pin 14
   
GND 14 < jumper from 
pin 14 to pin 10
   

Further Information:
 
Connecting a Windows-based panel to an IM308C (SIMATIC S5) via PROFIBUS DP Entry ID:
17053153
Connecting a Windows-based panel to the SIMATIC S5 (CP5431) via PROFIBUS DP Entry ID:
16640044
Which program changes have to be made in an S5 controller if a line or graphics operator panel with PROFIBUS connection is replaced by a Windows-based operator panel? Entry ID:
21688871
WinCC flexible Communication Manual Entry ID:
18797552
ProTool Communication Manual Entry ID:
1405528

 Entry ID:21923974   Date:2008-02-07 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour