show the entry list
WinCC -- Configuring and programming communication -- Communication to S7 (without PROFIBUS)
How do you integrate an existing WinCC project into a STEP 7 project?
Can I use the Slot PLC with WinCC V5.0?
What are the requirements for an online connection between WinCC and an S7 with MPI (CP5611)?
Which license do you need for communication via TCP/IP with WinCC?
What are the options for accessing an S7-200 with WinCC?
How do you set up a link via modem to an S7?
How can you link WinCC to S7 PLCSIM?
Which settings have to be made in WinCC to communicate with an S7 controller via the TS Adapter?
Which hardware and software is required in the WinCC system to communicate with an S7 via a CP343-1?
Which settings are required to access an S7 CPU with WinCC and SIMATIC NET via a CP5611, CP5613 or CP1613?
Industrial Ethernet PC software -- Configuring and programming communication -- Configuring connections
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S5, S7 and PC modules in the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via Industrial Ethernet in the SIMATIC NET Quick Start Collection?
Which hardware and software is required in the WinCC system to communicate with an S7 via a CP343-1?
How do you use the variable symbols defined in STEP 7 with the OPC server of SIMATIC NET?
How do you configure S5-compatible communication to the SIMATIC S5 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure S5-compatible communication to the SIMATIC S7 for a user application via Industrial Ethernet with the SIMATIC NET PC software?
How do you configure a PC station as PROFINET IO controller for connecting to a S7 station (as PROFINET IO device) for the SIMATIC NET OPC server with the SIMATIC NET PC software?
Establishing a connection from a PC to the S7-400 
How do you configure an S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
What should I watch out for when using an "S/R OPC Server" in the Fetch/Write service mode?
How do you configure S5-compatible communication to the SIMATIC S7 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you set up a Fetch/Write connection (S5-compatible communication) to the SIMATIC S5 via Ethernet for the SIMATIC NET OPC server with the SIMATIC NET CD 07/2001 or higher?
How do you configure S5-compatible communication to the SIMATIC S5 via Industrial Ethernet for the SIMATIC NET OPC server with the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for the SIMATIC NET OPC server via Industrial Ethernet with the SIMATIC NET PC software?
How do I create a Fetch/Write-connection (S5-compatible communication) to SIMATIC S7 for the SIMATIC NET-OPC Server via Ethernet with the SIMATIC NET CD 07/2001 or higher?
How do you configure an S7 connection via Industrial Ethernet with the SIMATIC NET OPC server and the SIMATIC NET PC software?
How do you configure a fault-tolerant S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software?
Which hardware and software is required in the WinCC system to communicate with an S7 via a CP343-1?
Part number:

Configuration Notes:
For communication between a CP343-1 and WinCC, on the WinCC side you need either a general network card (e.g. 3-Com) or a CP1613 card in the WinCC PC.

  • If you choose a general network card, you will need the SIMATIC NET "Softnet S7" license to be able to communicate with an S7. The corresponding SIMATIC NET driver must be installed.
  • If you choose a CP1613, you will need the SIMATIC NET "S7-1613" license to be able to communicate with an S7. The corresponding SIMATIC NET driver must be installed.

Note:
The relevant SIMATIC NET license ("Softnet S7") is included in the WinCC delivery package.

 Entry ID:21917403   Date:2005-08-25 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour