show the entry list
WinCC flexible ES -- Creating HMI configurations -- Loading and testing configurations
Why can you not transfer the HMI configuration to the panel?
How can you transfer a WinCC flexible configuration without configuration software to an operator panel (Pack&Go)?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC?
Which settings do you have to make so that a ProTool project or WinCC flexible project can be transferred via TeleService Adapter IE?
What can be the causes of the project download via TeleService not working?
How do you simulate the system keyboard via K or F-keys?
How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel?
How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel?
How can you transfer a WinCC flexible project serially to a panel?
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
How can you simulate with WinCC flexible the function keys of the various Windows-based operator panels via the PC keyboard?
Which cable can you use for data transfer between a Micro Panel and a configuration PC?
Why can't you simulate the Runtime for an OP73/OP73micro/TP177A/ TP177micro or OP77A in WinCC flexible on a PC?
Why can't you simulate the Runtime for an OP73/OP73micro/TP177A/ TP177micro or OP77A in WinCC flexible on a PC?
Part number:

Description:
In WinCC flexible 2004 / 2005 SP1 you have configured an OP73 / OP73micro / TP177A / TP177micro or OP77A. In the Engineering software the buttons and menu entries "Start Runtime" that are used for starting the Runtime simulation for other operator panels on the PC are grayed out and cannot be executed.

Explanation:
The Runtime simulation of an OP73 / OP73micro / TP177A / TP177micro or OP77A is not provided for in WinCC flexible 2004 nor in WinCC flexible 2005 SP1, so the corresponding selection options are grayed out and cannot be executed.

Note:
As of WinCC flexible 2007 it is now also possible to use the Runtime simulation of OP73 / OP73micro / TP177A / TP177micro or OP77A.

Remedy:
In order to be able to simulate the project nevertheless on the PC you can convert the operator panel into a comparable HMI device.

Procedure:
Open the project via "Project > Open" and then select "Project > Change Device Type...". Now select the relevant device type and confirm with "OK".
  

Operator panels without Runtime simulator

 

HMI device with Runtime simulator

OP73
OP73micro
OP77A
OP77B
TP177micro
TP177A
TP170A or TP177B

 Entry ID:21897529   Date:2006-05-22