show the entry list
WinCC flexible ES -- Working with projects -- Creating, editing, archiving and copying projects
Which entries are available in the internet concerning migration to STEP 7 V11 and WinCC V11 (TIA Portal)?
How can you change the column width of picture objects in WinCC flexible?
In WinCC flexible, how can you prevent pictures and picture objects being fitted automatically when you change the screen resolution (possibly widescreen)?
How do you activate access protection for a STEP 7 project and set up a user as project editor?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
What are the solutions offered for working with different versions of WinCC flexible?
Which problems might arise if the "log.LDF" file is not available in a WinCC flexible project?
Why does WinCC flexible close again automatically after the program start?
How can you save WinCC flexible projects / libraries as projects / libraries in the format of an earlier version of WinCC flexible?
How can you delete unused tags or objects from a WinCC flexible project?
What options do you have for copying pictures from one WinCC flexible project to another?
Copying HMI projects integrated in SIMATIC STEP 7 at file level
How can you open a WinCC project integrated in STEP 7 faster?
How do you archive projects in WinCC flexible and which files are required?
How do you back transfer the projects of an operator panel and what should you watch out for?
What transfer options are available in the various operator panels?
How do you archive projects in WinCC flexible and which files are required?
Part number:

Project archiving and migration
If you wish to archive a WinCC flexible project, you can reduce the volume and file size significantly by archiving just the following project files. Please refer also to the notes at the end of the entry on migrating WinCC flexible projects (opening a WinCC flexible project that is based on a previous version).

No. Project archiving in WinCC flexible 2007 and WinCC flexible 2008
1 Standalone project (a WinCC flexible project not integrated in STEP 7)
Start WinCC flexible ES and archive the project via the menu command "Project > Archive...". The project to be archived must not be opened during archiving.
The ZIP file created contains only the two files required for restoring your project - "Project.hmi" and "Project_log.LDF".
The next time you dearchive and open the project, the files deleted previously are automatically regenerated.


Fig. 01

2 WinCC flexible integrated in STEP 7
In the case of a project integrated in STEP 7, you use the archiving method of the SIMATIC Manager (File > Archive...).
From STEP 7 version V5.4 SP2 onwards, the WinCC flexible files are automatically reduced to files required for restoring your project. 

The next time you dearchive and open the project, the files deleted previously are automatically regenerated.

If you are using STEP 7 V5.4 + SP1, please refer to the information on "Project archiving in WinCC flexible 2005 SP1, Point 2".

 
No. Project archiving in WinCC flexible 2005 SP1
1 Standalone project (a WinCC flexible project not integrated in STEP 7)
If just the WinCC flexible project is to be archived without information for the delta compile, then only the following files are required.
  • ProjectName.hmi
  • ProjectName_log.ldf

The files are located in the relevant project directory.

The next time you open the project, the files deleted previously are automatically regenerated.

"Attachment 1" contains a breakdown of WinCC flexible files based on a sample configuration.

Attachment 1: Project_Data_2005.zip ( 11 KB )

2 WinCC flexible integrated in STEP 7
The procedure depends on the version of STEP 7:

Up to STEP 7 V5.4 SP1
If the WinCC flexible project integrated in STEP 7 is to be archived without information for the delta compile, you can delete the following files.

  • All files with the name "Project_n_{{..............................}}.data"
    e.g. -> PROJECT_1_{{9f58e235-cb6e-40eb-829f-e23350eedaca}}.data
  • Project_n.Device_1.fwx
    e.g. -> PROJECT_1.SIMATIC HMI Station(1).fwx

The files are located in your STEP 7 project directory under

  • "HmiES  > Devicename_n >"
    e.g. "HmiES  > PROJECT_1 >" 


Fig. 02

Then archive your STEP 7 project as usual.

The next time you open the project, the files deleted previously are automatically regenerated.

From STEP 7 V5.4 SP2 onwards
From STEP 7 version V5.4 SP2 onwards, you can use the archiving method of the SIMATIC Manager (File > Archive...).
The WinCC flexible files are automatically reduced to files required for restoring your project.

The next time you dearchive and open the project, the files deleted previously are automatically regenerated.

 
No. Project archiving in WinCC flexible 2004 / 2005
1 Standalone project (a WinCC flexible project not integrated in STEP 7)
If just the WinCC flexible project is to be archived without information for the delta compile, then only the following files are required.
  • ProjectName.hmi
  • ProjectName_log.ldf

The files are located in the relevant project directory.

The next time you open the project, the files deleted previously are automatically regenerated.

"Attachment 2" contains a breakdown of WinCC flexible files based on a sample configuration.

Attachment 2: Project_Data_2004.zip ( 11 KB )

2 WinCC flexible integrated in STEP 7
If the WinCC flexible project integrated in STEP 7 is to be archived without information for the delta compile, then only the following files of WinCC flexible are required.
  • GuidId.bin
  • GuidTp.bin
  • IdGuid.bin
  • ProjectName.devices
  • ProjectName.hmi
  • ProjectName_log.ldf

The files are located in your STEP 7 project directory under

  • "HmiES  > Devicename_n >"
    e.g. "HmiES  > PROJECT_1 >" 


Fig. 03

The next time you open the project, the files deleted previously are automatically regenerated.

Notes on migration
Opening a WinCC flexible project that is based on a previous version.
When you open a WinCC flexible ES project with more recent version of WinCC flexible ES, a message is displayed during the opening procedure indicating that the project to be opened has been created with a previous version of WinCC flexible.


Fig. 04

Acknowledge the message with the "OK" button and WinCC flexible automatically creates a backup file. The file is located in the same project directory as the remaining configuration.
You recognize the backup file generated by the names "Project_name.backup.hmi" and "Project_name.backup_log.LDF".

Example
MP370_Touch.backup.hmi, MP370_Touch.backup_log.LDF
You can archive these files elsewhere. They are not necessary for the WinCC flexible configuration.

Keywords:
Project archiving, Project file

 Entry ID:21896449   Date:2009-03-20 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour