show the entry list
Touch Panel / Operator Panel -- Setting up and parameterizing hardware -- Using additional components
What options are there for direct data communication between an FM 357-2 and a panel or Runtime (ProTool, WinCC flexible)?
What settings are to be made when connecting a printer to a Windows-based panel?
Which can be connected directly to a panel?
Printed page shifted in the log file with graphic machines and printer EPSON LQ300 
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
Floppy disk drive on OP 15, OP 17 and C7-624
How can you switch off the "Sleep" function on Brother printers?
What settings do you have to make to be able to print on a network printer with a Windows-based panel (except the 170 series)?
Cable for loading the configuration onto OP/TP
Connecting two printers to a panel with serial interfaces
Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have?
Mobile Panels -- Setting up and parameterizing hardware -- Using additional components
What options are there for direct data communication between an FM 357-2 and a panel or Runtime (ProTool, WinCC flexible)?
What settings are to be made when connecting a printer to a Windows-based panel?
What settings do you have to make to be able to print on a network printer with a Windows-based panel (except the 170 series)?
Which can be connected directly to a panel?
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
Which hardware can be connected to the USB port on Windows-based panels?
Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have?
Multi Panel -- Setting up and parameterizing hardware -- Using additional components
What options are there for direct data communication between an FM 357-2 and a panel or Runtime (ProTool, WinCC flexible)?
Which can be connected directly to a panel?
What settings are to be made when connecting a printer to a Windows-based panel?
How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this?
How can you switch off the "Sleep" function on Brother printers?
What settings do you have to make to be able to print on a network printer with a Windows-based panel (except the 170 series)?
Connecting two printers to a panel with serial interfaces
Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have?
HMI accessories -- Setting up and parameterizing hardware -- Using additional components
Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have?
Which hardware can be connected to the USB port on Windows-based panels?
Connecting two printers to a panel with serial interfaces
C7 6xx -- Product information -- Background and system information
Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have?
The C7 6xx complete devices are to be discontinued in October 2010 – what are their successors?
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
What transfer options are available in the various operator panels?
How many connection resources can be managed by the C7-CPU or the C7-OP?
Which GSD file do you need for a C7 Complete Device?
Which software do you need for the C7-621 module (with integrated AS interface master)?
How can you obtain an overview of the memory concept of SIMATIC S7-300 CPUs and C7 devices?
Why does the retentivity behavior of the S7-300 CPUs and C7 devices without MMC (Micro Memory Card) influence the contents of the variables?
Retentivity behavior of S7-300 CPU 31x and complete devices C7-6xx with MMC
Overview of components integrated in a C7 complete system
Comfort Panels -- Setting up and parameterizing hardware -- Using additional components
Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have?
What options are there for direct data communication between an FM 357-2 and a panel or Runtime (ProTool, WinCC flexible)?
Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have?
Part number:

Description
This FAQ shows operator panels with their associated interfaces. It also gives a list of the external storage media you can use.

Pictures of the storage media


Fig. 01: Multi Media Card (MMC)


Fig. 02: Secure Digital memory card (SD)


Fig. 03: Compact Flash card (CF)


Fig. 04: PC card adapter with CF card


Fig. 05: USB stick

Table of released storage media
 
Released storage media Order number
Multi Media CARD 6AV6 671-1CB00-0AX2
Secure Digital Memory CARD 256 MB 6AV6 671-8XB10-0AX0
Secure Digital Memory CARD 512 MB 6AV6 671-8XB10-0AX1
Secure Digital Memory CARD 2 GB 6AV2 181-8XP00-0AX0
PC Card Adapter und Compact Flash CARD 6AV6 574-2AC00-2AF1
Compact Flash CARD 6AV6 574-2AC00-2AA1
USB-Sticks 512 MB 6ES7 648-0DC20-0AA0
USB-Sticks     1 GB 6ES7 648-0DC30-0AA0
USB-Sticks     2 GB 6ES7 648-0DC40-0AA0
USB-Sticks     8 GB 6ES7 648-0DC50-0AA0

 Information

  • Function is guaranteed for memory cards and USB sticks tested and released by Siemens.
  • Siemens memory cards and USB sticks are available in Catalog ST80 in the chapter entitled "HMI Accessories".
  • MMCs can also be used on operator panels with SD slot.
  • The storage capacity of the memory cards and USB sticks might change with new products from the chip manufacturers.
  • MMCs for S7-300/400 controllers cannot be used on operator panels.
  • No difference between USB connections. There is no guarantee that "Storage Card USB" or "Storage Card USB2" will be assigned to a stick.

Assignment table for operator panels and associated interfaces
The operator panel assignment table and the associated interfaces are given in the PDF files attached. The assignment table also indicates which operator panels support USB sticks and in what capacity the storage media is supported.

21847868_HMI_Panels_Slots_e.pdf ( 78 KB )

Information about panels
You can use the following memory cards for a graphics OP:
 
Memory card MLFB Mbytes
SIMATIC S5, MEMORY CARD 6ES5 374-2FP21 8
SIMATIC S7, MEMORY CARD 6ES7952-1KL00-0AA0 2
SIMATIC S7, MEMORY CARD 6ES7952-1KM00-0AA0 4
SIMATIC S7, MEMORY CARD 6ES7952-1KP00-0AA0 8
SIMATIC S7, MEMORY CARD 6ES7952-1KS00-0AA0 16
RAM card 6AV1 903-0BB01 1
RAM card 6AV1 903-0BC01 2

Additional Keywords
MMC memory card, SD memory card, CF memory card, Universal Serial Bus, Flash drive, MMC-SD combi slot, MMC card, CF card, PC card, USB interface, Data storage, Data backup, WinCC flexible 2008, Export data externally, SD card

 Entry ID:21847868   Date:2013-01-16 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour