|
Description This FAQ shows operator panels with their associated interfaces. It also gives a list of the external storage media you can use.
Pictures of the storage media

Fig. 01: Multi Media Card (MMC)

Fig. 02: Secure Digital memory card (SD)

Fig. 03: Compact Flash card (CF)

Fig. 04: PC card adapter with CF card

Fig. 05: USB stick
Table of released storage media
| Released storage media |
Order number |
| Multi Media CARD |
6AV6 671-1CB00-0AX2 |
| Secure Digital Memory CARD 256 MB |
6AV6 671-8XB10-0AX0 |
| Secure Digital Memory CARD 512 MB |
6AV6 671-8XB10-0AX1 |
| Secure Digital Memory CARD 2 GB |
6AV2 181-8XP00-0AX0 |
| PC Card Adapter und Compact Flash CARD |
6AV6 574-2AC00-2AF1 |
| Compact Flash CARD |
6AV6 574-2AC00-2AA1 |
| USB-Sticks 512 MB |
6ES7 648-0DC20-0AA0 |
| USB-Sticks 1 GB |
6ES7 648-0DC30-0AA0 |
| USB-Sticks 2 GB |
6ES7 648-0DC40-0AA0 |
| USB-Sticks 8 GB |
6ES7 648-0DC50-0AA0 |
Information
- Function is guaranteed for memory cards and USB sticks tested and released by Siemens.
- Siemens memory cards and USB sticks are available in Catalog ST80 in the chapter entitled "HMI Accessories".
- MMCs can also be used on operator panels with SD slot.
- The storage capacity of the memory cards and USB sticks might change with new products from the chip manufacturers.
- MMCs for S7-300/400 controllers cannot be used on operator panels.
- No difference between USB connections. There is no guarantee that "Storage Card USB" or "Storage Card USB2" will be assigned to a stick.
Assignment table for operator panels and associated interfaces The operator panel assignment table and the associated interfaces are given in the PDF files attached. The assignment table also indicates which operator panels support USB sticks and in what capacity the storage media is supported.
21847868_HMI_Panels_Slots_e.pdf ( 78 KB )
Information about panels You can use the following memory cards for a graphics OP:
| Memory card |
MLFB |
Mbytes |
| SIMATIC S5, MEMORY CARD |
6ES5 374-2FP21 |
8 |
| SIMATIC S7, MEMORY CARD |
6ES7952-1KL00-0AA0 |
2 |
| SIMATIC S7, MEMORY CARD |
6ES7952-1KM00-0AA0 |
4 |
| SIMATIC S7, MEMORY CARD |
6ES7952-1KP00-0AA0 |
8 |
| SIMATIC S7, MEMORY CARD |
6ES7952-1KS00-0AA0 |
16 |
| RAM card |
6AV1 903-0BB01 |
1 |
| RAM card |
6AV1 903-0BC01 |
2 |
Additional Keywords
MMC memory card, SD memory card, CF memory card, Universal Serial Bus, Flash drive, MMC-SD combi slot, MMC card, CF card, PC card, USB interface, Data storage, Data backup, WinCC flexible 2008, Export data externally, SD card
|