show the entry list
WinCC flexible Options -- Product information -- WinCC flexible /Sm@rtService (Teleservicing)
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?
How can you use a PC to simulate or realize sending e-mails in the case of an HMI station message?
What should you watch out with regard to licenses for WinCC flexible and panels?
What are the options for remote maintenance of a WinCC flexible Runtime system (Panel/PC) via the Internet (WAN)?
Connection to the SIMATIC WinCC flexible Sm@rtServer gets lost (with active screensaver or "Shut Down")
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
Why do you get the message "Under Construction" in WinCC flexible 2004/2005 when attempting to connect to the MiniWeb via the HTML viewer?
Why, when you call the Sm@rtClient, is only an empty page displayed in the Internet Explorer?
How do you send e-mails from a Windows CE panel or PC with SIMATIC WinCC flexible?
How do you send short messages (SMS) from an SIMATIC WinCC flexible HMI station to a mobile phone?
Why, when you call the Sm@rtClient, is only an empty page displayed in the Internet Explorer?
Part number:


Description:
If, when you start the Sm@rtClient, only an empty page is displayed (Fig. 01), then the Java Runtime Environment (JRE) is probably missing on your computer.


Fig. 01

Remedy:
At the following link http://www.java.com you can download the Java software,
(the Java Runtime Environment (JRE)). 
For this you click on the "Java Software Download" button.

Once you have installed the Java software, after calling the Sm@rtServer, the remote screen is displayed in the Internet Explorer (Sm@rtClient) (Fig. 02).


Fig. 02
 

 

 

 Entry ID:21809933   Date:2005-07-18 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour