show the entry list
WinCC flexible ES -- Working with projects -- Creating multilingual projects
How do you change the language on an operator panel?
How do you configure Asian fonts in WinCC flexible?
What might be the cause for texts not being displayed completely after import, for example?
What might be the cause for not all the user interface languages being available for selection?
How can you reinstall project languages that are no longer supported after installing the Microsoft Security Patch MS07-040 (KB 939949)?
Which languages are available in WinCC flexible?
How can you export and import texts with WinCC flexible in Microsoft Windows XP or Windows 2000?
How do you get around the problems which arise when importing a second language in WinCC flexible?
How is the user interface language set in WinCC flexible?
Why is the current language set not saved on the operator panel?
How do you create a user dictionary in WinCC flexible and how can you use it in other projects?
How can you export and import texts with WinCC flexible in Microsoft Windows XP or Windows 2000?
Part number:

Instructions:
Proceed as follows to export project texts from WinCC flexible and import project texts into WinCC flexible.

Note:
You should also note that when you change languages and then restart the PC or you log on again to the PC, the active keyboard is the one set when you changed languages.
This means that when you change to Russian, for example, then the "Russian keyboard layout" is active.
If you have to log on to the PC, then it is made via the "Russian keyboard layout" => different font!

 
No. Settings required in Windows 2000
1 Note:
You need administrator rights for making settings in Windows 2000.
In general you also need the Microsoft Windows 2000 CD to retroinstall languages.

Retroinstalling Russian as language in Windows 2000:

  • Open the menu "Regional Options" via
    "Start > Settings > Control Panel > Regional Options". 
  • Select the "General" tab and under "Language settings for the system" set a check mark for "Cyrillic".
  • Click on "Apply".


Fig. 01  
 

  • The files required (from the Microsoft Windows 2000 CD) are retroinstalled and then you must restart the PC.
  • Reopen Regional Options on your computer.
  • Select "Russian" under "Your locale (location)".


Fig. 02  
 

  • Define Russian as system default via
    "Set default... > Russian".


Fig. 03  
 

This completes the settings in the Control Panel.

2

Text export in WinCC flexible

  • Open your project and in the WinCC flexible menu bar select
    "Options > Texts  > Export ...".

.
Fig. 04
 

  • Under "Storage Location (Path)" you define a storage location and under "Format" the desired  Excel format, e.g. Excel table (*.csv) or Excel workbook (*.xls) ("Arbeitsmappe"). Under "Languages" you select "Deutsch" (German), for example, as Source Language and "Russisch" (Russian) as Target Language.
    Acknowledge with "OK". The Excel files are then created.

Note:
Using the Language Support Tool, which is installed as from STEP 7 V5.3, you can also choose the export format *.xls (Excel workbook).


Fig. 05  
 

3

Setting the keyboard layout in Windows 2000

  • Set the Russian keyboard layout in Windows.


Fig. 06  
 

4 Editing the exported file
  • Use an editor, e.g. Microsoft Excel, to open the CSV file created by first opening Excel and then opening the file via "File  > Open".
    (do not open the file by double-clicking it).
  • Translate the texts in the second column (Column B) into Russian.
  • Save the changes in the files and then close the files.


Fig. 07  
 

5

Text import in WinCC flexible

  • Open your project and in the WinCC flexible menu bar select
    "Options > Texts  > Import ...".
  • Select the storage location in which the translated CSV or XLS files are located.
  • Under "Format" select the relevant file format and acknowledge with "OK".


Fig. 08  
 

The translated texts are now integrated in the configuration.
You can view the translated texts in the configuration by changing the editing language accordingly.

 
No. Settings required in Windows XP
1 Note:
You need administrator rights for making settings in Windows XP.
In general you also need the Microsoft Windows XP CD to retroinstall languages.

Retroinstalling Russian as language in Windows XP:

  • Open the menu "Regional and Language Options" via
    "Start > Settings > Control Panel > Regional and Language Options". 
  • Select the "Advanced" tab and under "Code page conversion tables" set a check mark for "Cyrillic".
  • Click on "Apply".
  • You might have to retroinstall files (from the Windows XP CD) and then you must restart the computer.
  • Reopen "Regional and Language Options" on your computer.
  • Select "Russian" as the language under "Language for non-Unicode programs".


Fig. 09  
 

  • Switch to the "Regional Options" tab.
  • Under "Standards and formats" you select "Russian" as the language.


Fig. 10
 

Setting the keyboard layout in Win XP

  • Then open the "Languages" tab.
  • Click on the "Details" button to open the dialog for defining the default input language and methods.
  • In the "Settings" tab select "Russian-Russian" under "Default input language"


Fig. 11
 

Close the Regional and Language Options dialog with "OK".
This completes the settings in the Control Panel.

2

Text export in WinCC flexible

  • Open your project and in the WinCC flexible menu bar select
    "Options > Texts  > Export ...".

.
Fig. 12  
 

  • Under "Storage Location (Path)" you define a storage location and under "Format" the desired  Excel format, e.g. Excel table (*.csv) or Excel workbook (*.xls) ("Arbeitsmappe"). Under "Languages" you select "Deutsch" (German), for example, as Source Language and "Russisch" (Russian) as Target Language.
    Acknowledge with "OK". The Excel files are then created.

Note:
Using the Language Support Tool, which is installed as from STEP 7 V5.3, you can also choose the export format *.xls (Excel workbook).


Fig. 13  
 

3 Editing the exported file
  • Use an editor, e.g. Microsoft Excel, to open the CSV file created by first opening Excel and then opening the file via "File  > Open".
    (do not open the file by double-clicking it).
  • Translate the texts in the second column (Column B) into Russian.
  • Save the changes in the files and then close the files.


Fig. 14  
 

4

Text import in WinCC flexible

  • Open your project and in the WinCC flexible menu bar select
    "Options > Texts  > Import ...".
  • Select the storage location in which the translated CSV or XLS files are located.
  • Under "Format" select the relevant file format and acknowledge with "OK".


Fig. 15  
 

The translated texts are now integrated in the configuration.
You can view the translated texts in the configuration by changing the editing language accordingly.

General notes:

  • Do not change your WinCC flexible project between exporting and importing the language texts.
  • Only add the translations in the CSV or XLS files. If you make changes to the source language texts (first column), then the CSV or XLS file can no longer be imported.
  • You can only translate the texts on a Russian Windows 2000/ Windows XP or a Windows 2000 / Windows XP MUI set to Russian.
  • If, after adding the Russian translation in the CSV or XLS file, you change the regional default setting back to Germany, the Russian translations are no longer displayed in the file, even if you set the default input language to Russian. Only special characters are displayed instead of the Cyrillic characters. However, after importing the translation in WinCC flexible, the Russian translations originally configured are displayed correctly in WinCC flexible.
  • In order to add Asian languages to a project you need Asian Windows 2000/ Windows XP and Asian Excel. You do not need Asian WinCC flexible on the computer on which the translations are made. You can import the finished texts into the project on a PG/PC with a European WinCC flexible.

 Entry ID:21752508   Date:2005-07-06 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour