Mostrar lista de artículos
ET 200M (standard modules) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Configuring SIPLUS extreme modules
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Which options are available for configuring the ET 200 stations?
Parameterization data of an analog module in an ET 200 are not transferred when using an external master
Configuring a power supply for an IMxxx in the ET200M
Configuring the Dummy Module => BF in ET200M
Parameterizing the ET200-M (IM153-x) only possible in hex code
The input values of an analog module in the ET 200M sporadically have the value zero
ET200-M with active backplane bus.
Configuring IM153-3 (ET200-M)
"Change of module during operation" parameter option on an ET 200 M
Operating ET200M as slave on master station CPU315-2DP
No startup of ET200M station when using blank slots
"Module change during operation" - Configuration and system requirements
Display of the "Parameter Assignment" tab for the configuration of modules
Output channels of SM 335 do not work
How do you calculate the times for the clock-synchronized operation of ET 200M?
Operating ET200M as slave on master station CPU315-2DP
Referencia:

QUESTION:
How can I link a slave station of the ET200M type to a master station CPU315-2DP?

ANSWER:
There are 2 steps to configuring an ET200M slave station:
In the first step you link the station and parameterize it.

In the second step you configure the slave by selecting and parameterizing the modules that are to be processed in the slave.

Step 1: Link slave to master station
After configuring the master station you will find three interface modules of the type IM 153-1 under +PROFIBUS-DP > ET200M in the "H/W CATALOG”. Select the interface module you require and pull it onto your DP master's slave phase.

As a result the dialog box "Properties-PROFIBUS users” opens with General and Network Connection tabs.
In the Network Connection tab you set the required L2 user address for the slave (options between 1 and 125), and under the PROPERTIES you can set the parameters of the PROFIBUS network (baud rate, highest PROFIBUS address in the network).
In the General tab you read the data and change the name of the station.
Acknowledge with "OK” and the dialog box "Properties-DP slave” opens. In this you enter the diagnostics address under which you can process the slave data in the master station.
When you have entered the data and transferred with "OK”, then the slave station is output with the current L2 user address (x) in the tool "H/W CONFIG”.

Step 2: Configure slave
In "H/W CATALOG” you select the required module under the previously selected master interface module (IM153-1) and place it on the required slot (4 to 11) of the ET200M. Finally you parameterize the address and operating parameters of the single module.

The following limits must be observed when configuring the ET200M slave:

  • Maximum of 8 modules in 1 station
  • Address area is limited to a maximum of 122 input bytes and 122 output bytes.
  • Maximum of 7 analog cards with 8 channels is possible, since 7 * 8 *2 bytes =112 bytes (each channel requires 2 bytes).

 Nr. de identificación (ID):217410   Fecha:1998-02-05