Instructions: If the data has been sent successfully
to WinCC, the parameter "DONE" of the AR_SEND block is set to "1".
In WinCC there is no way of checking whether the data has been
stored successfully in the archive.
Note:
If the data has its own time stamp in AR_SEND, it is also stored
chronologically in WinCC. Detailed information on
parameterizing the AR_SEND block is available in the WinCC
Information System (WinCC Online Help) under the keyword "AR_SEND:
Data Block Structures - Structures and Parameters". Note the
examples given there.
|