Instructions Process values transferred via the AR_SEND are stored by default in the WinCC archive "TagLogging Fast".
For WinCC V6.0
In WinCC V6.0 it is not possible to parameterize the storage location for this data.
For WinCC V6.2 onwards
In WinCC V6.2 you can choose whether the process values are to be stored in the "TagLogging Fast" or "TagLogging Slow" archive.
For this you open the "Tag Logging" editor and then the properties of the "TagLogging Fast" archive. Select the "Archive contents" tab.

Fig. 01
To archive process values in the "TagLogging Fast" archive, you now select the "Process-controlled measured values" check box. If the check box is not selected, the process values are archived in the "TagLogging Slow" archive.
More information is available in the WinCC Information System (WinCC Online Help) under the keyword "Storing Process Values".
|