show the entry list
SIMOTION -- hardware -- Configuring and parameterizing SIMATIC I/O modules
Integration of AS interface slaves (DP/AS interface link 20 E ) via I/O interface or system functions.
Integration of the SIWAREX CS (7MH4910-0AA01) Electronic Weighing System into SIMOTION.
SIMOTION with RFID system ASM 456 and Moby D.
Integration of AS interface slaves using CP343-2 via I/O interface or system functions.
Integration of the ASM470 Interface Module via I/O Interface.
Integration of the MOBY ASM450 Interface Module via I/O interface.
Approved I/O modules for SIMOTION.
Integration of the SIWAREX CS (7MH4910-0AA01) Electronic Weighing System into SIMOTION.
Part number:

QUESTION:
How is the SIWAREX CS electronic weighing system integrated into SIMOTION?

 

ANSWER:
The function blocks "FB SICS_BA" and "FB SICS_DR" provided for the SIMATIC S7 are currently not available for SIMOTION. With certain restrictions (i.e. no service, adjusting and weighing commands), the SIWAREX CS electronic weighing system can nevertheless be integrated into SIMOTION via the I/O interface and the data block communication. 

The attached example illustrates the integration via the I/O interface and data block communication.

Siwarex_e.pdf ( 18 KB )

Siw_CS.zip ( 1 KB )

 Entry ID:21554724   Date:2005-05-11