Configuration Notes This entry provides information about which function modules can be configured in an ET 200M remote IO system and which can then be operated remotely.
Below is a list of the function modules that can be configured and used behind the PROFIBUS interface modules of the ET 200M.
In the compatibility list a difference is made between configuration via the metaknowledge integrated in STEP 7 and GSD configuration.
21536617_Compatibility_FM_with_PROFIBUS_InterfaceModules_en.pdf ( 83 KB )
In the entry below is a list of the function modules that can be configured and used behind the PROFINET interface modules of the ET 200M: 45313498.
Note
The entry below provides you with more information about function modules which use the functions "Read data record" and "Write data record": 15364459.
The entry below provides more information about using a positioning module FM 357-2: 21385102.
|