show the entry list
ET 200M (standard modules) -- Product information -- Checking compatibility
Which PROFIBUS connectors can you use in Zone 1 or 2?
Y link: in spare parts case, only replacement of the defective IM157 is necessary
Which function modules (FM) can be used remotely in an ET 200M?
FM 350-1, 350-2, 450, SM338 -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How can the counter values of compact CPUs and of the FM 350 counter module be made available again after a power failure?
How do you commission the FM350-2 counter module (6ES7350-2AH01-0AE0) in STEP 7 Professional V11 and higher?
How do you commission the FM350-1 counter module (6ES7350-1AH03-0AB0) in STEP 7 Professional V11 and higher?
Why with module FM350-1 does the internal gate STS_GATE remain open in single count mode although the software gate SW_GATE closes?
Which function modules (FM) can be used remotely in an ET 200M?
How do you interconnect an FM350-2 in PCS 7?
How can you retain the counter value of counter modules (6ES7350-1AH03-0AE0, 6ES7350-2AH00-0AE0, 6ES7450-1AP00-0AE0) after a STOP to RUN transition of the CPU?
How can you fast load an initial value in the counter group FM350-1 or FM450-1?
How can you generate a process alarm with the latch function on the "FM350-1" module?
Images mixed up in the FM450-1¿s configuration package for displaying the hardware gate controller 
Specifying direct I/O access to the FM 350-2, 2 channels
SM 338: how do you handle disconnected channels?
FM 351, 451 -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you commission the FM351 positioning module (6ES7351-1AH02-0AE0) in STEP 7 Professional V11 and higher?
Which function modules (FM) can be used remotely in an ET 200M?
How can you prevent losing the absolute value encoder adjustment/cam parameters when you restart your CPU or FM?
FM351 for the measuring of the actual value
FM351 with CPU WinLC V4.0
FM 352-5 -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
What can you do if the required FM352-5 is not in the catalog in the HW Config after installation of the programming environment V1.2 SP2?
Which function modules (FM) can be used remotely in an ET 200M?
Why do errors occur in FM352-5 with nested logic program?
FM 352-5 parameterization for Standalone mode
FM352-5: What should I do if the compiling of the application function block is aborted with an error message?
FM352-5 Know How Protection
FM 353, 354, 453 -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
What must be considered when using the SIMATIC S7 FM354 module with incremental encoder?
What should you watch out for when calling FB POS_CTRL and FB POS_MSRM?
Which function modules (FM) can be used remotely in an ET 200M?
What should you watch out for when parameterizing a digital input for the "Set flying actual value" function in Automatic mode?
How do you assign parameters to an FM354 when using an absolute linear rule?
What does MD38 signify with FM 353?
How can you reduce the positioning times for short distances?
What invokes the procedure program error 0x0801 "Program selection subprogram error"?
How many FM 353s or FM 354s can the communicate with an OP that is connected to the CPU via MPI?
Transferring an NC block (traversing program) by user program to an FM353 / FM354
Aborting an active MDI record of an FM353 or FM354
Behavior of the FM 354 upon signal change at the release input
FM 355, 455 -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Which function modules (FM) can be used remotely in an ET 200M?
Rated value configuration of the FM355C
What should you pay attention to when the ramp function of FM 355-2 is switched on?
What is the function of the SDB_SEL parameter of the FB PID_FM?
What should you watch out for with a fuzzy closed-loop control with the FM 355 / FM 455?
How can I prevent the FM 355C from overshooting when switching from safety mode to "control mode"?
Refreshing the controller parameter in the FM355-2
FM 357 -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Which function modules (FM) can be used remotely in an ET 200M?
What has to be considered when using the FM357-2 in a distributed configuration?
What must be considered when using curve tables with SPLINE?
How can you use SIMATIC HMI Operator Panels in conjunction with the module FM 357?
Functions and Samples: Implementing the Function "Set Setpoint Value on the Fly" with FM357-2
Restart of the FM357-2
Modification of the zero shifts on the FM357-2
Notes regarding the commissioning of a FM 357-2 with PROFIBUS-Drives
What options are there for direct data communication between an FM 357-2 and a panel or Runtime (ProTool, WinCC flexible)?
FM 352, 452 -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How do you commission the FM352 cam controller (6ES7352-1AH02-0AE0) in STEP 7 Professional V11 and higher?
What I need to take care if an old FM 352(6ES7352-1AH01-0AE0) will be replaced by a new FM 352(6ES7352-1AH02-0AE0)?
What should you watch out for when writing machine data to the FM352?
Which function modules (FM) can be used remotely in an ET 200M?
How can you prevent losing the absolute value encoder adjustment/cam parameters when you restart your CPU or FM?
What do you need to watch out for when loading parameters with the commissioning software for the FM352?
Changing dynamization times in operation by "fast cam" on an FM352
FM352/452: Processing of process alarms
Which function modules (FM) can be used remotely in an ET 200M?
Part number:

Configuration Notes
This entry provides information about which function modules can be configured in an ET 200M remote IO system and which can then be operated remotely.

Below is a list of the function modules that can be configured and used behind the PROFIBUS interface modules of the ET 200M.
In the compatibility list a difference is made between configuration via the metaknowledge integrated in STEP 7 and GSD configuration.

21536617_Compatibility_FM_with_PROFIBUS_InterfaceModules_en.pdf ( 83 KB )

In the entry below is a list of the function modules that can be configured and used behind the PROFINET interface modules of the ET 200M: 45313498.

Note
The entry below provides you with more information about function modules which use the functions "Read data record" and "Write data record": 15364459.
The entry below provides more information about using a positioning module FM 357-2: 21385102.

 Entry ID:21536617   Date:2011-03-28 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour