show the entry list
ET 200S (standard modules) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How can you group together the address area of the ET 200S in STEP 7 (TIA Portal) using the "Pack Addresses" function?
How do you commission the serial interface module 1SI 3964/ASCII (6ES7138-4DF01-0AB0) in STEP 7 Professional V11 and higher?
How do you commission the serial interface module 1SI MODBUS/USS (6ES7138-4DF11-0AB0) in STEP 7 Professional V11 and higher?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you reset the IP address and device name of an I device?
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find information of the reproducibility of delay interrupts and cyclic interrupts for IM151-8 and IM154-8?
How is reparameterization performed when replacing the IO link master module or the IO link device?
Which options are available for configuring the ET 200 stations?
Where can you find information on installation guidelines for an ET 200S station?
Which diagnostics messages might you get when commissioning the ET 200S as PROFINET IO device?
Which diagnostics messages might you get when commissioning the ET 200S as PROFIBUS DP slave?
TeleService with ET200S (IM151-CPU) and TS Adapter
Can I use a Quickstop function with an ET 200S Motor Starter?
How can you combine fail-safe and standard modules in the ET 200 stations?
Parameterizing ET 200 S DI 4xNAMUR (6ES7 131-4RD00-0AB0)
Temperature compensation of a thermocouple using a resistance thermometer Pt100 to capture the reference junction temperature
Temperature Compensation of a Thermo-element via the Electronic module 2AI TC HF
How can you group the addresses of ET200S IM151-1 HF (pack addresses) in HW Config?
IM 151-7 CPU: Porting Programs with Packed Addresses
How can you group together the address area of the ET 200S (pack addresses)?
Which ET 200S modules support the option handling function?
What conditions do you have to comply with when configuring ET 200S modules?
What should you watch out for regarding the compatibility of I/O modules and interface modules when configuring an ET 200S?
How can you use Bürkert pneumatic modules in the ET 200S remote I/O system?
How can you prevent the bus error LED from lighting on interface module IM 151 when using reserve modules?
How can you prevent the bus error LED from lighting on interface module IM 151 when using reserve modules?
Part number:

 

The bus error LED lights on the interface module in this case because the DP master expects other modules. In the case of defective modules or incorrect parameters this behavior might be welcome

The reserve modules are implemented when specific functions are to be added to a system. For this reason, the parameters for the final configuration of the system are assigned, but reserve modules are slotted instead of the input/output modules. The "Option Handling" function is provide for the Hardware Configuration to reserve the addresses required.

Instructions:
Proceed as follows to configure option handling:
 
No. Configuring option handling
1 Configure the ET 200S station as it should be in the extended state.
2 Open the Object Properties of the ET 200S slave.


Fig. 01

3 Here you can select the modules on which you want to enable the "Option Handling" function.


Fig. 02

4 Now switch to the Object Properties of the power module.


Fig. 03

5 Here you also activate option handling.


Fig. 04

Note
If, when you remove one I/O module, the ET 200S station is to maintain cyclic data communication, you must select the option "Operate with setpoint <> actual configuration" in the Object Properties of the DP station. If you do not select this option, then when you remove one module, the whole station fails (including call of OB 86 in the DP master).

More information on option handling is available in the manual "ET 200S Distributed I/O System". The manual is available in Entry ID: 1144348 .

 Entry ID:21407118   Date:2006-02-07